30 Built-In DSP Functions
Many PIC32 MCUs support a DSP engine, including instructions that are designed to improve the performance of DSP and media applications. The DSPr2 engine provides instructions that operate on packed 8-bit/16-bit integer data, Q7, Q15 and Q31 fractional data.
The XC32 C compiler supports these DSP operations using both the generic vector
extensions and a collection of built-in functions. Both kinds of support are enabled
automatically when you select a DSP device with the -mprocessor
option.
The SCOUNT and POS bits of the DSP control register are global. The WRDSP, EXTPDP, EXTPDPV and MTHLIP instructions modify the SCOUNT and POS bits. During optimization, the compiler will not delete these instructions and it will not delete calls to functions containing these instructions.
At present, the XC32 C compiler provides support for only operations on 32-bit vectors. The vector type associated with 8-bit integer data is usually called v4i8, the vector type associated with Q7 is usually called v4q7, the vector type associated with 16-bit integer data is usually called v2i16, and the vector type associated with Q15 is usually called v2q15. They can be defined in C as follows:
typedef signed char v4i8 __attribute__ ((vector_size(4)));
typedef signed char v4q7 __attribute__ ((vector_size(4)));
typedef short v2i16 __attribute__ ((vector_size(4)));
typedef short v2q15 __attribute__ ((vector_size(4)));The v4i8, v4q7, v2i16 and v2q15 values are initialized in the same way as aggregates. For example:
v4i8 a = {1, 2, 3, 4};
v4i8 b;
b = (v4i8) {5, 6, 7, 8};
v2q15 c = {0x0fcb, 0x3a75};
v2q15 d;
d = (v2q15) {0.1234 * 0x1.0p15, 0.4567 * 0x1.0p15};- The first value is the least significant and the last value is the most significant. The code above will set the lowest byte of a to 1.
- Q7, Q15 and Q31 values must be initialized with their integer representation. As shown in this example, the integer representation of a Q7 value can be obtained by multiplying the fractional value by 0x1.0p7. The equivalent for Q15 values is to multiply by 0x1.0p15. The equivalent for Q31 values is to multiply by 0x1.0p31.
The table below lists the v4i8 and v2q15 operations for which hardware support exists. The a and b are v4i8 values, and c and d are v2q15 values.
| C Code | Instruction |
|---|---|
a + b | addu.qb |
c + d | addq.ph |
a - b | subu.qb |
c - d | subq.ph |
The table below lists the v2i16 operation for which hardware support exists. The e and
f are v2i16 values.
| C Code | Instruction |
|---|---|
e * f | mul.ph |
It is easier to describe the DSP built-in functions if the types are defined beforehand.
typedef int q31;
typedef int i32;
typedef unsigned int ui32;
typedef long long a64;The q31 and i32 operations are actually the same as int, but q31 is used
to indicate a Q31 fractional value and i32 to indicate a 32-bit integer value.
Similarly, a64 is the same as long long, but a64 is used to indicate
values that will be placed in one of the four DSP accumulators ($ac0, $ac1, $ac2 or
$ac3).
Also, some built-in functions prefer or require immediate numbers as parameters, because the corresponding DSP instructions accept both immediate numbers and register operands, or accept immediate numbers only. The immediate parameters are listed as follows.
imm0_3: 0 to 3.
imm0_7: 0 to 7.
imm0_15: 0 to 15.
imm0_31: 0 to 31.
imm0_63: 0 to 63.
imm0_255: 0 to 255.
imm_n32_31: -32 to 31.
imm_n512_511: -512 to 511.The following built-in functions map directly to a particular DSP instruction. Please
refer to the PIC32 DSP documentation for details on what each instruction does. In the
table below, the function provides a way to generate the DSP instruction in your code.
For example, in v2q15 __builtin_mips_addq_ph (v2q15, v2q15), the
addq_ph is the actual DSP instruction.
v2q15 __builtin_mips_absq_s_ph (v2q15) |
q31 __builtin_mips_absq_s_w (q31) |
v2q15 __builtin_mips_addq_ph (v2q15, v2q15) |
v2q15 __builtin_mips_addq_s_ph (v2q15,
v2q15) |
q31 __builtin_mips_addq_s_w (q31, q31) |
i32 __builtin_mips_addsc (i32, i32) |
v4i8 __builtin_mips_addu_qb (v4i8, v4i8) |
v4i8 __builtin_mips_addu_s_qb (v4i8, v4i8) |
i32 __builtin_mips_addwc (i32, i32) |
i32 __builtin_mips_bitrev (i32) |
i32 __builtin_mips_bposge32 (void) |
void __builtin_mips_cmp_eq_ph (v2q15, v2q15) |
void __builtin_mips_cmp_le_ph (v2q15, v2q15) |
void __builtin_mips_cmp_lt_ph (v2q15, v2q15) |
i32 __builtin_mips_cmpgu_eq_qb (v4i8, v4i8) |
i32 __builtin_mips_cmpgu_le_qb (v4i8, v4i8) |
i32 __builtin_mips_cmpgu_lt_qb (v4i8, v4i8) |
void __builtin_mips_cmpu_eq_qb (v4i8, v4i8) |
void __builtin_mips_cmpu_le_qb (v4i8, v4i8) |
void __builtin_mips_cmpu_lt_qb (v4i8, v4i8) |
a64 __builtin_mips_dpaq_s_w_ph (a64, v2q15,
v2q15) |
a64 __builtin_mips_dpaq_sa_l_w (a64, q31,
q31) |
a64 __builtin_mips_dpau_h_qbl (a64, v4i8,
v4i8) |
a64 __builtin_mips_dpau_h_qbr (a64, v4i8,
v4i8) |
a64 __builtin_mips_dpsq_s_w_ph (a64, v2q15,
v2q15) |
a64 __builtin_mips_dpsq_sa_l_w (a64, q31,
q31) |
a64 __builtin_mips_dpsu_h_qbl (a64, v4i8,
v4i8) |
a64 __builtin_mips_dpsu_h_qbr (a64, v4i8,
v4i8) |
i32 __builtin_mips_extp (a64, i32) |
i32 __builtin_mips_extp (a64, imm0_31) |
i32 __builtin_mips_extpdp (a64, i32) |
i32 __builtin_mips_extpdp (a64, imm0_31) |
i32 __builtin_mips_extr_r_w (a64, i32) |
i32 __builtin_mips_extr_r_w (a64, imm0_31) |
i32 __builtin_mips_extr_rs_w (a64, i32) |
i32 __builtin_mips_extr_rs_w (a64, imm0_31) |
i32 __builtin_mips_extr_s_h (a64, i32) |
i32 __builtin_mips_extr_s_h (a64, imm0_31) |
i32 __builtin_mips_extr_w (a64, i32) |
i32 __builtin_mips_extr_w (a64, imm0_31) |
i32 __builtin_mips_insv (i32, i32) |
i32 __builtin_mips_lbux (void *, i32) |
i32 __builtin_mips_lhx (void *, i32) |
i32 __builtin_mips_lwx (void *, i32) |
a64 __builtin_mips_maq_s_w_phl (a64, v2q15,
v2q15) |
a64 __builtin_mips_maq_s_w_phr (a64, v2q15,
v2q15) |
a64 __builtin_mips_maq_sa_w_phl (a64, v2q15,
v2q15) |
a64 __builtin_mips_maq_sa_w_phr (a64, v2q15,
v2q15) |
i32 __builtin_mips_modsub (i32, i32) |
a64 __builtin_mips_mthlip (a64, i32) |
q31 __builtin_mips_muleq_s_w_phl (v2q15,
v2q15) |
q31 __builtin_mips_muleq_s_w_phr (v2q15,
v2q15) |
v2q15 __builtin_mips_muleu_s_ph_qbl (v4i8,
v2q15) |
v2q15 __builtin_mips_muleu_s_ph_qbr (v4i8,
v2q15) |
v2q15 __builtin_mips_mulq_rs_ph (v2q15,
v2q15) |
a64 __builtin_mips_mulsaq_s_w_ph (a64, v2q15,
v2q15) |
v2q15 __builtin_mips_packrl_ph (v2q15,
v2q15) |
v2q15 __builtin_mips_pick_ph (v2q15, v2q15) |
v4i8 __builtin_mips_pick_qb (v4i8, v4i8) |
q31 __builtin_mips_preceq_w_phl (v2q15) |
q31 __builtin_mips_preceq_w_phr (v2q15) |
v2q15 __builtin_mips_precequ_ph_qbl (v4i8) |
v2q15 __builtin_mips_precequ_ph_qbla (v4i8) |
v2q15 __builtin_mips_precequ_ph_qbr (v4i8) |
v2q15 __builtin_mips_precequ_ph_qbra (v4i8) |
v2q15 __builtin_mips_preceu_ph_qbl (v4i8) |
v2q15 __builtin_mips_preceu_ph_qbla (v4i8) |
v2q15 __builtin_mips_preceu_ph_qbr (v4i8) |
v2q15 __builtin_mips_preceu_ph_qbra (v4i8) |
v2q15 __builtin_mips_precrq_ph_w (q31, q31) |
v4i8 __builtin_mips_precrq_qb_ph (v2q15,
v2q15) |
v2q15 __builtin_mips_precrq_rs_ph_w (q31,
q31) |
v4i8 __builtin_mips_precrqu_s_qb_ph (v2q15,
v2q15) |
i32 __builtin_mips_raddu_w_qb (v4i8) |
i32 __builtin_mips_rddsp (imm0_63) |
v2q15 __builtin_mips_repl_ph (i32) |
v2q15 __builtin_mips_repl_ph (imm_n512_511) |
v4i8 __builtin_mips_repl_qb (i32) |
v4i8 __builtin_mips_repl_qb (imm0_255) |
a64 __builtin_mips_shilo (a64, i32) |
a64 __builtin_mips_shilo (a64, imm_n32_31) |
v2q15 __builtin_mips_shll_ph (v2q15, i32) |
v2q15 __builtin_mips_shll_ph (v2q15,
imm0_15) |
v4i8 __builtin_mips_shll_qb (v4i8, i32) |
v4i8 __builtin_mips_shll_qb (v4i8, imm0_7) |
v2q15 __builtin_mips_shll_s_ph (v2q15, i32) |
v2q15 __builtin_mips_shll_s_ph (v2q15,
imm0_15) |
q31 __builtin_mips_shll_s_w (q31, i32) |
q31 __builtin_mips_shll_s_w (q31, imm0_31) |
v2q15 __builtin_mips_shra_ph (v2q15, i32) |
v2q15 __builtin_mips_shra_ph (v2q15,
imm0_15) |
v2q15 __builtin_mips_shra_r_ph (v2q15, i32) |
v2q15 __builtin_mips_shra_r_ph (v2q15,
imm0_15) |
q31 __builtin_mips_shra_r_w (q31, i32) |
q31 __builtin_mips_shra_r_w (q31, imm0_31) |
v4i8 __builtin_mips_shrl_qb (v4i8, i32) |
v4i8 __builtin_mips_shrl_qb (v4i8, imm0_7) |
v2q15 __builtin_mips_subq_ph (v2q15, v2q15) |
v2q15 __builtin_mips_subq_s_ph (v2q15,
v2q15) |
q31 __builtin_mips_subq_s_w (q31, q31) |
v4i8 __builtin_mips_subu_qb (v4i8, v4i8) |
v4i8 __builtin_mips_subu_s_qb (v4i8, v4i8) |
void __builtin_mips_wrdsp (i32, imm0_63) |
The following built-in functions map directly to a particular MIPS DSP REV 2 instruction. Please refer to the PIC32 DSP documentation for details on what each instruction does.
v4q7 __builtin_mips_absq_s_qb (v4q7); |
v2q15 __builtin_mips_addqh_ph (v2q15,
v2q15); |
v2q15 __builtin_mips_addqh_r_ph (v2q15,
v2q15); |
q31 __builtin_mips_addqh_r_w (q31, q31); |
q31 __builtin_mips_addqh_w (q31, q31); |
v2i16 __builtin_mips_addu_ph (v2i16, v2i16); |
v2i16 __builtin_mips_addu_s_ph (v2i16,
v2i16); |
v4i8 __builtin_mips_adduh_qb (v4i8, v4i8); |
v4i8 __builtin_mips_adduh_r_qb (v4i8, v4i8); |
i32 __builtin_mips_append (i32, i32,
imm0_31); |
i32 __builtin_mips_balign (i32, i32,
imm0_3); |
i32 __builtin_mips_cmpgdu_eq_qb (v4i8,
v4i8); |
i32 __builtin_mips_cmpgdu_le_qb (v4i8,
v4i8); |
i32 __builtin_mips_cmpgdu_lt_qb (v4i8,
v4i8); |
a64 __builtin_mips_dpa_w_ph (a64, v2i16,
v2i16); |
a64 __builtin_mips_dpaqx_s_w_ph (a64, v2q15,
v2q15); |
a64 __builtin_mips_dpaqx_sa_w_ph (a64, v2q15,
v2q15); |
a64 __builtin_mips_dpax_w_ph (a64, v2i16,
v2i16); |
a64 __builtin_mips_dps_w_ph (a64, v2i16,
v2i16); |
a64 __builtin_mips_dpsqx_s_w_ph (a64, v2q15,
v2q15); |
a64 __builtin_mips_dpsqx_sa_w_ph (a64, v2q15,
v2q15); |
a64 __builtin_mips_dpsx_w_ph (a64, v2i16,
v2i16); |
a64 __builtin_mips_madd (a64, i32, i32); |
a64 __builtin_mips_maddu (a64, ui32, ui32); |
a64 __builtin_mips_msub (a64, i32, i32); |
a64 __builtin_mips_msubu (a64, ui32, ui32); |
v2i16 __builtin_mips_mul_ph (v2i16, v2i16); |
v2i16 __builtin_mips_mul_s_ph (v2i16,
v2i16); |
q31 __builtin_mips_mulq_rs_w (q31, q31); |
v2q15 __builtin_mips_mulq_s_ph (v2q15,
v2q15); |
q31 __builtin_mips_mulq_s_w (q31, q31); |
a64 __builtin_mips_mulsa_w_ph (a64, v2i16,
v2i16); |
a64 __builtin_mips_mult (i32, i32); |
a64 __builtin_mips_multu (ui32, ui32); |
v4i8 __builtin_mips_precr_qb_ph (v2i16,
v2i16); |
v2i16 __builtin_mips_precr_sra_ph_w (i32, i32,
imm0_31); |
v2i16 __builtin_mips_precr_sra_r_ph_w (i32, i32,
imm0_31); |
i32 __builtin_mips_prepend (i32, i32,
imm0_31); |
v4i8 __builtin_mips_shra_qb (v4i8, i32); |
v4i8 __builtin_mips_shra_qb (v4i8, imm0_7); |
v4i8 __builtin_mips_shra_r_qb (v4i8, i32); |
v4i8 __builtin_mips_shra_r_qb (v4i8,
imm0_7); |
v2i16 __builtin_mips_shrl_ph (v2i16, i32); |
v2i16 __builtin_mips_shrl_ph (v2i16,
imm0_15); |
v2q15 __builtin_mips_subqh_ph (v2q15,
v2q15); |
v2q15 __builtin_mips_subqh_r_ph (v2q15,
v2q15); |
q31 __builtin_mips_subqh_r_w (q31, q31); |
q31 __builtin_mips_subqh_w (q31, q31); |
v2i16 __builtin_mips_subu_ph (v2i16, v2i16); |
v2i16 __builtin_mips_subu_s_ph (v2i16,
v2i16); |
v4i8 __builtin_mips_subuh_qb (v4i8, v4i8); |
v4i8 __builtin_mips_subuh_r_qb (v4i8, v4i8); |