4.4.3 xc32-gcc (32-bit C Compiler)

A subset of command-line options may be specified in MPLAB X IDE. Select a category and set up compiler options.

See also Options Page Features.

Table 4-4. XC32-GCC General Category
OptionDescriptionCommand Line
Have symbols in production buildBuild for debugging in a production build image.-g
Enable App IOSupport the APPIN/APPOUT debugging feature with REAL ICE.-mappio-debug
Isolate each function in a sectionThis option is often used with the linker's --gc-sections option to remove unreferenced functions.

Check to place each function into its own section in the output file. The name of the function determines the section’s name in the output file.

Note: When you specify this option, the assembler and linker may create larger object and executable files and will also be slower.

Uncheck to place multiple functions in a section.

-ffunction-sections
Place data into its own sectionThis option is often used with the linker's --gc-sections option to remove unreferenced statically-allocated variables.

Place each data item into its own section in the output file.

The name of the data item determines the name of the section. When you specify this option, the assembler and linker may create larger object and executable files and will also be slower.

-fdata-sections
Enable toplevel reorderingAllows the compiler to reorder top-level functions, variables, and asm statements, in which case, they might not be output in the same order that they appear in the input file.-ftoplevel-reorder
Use indirect callsEnable full-range calls.-mlong-calls
Generate MIPS16 16-bit codeGenerate code for the MIPS16 instruction set, reducing code size.-[mno-]mips16
Generate microMIPS compressed codeGenerate code using the microMIPS instructions. This feature is available only in the PRO edition.-m[no-]micromips
Exclude floating-point libraryExclude support for floating-point operations reducing code size for applications that do not require floating-point support.-mno-float

Note that some of the compiler options specified by fields in Project Property Categories other than Optimization can affect the size and execution speed of your project. Consider using the Compiler Advisor, accessible via the MPLAB X IDE Tools > Analysis > Compiler Advisor menu item, to compare the size of your project when built with different combination of compiler options.

Table 4-5. XC32-GCC Optimization Category
OptionDescriptionCommand Line
Optimization LevelSelect an optimization level. Your compiler edition may support only some optimizations. Equivalent to -On option, where n is an option below:

0 - Do not optimize. The compiler’s goal is to reduce the cost of compilation and to make debugging produce the expected results.

1 - Optimize. Optimizing compilation takes somewhat longer and a lot more host memory for a large function. The compiler tries to reduce code size and execution time.

2 - Optimize even more. The compiler performs nearly all supported optimizations that do not involve a space-speed trade-off.

3 - Optimize yet more favoring speed (superset of O2).

s - Optimize yet more favoring size (superset of O2).

-O0 -O1 -O2 -O3 -Os
Unroll loopsThis option often increases execution speed at the expense of larger code size.

Check to perform the optimization of loop unrolling. This is only done for loops whose number of iterations can be determined at compile time or run time.

Uncheck to not unroll loops.

-funroll-loops
Omit frame pointerCheck to not keep the Frame Pointer in a register for functions that don’t need one.

Uncheck to keep the Frame Pointer.

-fomit-frame-pointer
Pre-optimization instruction schedulingDefault for optimization level:

- Disable

- Enable

-f[no-]schedule-insns
Post-optimization instruction schedulingDefault for optimization level:

- Disable

- Enable

-f[no-]schedule-insns2
Use common tentative definitionsControls the placement of global variables defined without an initializer.-f[no-]common
Table 4-6. XC32-GCC Preprocessing and Messages Category
OptionDescriptionCommand Line
Preprocessor macrosProject-specific preprocessor macro defines passed via the compiler's –D option.

-Dmacro=defn

Include directoriesSearch these directories for project-specific include files.

-I dir

Make warnings into errorsCheck to halt compilation based on warnings as well as errors.

Uncheck to halt compilation based on errors only.

-Werror
Additional warningsCheck to enable all warnings.

Uncheck to disable warnings.

-Wall
Enable address-attribute warning-Waddress-attribute-use
support-ansiCheck to issue all warnings demanded by strict ANSI C.

Uncheck to issue all warnings.

-ansi
strict-ansiIssue all the warnings demanded by strict ISO C and ISO C++; reject all programs that use forbidden extensions, and some other programs that do not follow ISO C and ISO C++.-pedantic
Use CCI syntaxEnable support for the CCI syntax (see Common C Interface).-mcci
Use IAR syntaxEnable support for syntax used by other toolchain vendors.-mext=IAR