3.3.1.4 How Can I Use A Variable Defined In Another Source File?
Provided the variable defined in the other source file is not
static (see Static Variables) or auto (see Auto Variable Allocation and Access), adding a declaration
for that variable into the current file will allow you to access it. A declaration consists
of the keyword extern in addition to the type and the name of the
variable, as specified in its definition, for example,
extern int systemStatus;
This is part of the C language. Your favorite C textbook will give you more information.
The position of the declaration in the current file determines the scope of the variable. That is, if you place the declaration inside a function, it will limit the scope of the variable to that function. If you place it outside of a function, it allows access to the variable in all functions for the remainder of the current file.
Often, declarations are placed in header files and then they are
#included into the C source code (see Preprocessor Directives).