5.4.1 Location and Naming Convention
By default, the compiler uses the directory <install-directory>/lib/gcc/ to store the specific libraries and the directory <install-directory>/pic32m/lib to store the target-specific libraries, based on the target device family.
- Size vs. speed
(
-Osvs.-O3) - MIPS16 vs. MIPS32 vs. microMIPS
ISA mode (
-mips16vs.-mno-mips16vs.-mmicromips) - Software floating-point vs no floating-point support
(
-msoft-floatvs.-mno-float)
The following examples provide details on which of the library subdirectories are searched.
If no optimization option has been specified or an optimization of level 2 or
lower has been specified, for example, xc32-gcc -O1 foo.c, then the
libraries in the top-level of the library subdirectories are used.
If -Os level optimizations have been chosen, for example,
xc32-g++ -Os foo.cpp, then the libraries in the
size directories of the library subdirectories are used.
If -Os level optimizations and the MIPS16 instruction set option have
both been chosen, for example, xc32-gcc -Os -mips16 foo.c, then the
libraries in the size/mips16 directories of the library
subdirectories are searched.