4.4.2 xc32-as (32-bit Assembler)
Select a category and set up assembler options. Note that the options specified are for the
assembler tool (xc32-as) and are not for the xc32-gcc
option. For additional options, see MPLAB® XC32 Assembler,
Linker And Utilities User’s Guide documentation. See also Options Page Features.
| Option | Description | Command Line |
|---|---|---|
| Have symbols in production build | Generate debugging information for source-level debugging in MPLAB X. |
|
| Keep local symbols | Check to keep local symbols, that is, labels beginning with Uncheck to discard local symbols. | --keep-localsSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Exclude floating-point library | Exclude support for floating-point operations reducing code size for applications that do not require floating-point support. | -mno-float |
| Generate MIPS16 16-bit code | Changes the assembler's default assembly mode so it will attempt to build for the MIPS16 ISA. You can still override this setting with the .set isa-mode directives. |
|
| Generate microMIPS compressed code | Changes the assembler's default assembly mode so it will attempt to build for the microMIPS ISA. You can still override this setting with the .set isa-mode directives. |
|
| Preprocessor macro definitions | Project-specific preprocessor macro defines passed via the compiler's –D option. |
|
| Assembler symbols | Define symbol sym to a given value. | --defsym sym=valueSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Preprocessor Include directories | Add a directory to the list of those searched for headers included by the preprocessor. Relative paths are from MPLAB X project directory. |
|
| Assembler Include directories | Add a directory to the list of those searched for files specified in You may add as many directories as necessary to include a variety of paths. The current working directory is always searched first and then | -IdirSee the MPLAB ®XC32 Assembler, Linker and Utilities User's Guide. |
| Option | Description | Command Line |
|---|---|---|
| Diagnostics level | Select warnings to display in the Output window. Select “Generate warnings” to have the usual warnings issued by the compiler; “Suppress warnings”to have only errors displayed, and "Fatal Warnings" to have the assembler treat warnings as if they were errors. |
See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Include source code | Check for a high-level language listing. High-level listings require that the assembly source code is generated by a compiler, a debugging option like -g is given to the compiler, and assembly listings (-al) are requested.Uncheck for a regular listing. | -ah See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Expand macros | Check to expand macros in a listing. Uncheck to collapse macros. | -am See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Include false conditionals | Check to include false conditionals (.if, .ifdef) in a listing.Uncheck to omit false conditionals. | -acSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Omit forms processing | Check to turn off all forms processing that would be performed by the listing directives .psize, .eject, .title and .sbttl.Uncheck to process by listing directives. | -anSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Include assembly | Check for an assembly listing. This Uncheck to exclude an assembly listing. | -alSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| List symbols | Check for a symbol table listing. Uncheck to exclude the symbol table from the listing. | -asSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| Omit debugging directives | Check to omit debugging directives from a listing. This can make the listing cleaner. Uncheck to included debugging directives. | -adSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |
| List to file | Use this option if you want the assembly listing for any assembly source files in the project. They will have the same basename as the source, with a | -a=file.lstSee the MPLAB® XC32 Assembler, Linker and Utilities User's Guide |