4.1.2 XC32 Assembler Options

The following assembler feature controls are displayed in the MPLAB X IDE and VS Code project property dialogs, along with their corresponding driver options. When used, these options are passed to the assembler application xc32-as and are not relevant for the xc32-gcc driver. For additional assembler options, see the MPLAB® XC32 Assembler, Linker And Utilities User’s Guide.

Table 4-2. XC32 Assembler General Options Category
OptionDescriptionCommand Line
Have symbols in production buildGenerate debugging information for source-level debugging in MPLAB X.

--gdwarf-2 See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Keep local symbols

Check to keep local symbols, that is, labels beginning with .L (upper case only).

Uncheck to discard local symbols.

--keep-locals

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Exclude floating-point libraryExclude support for floating-point operations reducing code size for applications that do not require floating-point support.-mno-float
Generate MIPS16 16-bit code (X IDE only)Changes the assembler's default assembly mode so it will attempt to build for the MIPS16 ISA. You can still override this setting with the .set isa-mode directives.

-mips16 See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Generate microMIPS compressed code (X IDE only)Changes the assembler's default assembly mode so it will attempt to build for the microMIPS ISA. You can still override this setting with the .set isa-mode directives.

-mmicromips See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Preprocessor macro definitionsProject-specific preprocessor macro defines passed via the compiler's –D option.

-Dmacro[=defn] See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Assembler symbolsDefine symbol sym to a given value.--defsym sym=value

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Preprocessor Include directoriesAdd a directory to the list of those searched for headers included by the preprocessor. Relative paths are from MPLAB X project directory.

-I dir See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Assembler Include directories

Add a directory to the list of those searched for files specified in .include directives. Relative paths are from MPLAB X project directory.

You may add as many directories as necessary to include a variety of paths. The current working directory is always searched first and then -I directories in the order in which they were specified (left to right) here.

-Idir

See the MPLAB ®XC32 Assembler, Linker and Utilities User's Guide.

Additional Options (VS Code only)Add options which do not have a dedicated control widget present in the properties dialog.

Table 4-3. XC32 Assembler Other Options Category
OptionDescriptionCommand Line
Diagnostics level

Select warnings to display in the Output window. Select “Generate warnings” to have the usual warnings issued by the compiler; “Suppress warnings”to have only errors displayed, and "Fatal Warnings" to have the assembler treat warnings as if they were errors.

--[no-]warn

--fatal-warnings

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Include source codeCheck for a high-level language listing. High-level listings require that the assembly source code is generated by a compiler, a debugging option like -g is given to the compiler, and assembly listings (-al) are requested.

Uncheck for a regular listing.

-ah See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide
Expand macrosCheck to expand macros in a listing.

Uncheck to collapse macros.

-am See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide
Include false conditionalsCheck to include false conditionals (.if, .ifdef) in a listing.

Uncheck to omit false conditionals.

-ac

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Omit forms processingCheck to turn off all forms processing that would be performed by the listing directives .psize, .eject, .title and .sbttl.

Uncheck to process by listing directives.

-an

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Include assembly

Check for an assembly listing. This -a suboption may be used with other suboptions.

Uncheck to exclude an assembly listing.

-al

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

List symbolsCheck for a symbol table listing.

Uncheck to exclude the symbol table from the listing.

-as

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Omit debugging directivesCheck to omit debugging directives from a listing. This can make the listing cleaner.

Uncheck to included debugging directives.

-ad

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

List to fileUse this option if you want the assembly listing for any assembly source files in the project.

They will have the same basename as the source, with a .lst extension.

-a=file.lst

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide