1.3 Fuse Configurations
- The Bootloader project has the Fuse
settings set to default except below Fuse bits:
- Bootloader region size is
specified using BOOTPROT Fuse bit. BOOTPROT (BS) -
8192Bytes (for PIC32CM SG00).
- Bootloader region size is
specified using BOOTPROT Fuse bit. BOOTPROT (BS) -
- The Fuse settings can be changed in following ways:
- The Bootloader provides a separate command to program the Fuse Bits received from the Host. Refer to the Bootloader protocol documentation and respective Host utility documentation for additional information.
- The application can check the Fuse bits during the boot-up, and then program any change required using the NVMCTRL peripheral.
- The Fuse settings are placed in a higher memory location in the Flash. The Fuse settings need to be disabled for the application project, which will be boot-loaded, as the size of the binary file becomes too large when the Fuse settings are enabled.
- When updating the Bootloader itself, make sure that the Fuse settings for the Bootloader application are disabled.
For PIC32CM SG00:
- Proper Fuse settings required by the application have to be sent along with application binary.
- Peripherals used by the Bootloader (SERCOM0, SERCOM1, BOOT Pin) should not be configured as Non-Secure while updating the Fuse settings.
- When WDT is enabled from the Fuse settings, the Bootloader refreshes the WDT at intervals to avoid reset. Therefore, the WDT peripheral should not be configured as Non-Secure if it is enabled through Fuse settings.