1.1 Conventions Used in This Guide
The following conventions may appear in this documentation. In most cases, formatting conforms to the OASIS Darwin Information Typing Architecture (DITA) Version 1.3 Part 3: All-Inclusive Edition, 19 June 2018.
| Description | Implementation | Examples | 
|---|---|---|
| References | DITA: cite | MPLAB® XC8 PIC® Assembler User's Guide. | 
| Emphasized text | Italics | ...is the only compiler... | 
| A window, window pane or dialog name. | DITA: wintitle | the
                                Output window. the New Watch dialog.  | 
| A field name in a window or dialog. | DITA: uicontrol | Select the Optimizations option category. | 
| A menu name or item. | DITA: uicontrol | Select the File menu and then Save. | 
| A menu path. | DITA: menucascade, uicontrol | |
| A tab | DITA: uicontrol | Click the Power tab. | 
| A software button. | DITA: uicontrol | Click the OK button. | 
| A key on the keyboard. | DITA: uicontrol | Press the F1 key. | 
| File names and paths. | DITA: filepath | C:\Users\User1\Projects | 
| Source code: inline. | DITA: codeph | Remember to
                                #define START at the beginning of your
                            code. | 
| Source code: block. | DITA: codeblock | An example
                            is: | 
| User-entered data. | DITA: userinput | Type in a device name, for example PIC18F47Q10. | 
| Keywords | DITA: codeph | static, auto,
                                extern | 
| Command-line options. | DITA: codeph | -Opa+, -Opa- | 
| Bit values | DITA: codeph | 0,
                                1 | 
| Constants | DITA: codeph | 0xFF,
                                'A' | 
| A variable argument. | DITA: codeph + option | file.o, where
                                    file can be any valid file
                            name. | 
| Optional arguments | Square brackets [ ] | xc8
                                    [options]
                            files | 
| Choice of mutually exclusive arguments; an OR selection. | Curly brackets and pipe character: { | } | errorlevel {0|1} | 
| Replaces repeated text. | Ellipses... | var_name [,
                                var_name...] | 
| Represents code supplied by user. | Ellipses... | void
                                main (void)
 
  | 
| A number in verilog format, where N is the total number of digits, R is the radix and n is a digit. | N‘Rnnnn | 4‘b0010, 2‘hF1 | 
| Device Dependent insignia. Specifies that a feature is not supported on all devices. Devices supported will be listed in the title or text. | [DD] | xmemory
                            attribute |