8.1 Messages 0 Thru 499
(1) too many errors (*) (all applications)
The executing compiler application has encountered too many errors and will exit
immediately. Other uncompiled source files will be processed, but the compiler
applications that would normally be executed in due course will not be run. The
number of errors that can be accepted is controlled using the
-fmax-errors option.
(2) error/warning (*) generated but no description available (all applications)
The executing compiler application has emitted a message (advisory/warning/error), but there is no description available in the message description file (MDF) to print. This could be because the MDF is out-of-date, or the message issue has not been translated into the selected language.
(3) malformed error information on line * in file * (all applications)
The compiler has attempted to load the messages for the selected language, but the message description file (MDF) was corrupted and could not be read correctly.
(100) unterminated #if[n][def] block from line * (Preprocessor)
#if or similar block was not terminated with a
matching #endif, for example:
#if INPUT /* error flagged here */
int main(void)
{
run();
} /* no #endif was found in this module */
(101) #* cannot follow #else (Preprocessor)
#else or #elif has been used in the
same conditional block as a #else. These can only follow a
#if, for example:
#ifdef FOO
result = foo;
#else
result = bar;
#elif defined(NEXT) /* the #else above terminated the #if */
result = next(0);
#endif
(102) #* must be in an #if (Preprocessor)
#elif, #else or
#endif directive must be preceded by a matching
#if line. If there is an apparently corresponding
#if line, check for things like extra #endifs,
or improperly terminated comments, for example:
#ifdef FOO
result = foo;
#endif
result = bar;
#elif defined(NEXT) /* the #endif above terminated the #if */
result = next(0);
#endif
(103) #error: * (Preprocessor)
This is a programmer generated error; there is a directive causing a deliberate error. This is normally used to check compile time defines, etc. Remove the directive to remove the error, but first determine why the directive is there.
(104) preprocessor #assert failure (Preprocessor)
#assert directive has
evaluated to zero. This is a programmer induced error.
#assert SIZE == 4 /* size should never be 4 */
(105) no #asm before #endasm (Preprocessor)
#endasm operator has been encountered, but there was
no previous matching #asm, for example:
void cleardog(void)
{
clrwdt
#endasm /* in-line assembler ends here, only where did it begin? */
}
(106) nested #asm directives (Preprocessor)
#asm directives. Check for a
missing or misspelled #endasm directive, for example:
#asm
MOVE r0, #0aah
#asm ; previous #asm must be closed before opening another
SLEEP
#endasm
(107) illegal # directive “*” (Preprocessor, Parser)
# directive. It is
probably a misspelling of a directive token, for example:
#indef DEBUG /* oops -- that should be #undef DEBUG */
(108) #if[n][def] without an argument (Preprocessor)
#if,
#ifdef, and #ifndef must have an argument. The
argument to #if should be an expression, while the argument to
#ifdef or #ifndef should be a single name, for
example:
#if /* oops -- no argument to check */
output = 10;
#else
output = 20;
#endif
(109) #include syntax error (Preprocessor)
#include is
invalid. The argument to #include must be a valid file name, either
enclosed in double quotes " " or angle brackets <
>. Spaces should not be included and the closing quote or bracket
must be present. There should be nothing else on the line other than comments, for
example:
#include stdio.h /* oops -- should be: #include <stdio.h> */
(110) too many file arguments; usage: cpp [input [output]] (Preprocessor)
CPP should be invoked with at most two file arguments. Contact Microchip Technical Support if the preprocessor is being executed by a compiler driver.
(111) redefining preprocessor macro “*” (Preprocessor)
#define ONE 1
/* elsewhere: */
/* Is this correct? It will overwrite the first definition. */
#define ONE one
(112) #define syntax error (Preprocessor)
#define FOO(a, 2b) bar(a, 2b) /* 2b is not to be! */
(113) unterminated string in preprocessor macro body (Preprocessor, Assembler)
A macro definition contains a string that lacks a closing quote.
(114) illegal #undef argument (Preprocessor)
#undef must be a valid name. It must
start with a letter, for example:
#undef 6YYY /* this isn’t a valid symbol name */
(115) recursive preprocessor macro definition of “*” defined by “*” (Preprocessor)
The named macro has been defined in such a manner that expanding it causes a recursive expansion of itself.
(116) end of file within preprocessor macro argument from line * (Preprocessor)
#define FUNC(a, b) func(a+b)
FUNC(5, 6; /* oops -- where is the closing bracket? */
(117) misplaced constant in #if (Preprocessor)
#if expression should only occur in
syntactically correct places. This error is probably caused by omission of an
operator, for example:
#if FOO BAR /* oops -- did you mean: #if FOO == BAR ? */
(118) stack overflow processing #if expression (Preprocessor)
The preprocessor filled up its expression evaluation stack in a
#if expression. Simplify the expression – it probably contains
too many parenthesized subexpressions.
(119) invalid expression in #if line (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(120) operator “*” in incorrect context (Preprocessor)
#if expression
that is incorrectly placed (two binary operators are not separated by a value), for
example:
#if FOO * % BAR == 4 /* what is "* %" ? */
#define BIG
#endif
(121) expression stack overflow at operator “*” (Preprocessor)
Expressions in #if lines are evaluated using a stack
with a size of 128. It is possible for very complex expressions to overflow this.
Simplify the expression.
(122) unbalanced parenthesis at operator “*” (Preprocessor)
#if expression found mismatched
parentheses. Check the expression for correct parenthesizing, for example:
#if ((A) + (B) /* oops -- a missing ), I think */
#define ADDED
#endif
(123) misplaced “?” or “:”; previous operator is “*” (Preprocessor)
#if
expression that does not match up with a corresponding ? operator,
for example:
#if XXX : YYY /* did you mean: #if COND ? XXX : YYY */
(124) illegal character “*” in #if (Preprocessor)
#if expression that should
not be there. Valid characters are the letters, digits and those comprising the
acceptable operators, for example:
#if YYY /* what are these characters doing here? */
int m;
#endif
(125) illegal character (* decimal) in #if (Preprocessor)
#if expression
that should not be there. Valid characters are the letters, digits and those
comprising the acceptable operators, for example:
#if ^S YYY /* what is this control characters doing here? */
int m;
#endif
(126) strings can’t be used in #if (Preprocessor)
#if expressions, for example:
/* no string operations allowed by the preprocessor */
#if MESSAGE > "hello"
#define DEBUG
#endif
(127) bad syntax for defined() in #[el]if (Preprocessor)
defined() pseudo-function in a preprocessor
expression requires its argument to be a single name. The name must start with a
letter and should be enclosed in parentheses, for example:
/* oops -- defined expects a name, not an expression */
#if defined(a&b)
input = read();
#endif
(128) illegal operator in #if (Preprocessor)
#if expression has an illegal operator. Check for
correct syntax, for example:
#if FOO = 6 /* oops -- should that be: #if FOO == 5 ? */
(129) unexpected “\” in #if (Preprocessor)
#if statement, for
example: #if FOO == \34
#define BIG
#endif
(130) unknown type “*” in #[el]if sizeof() (Preprocessor)
sizeof(). The
preprocessor can only evaluate sizeof() with basic types, or
pointers to basic types, for example:
#if sizeof(unt) == 2 /* should be: #if sizeof(int) == 2 */
i = 0xFFFF;
#endif
(131) illegal type combination in #[el]if sizeof() (Preprocessor)
sizeof() in a #if expression, for example:
/* To sign, or not to sign, that is the error. */
#if sizeof(signed unsigned int) == 2
i = 0xFFFF;
#endif
(132) no type specified in #[el]if sizeof() (Preprocessor)
sizeof() was used in a preprocessor
#if expression, but no type was specified. The argument to
sizeof() in a preprocessor expression must be a valid simple
type, or pointer to a simple type, for example:
#if sizeof() /* oops -- size of what? */
i = 0;
#endif
(133) unknown type code (0x*) in #[el]if sizeof() (Preprocessor)
The preprocessor has made an internal error in evaluating a
sizeof() expression. Check for a malformed type specifier. This
is an internal error. Contact Microchip Technical Support with details.
(134) syntax error in #[el]if sizeof() (Preprocessor)
sizeof() in a #if expression. Probable causes
are mismatched parentheses and similar things, for example:
#if sizeof(int == 2) // oops - should be: #if sizeof(int) == 2
i = 0xFFFF;
#endif
(135) unknown operator (*) in #if (Preprocessor)
The preprocessor has tried to evaluate an expression with an operator it does not understand. This is an internal error. Contact Microchip Technical Support with details.
(137) strange character “*” after ## (Preprocessor)
## that is neither a letter nor a digit. Because the result of
this operator must be a legal token, the operands must be tokens containing only
letters and digits, for example:
/* the ’ character will not lead to a valid token */
#define cc(a, b) a ## ’b
(138) strange character (*) after ## (Preprocessor)
## that is neither a letter nor a digit. Because the
result of this operator must be a legal token, the operands must be tokens
containing only letters and digits, for example:
/* the ’ character will not lead to a valid token */
#define cc(a, b) a ## ’b
(139) end of file in comment (Preprocessor)
/* Here the comment begins. I’m not sure where I end, though
}
(140) can’t open * file “*”: * (Driver, Preprocessor, Code Generator, Assembler)
xc8 @commundsshould that be:
xc8 @commands
(141) can’t open * file “*”: * (Any)
An output file could not be created. Confirm the spelling and path of the file specified on the command line.
(144) too many nested #if blocks (Preprocessor)
#if, #ifdef, etc., blocks can only be
nested to a maximum of 32.
(146) #include filename too long (Preprocessor)
A filename constructed while looking for an include file has exceeded the length of an internal buffer. Because this buffer is 4096 bytes long, this is unlikely to happen.
(147) too many #include directories specified (Preprocessor)
A maximum of 7 directories can be specified for the preprocessor to search for include files. The number of directories specified with the driver is too many.
(148) too many arguments for preprocessor macro (Preprocessor)
A macro can only have up to 31 parameters, per the C Standard.
(149) preprocessor macro work area overflow (Preprocessor)
The total length of a macro expansion has exceeded the size of an internal table. This table is normally 32768 bytes long. Thus any macro expansion must not expand to a total of more than 32K bytes.
(150) illegal “__” preprocessor macro “*” (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(151) too many arguments in preprocessor macro expansion (Preprocessor)
There were too many arguments supplied in a macro invocation. The maximum number allowed is 31.
(152) bad dp/nargs in openpar(): c = * (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(153) out of space in preprocessor macro * argument expansion (Preprocessor)
A macro argument has exceeded the length of an internal buffer. This buffer is normally 4096 bytes long.
(155) work buffer overflow concatenating “*” (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(156) work buffer “*” overflow (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(157) can’t allocate * bytes of memory (Code Generator, Assembler)
This is an internal compiler error. Contact Microchip Technical Support with details.
(158) invalid disable in preprocessor macro “*” (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(159) too many calls to unget() (Preprocessor)
This is an internal compiler error. Contact Microchip Technical Support with details.
(161) control line “*” within preprocessor macro expansion (Preprocessor)
A preprocessor control line (one starting with a #) has
been encountered while expanding a macro. This should not happen.
(162) #warning: * (Preprocessor, Driver)
This warning is either the result of user-defined
#warning preprocessor directive, or the driver encountered a
problem reading the map file. If the latter, contact Microchip Technical Support
with details
(163) unexpected text in control line ignored (Preprocessor)
#if defined(END)
#define NEXT
#endif END /* END would be better in a comment here */
(164) #include filename “*” was converted to lower case (Preprocessor)
#include file name had to be converted to lowercase
before it could be opened, for example:
#include <STDIO.H> /* oops -- should be: #include <stdio.h> */(165) #include filename “*” does not match actual name (check upper/lower case) (Preprocessor)
In Windows versions this means the file to be included actually exists
and is spelled the same way as the #include filename; however, the
case of each does not exactly match. For example, specifying #include
“code.c” will include Code.c, if it is found. In
Linux versions this warning could occur if the file wasn’t found.
(166) too few values specified with option “*” (Preprocessor)
The list of values to the preprocessor (CPP) -S option
is incomplete. This should not happen if the preprocessor is being invoked by the
compiler driver. The values passed to this option represent the sizes of
char, short, int,
long, float and double
types.
(167) too many values specified with -S option; “*” unused Preprocessor)
There were too many values supplied to the -S
preprocessor option. See message 166.
(168) unknown option “*” (Any)
The option given to the component which caused the error is not recognized.
(169) strange character (*) after ## (Preprocessor)
There is an unexpected character after #.
(170) symbol “*” in undef was never defined (Preprocessor)
#undef was not
already defined. This warning can be disabled with some compilers. This warning can
be avoided with code like:
#ifdef SYM
#undef SYM /* only undefine if defined */
#endif
(171) wrong number of preprocessor macro arguments for “*” (* instead of *) (Preprocessor)
#define ADD(a, b) (a+b)
ADD(1, 2, 3) /* oops -- only two arguments required */
(172) formal parameter expected after # (Preprocessor)
# (not to be confused with
the leading # used for preprocessor control lines) must be followed
by a formal macro parameter, for example:
#define str(x) #y /* oops -- did you mean x instead of y? */If you need to stringize a token, you will need to define a special macro to do it, for example:
#define __mkstr__(x) #x
then use __mkstr__(token) wherever you need
to convert token into a string.
(173) undefined symbol “*” in #if; 0 used (Preprocessor)
#if expression was not a defined
preprocessor macro. For the purposes of this expression, its value has been taken as
zero. This warning can be disabled with some compilers. Example:
#if FOO+BAR /* e.g. FOO was never #defined */
#define GOOD
#endif
(174) multi-byte constant “*” isn’t portable (Preprocessor)
#if CHAR == ’ab’
#define MULTI
#endif
(175) division by zero in #if; zero result assumed (Preprocessor)
#if expression, there is a division by zero
which has been treated as yielding zero, for example:
#if foo/0 /* divide by 0: was this what you were intending? */
int a;
#endif
(176) missing newline (Preprocessor)
A new line is missing at the end of the line. Each line, including the last line, must have a new line at the end. This problem is normally introduced by editors.
(177) symbol “*” in -U option was never defined (Preprocessor)
A macro name specified in a -U option to the
preprocessor was not initially defined, and thus cannot be undefined.
(179) nested comments (Preprocessor)
output = 0; /* a comment that was left unterminated
flag = TRUE; /* next comment:
hey, where did this line go? */
(180) unterminated comment in included file (Preprocessor)
Comments begun inside an included file must end inside the included file.
(181) non-scalar types can’t be converted to other types (Parser)
struct TEST test;
struct TEST * sp;
sp = test; /* oops -- did you mean: sp = &test; ? */
(182) illegal conversion between types (Parser)
struct LAYOUT layout;
int i;
layout = i; /* int cannot be converted to struct */Note that even if a structure only contains an int
, for example, it cannot be assigned to an int variable and vice
versa.
(183) function or function pointer required (Parser)
int a, b, c, d;
a = b(c+d); /* b is not a function -- did you mean a = b*(c+d) ? */
(184) calling an interrupt function is illegal (Parser)
A function-qualified interrupt cannot be called from other functions. It can only be called by a hardware (or software) interrupt. This is because an interrupt function has special function entry and exit code that is appropriate only for calling from an interrupt. An interrupt function can call other non-interrupt functions.
(185) function does not take arguments (Parser, Code Generator)
int get_value(void);
int main(void)
{
int input;
input = get_value(6); /* oops --
parameter should not be here */
}
(186) too many function arguments (Parser)
void add(int a, int b);
add(5, 7, input); /* call has too many arguments */
(187) too few function arguments (Parser)
void add(int a, int b);
add(5); /* this call needs more arguments */
(188) constant expression required (Parser)
int a;
switch(input) {
case a: /* oops!
cannot use variable as part of a case label */
input++;
}
(189) illegal type for array dimension (Parser)
int array[12.5]; /* oops -- twelve and a half elements, eh? */
(190) illegal type for index expression (Parser)
int i, array[10];
i = array[3.5]; /* oops --
exactly which element do you mean? */
(191) cast type must be scalar or void (Parser)
void, for example:
lip = (long [])input; /* oops -- possibly: lip = (long *)input */
(192) undefined identifier “*” (Parser)
This symbol has been used in the program, but has not been defined or declared. Check for spelling errors if you think it has been defined.
(193) not a variable identifier “*” (Parser)
This identifier is not a variable; it can be some other kind of object, i.e., a label.
(194) “)” expected (Parser)
if(a == b /* the closing parenthesis is missing here */
b = 0; /* the error is flagged here */
(195) expression syntax (Parser)
a /=% b; /* oops -- possibly that should be: a /= b; */
(196) struct/union required (Parser)
.” , for example:
int a;
a.b = 9; /* oops -- a is not a structure */
(197) struct/union member expected (Parser)
A structure or union member name must follow a dot “.”
or an arrow (“->”).
(198) undefined struct/union “*” (Parser)
struct WHAT what; /* a definition for WHAT was never seen */
(199) logical type required (Parser)
if,
while statements or to boolean operators like
! and && must be a scalar integral
type, for example:
struct FORMAT format;
if(format) /* this operand must be a scaler type */
format.a = 0;
(200) taking the address of a register variable is illegal (Parser)
& operator, for example:
int * proc(register int in)
{
int * ip = ∈
/* oops -- in cannot have an address to take */
return ip;
}
(201) taking the address of this object is illegal (Parser)
&
operator is not one that denotes memory storage (“an lvalue”) and therefore its
address cannot be defined, for example:
ip = &8; /* oops -- you cannot take the address of a literal */
(202) only lvalues can be assigned to or modified (Parser)
int array[10];
int * ip;
char c;
array = ip; /* array is not a variable, it cannot be written to */A typecast does not yield an lvalue, for example:
/* the contents of c cast to int is only a intermediate value */
(int)c = 1;
However, you can write this using pointers:
*(int *)&c = 1
(203) illegal operation on bit variable (Parser)
bit b;
int * ip;
ip = &b; /* oops -- cannot take the address of a bit object */
(204) void function can’t return a value (Parser)
void run(void)
{
step();
return 1; /* either run should not be void, or remove the 1 */
}
(205) integral type required (Parser)
This operator requires operands that are of integral type only.
(206) illegal use of void expression (Parser)
A void expression has no value and therefore you cannot
use it anywhere an expression with a value is required, i.e., as an operand to an
arithmetic operator.
(207) simple type required for “*” (Parser)
A simple type (i.e., not an array or structure) is required as an operand to this operator.
(208) operands of “*” not same type (Parser)
int * ip;
char * cp, * cp2;
cp = flag ? ip : cp2; /* result of ? : will be int * or char * */Possibly, you meant something like:
cp = flag ? (char *)ip : cp2;
(209) type conflict (Parser)
The operands of this operator are of incompatible types.
(210) bad size list (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(211) taking sizeof bit is illegal (Parser)
It is illegal to use the sizeof() operator with the C
__bit type. When used against a type, the
sizeof() operator gives the number of bytes required to store
an object that type. Therefore its usage with the __bit type make
no sense and it is an illegal operation.
(212) missing number after pragma “pack” (Parser)
pragma pack requires a decimal number as argument.
This specifies the alignment of each member within the structure. Use this with
caution as some processors enforce alignment and will not operate correctly if word
fetches are made on odd boundaries, for example:
#pragma pack /* what is the alignment value */Possibly, you meant something like:
#pragma pack 2
(214) missing number after pragma “interrupt_level” (Parser)
The pragma interrupt_level requires an argument to
indicate the interrupt level. It will be the value 1 for mid-range devices, or 1 or
2 or PIC18 devices.
(215) missing argument to pragma “switch” (Parser)
pragma switch requires an argument of auto, direct
or simple, for example:
#pragma switch /* oops -- this requires a switch mode */Possibly, you meant something like:
#pragma switch simple
(216) missing argument to pragma “psect” (Parser)
pragma psect requires an argument of the form
oldname = newname where
oldname is an existing psect name known to the
compiler and newname is the desired new name, for example:
#pragma psect /* oops -- this requires an psect to redirect */Possibly, you meant something like:
#pragma psect text=specialtext
(218) missing name after pragma “inline” (Parser)
inline pragma expects the name of a function to
follow. The function name must be recognized by the code generator for it to be
expanded; other functions are not altered, for example:
#pragma inline /* what is the function name? */Possibly, you meant something like:
#pragma inline memcpy
(219) missing name after pragma “printf_check” (Parser)
printf_check pragma expects the name of a function
to follow. This specifies printf-style format string checking for the function, for
example:
#pragma printf_check /* what function is to be checked? */Possibly, you meant something like:
#pragma printf_check sprintf
Pragmas for all the standard printf-like function are already
contained in <stdio.h>.
(220) exponent expected (Parser)
e or E, for example:
float f;
f = 1.234e; /* oops -- what is the exponent? */
(221) hexadecimal digit expected (Parser)
0x should follow at least one of the HEX digits
0-9 and A-F or a-f, for example:
a = 0xg6; /* oops -- was that meant to be a = 0xf6 ? */
(222) binary digit expected (Parser)
0b format
specifier, for example:
i = 0bf000; /* oops -- f000 is not a base two value */
(223) digit out of range (Parser, Assembler)
0X or 0x. For example:
int a = 058; /* leading 0 implies octal which has digits 0 - 7 */
(224) illegal “#” directive (Parser)
An illegal # preprocessor has been detected. Likely, a
directive has been misspelled in your code somewhere.
(225) missing character in character constant (Parser)
char c = "; /* the character value of what? */
(226) char const too long (Parser)
c = ’12’; /* oops -- only one character can be specified */
(227) “.” expected after “..” (Parser)
The only context in which two successive dots can appear is as part of the ellipsis symbol, which must have 3 dots (an ellipsis is used in function prototypes to indicate a variable number of parameters).
Either .. was meant to be an ellipsis symbol which would require you to add an extra dot, or it was meant to be a structure member operator which would require you to remove one dot.
(228) illegal character (*) (Parser)
c = a; /* oops -- did you mean c = ’a’; ? */
(229) unknown qualifier “*” given to -A (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(230) missing argument to -A (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(231) unknown qualifier “*” given to -I (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(232) missing argument to -I (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(233) bad -Q option “*” (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(234) close error (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(236) simple integer expression required (Parser)
__at() operator, used to associate an absolute address with a
variable, for example:
int address;
char LOCK __at(address);
(237) function “*” redefined (Parser)
int twice(int a)
{
return a*2;
}
/* only one prototype & definition of rv can exist */
long twice(long a)
{
return a*2;
}
(238) illegal initialization (Parser)
typedef declaration, because it
does not reserve any storage that can be initialized, for example:
/* oops -- uint is a type, not a variable */
typedef unsigned int uint = 99;
(239) identifier “*” redefined (from line *) (Parser)
int a; /* a filescope variable called "a" */
int a; /* attempting to define another of the same name */Note that variables with the same name, but defined with different scopes, are legal; but; not recommended.
(240) too many initializers (Parser)
/* three elements, but four initializers */
int ivals[3] = { 2, 4, 6, 8};
(241) initialization syntax (Parser)
int iarray[10] = {{’a’, ’b’, ’c’};
/* oops -- one two many {s */
(242) illegal type for switch expression (Parser)
switch() operator must have an expression that is
either an integral type or an enumerated value, e.g:
double d;
switch(d) { /* oops -- this must be integral */
case ’1.0’:
d = 0;
}
(243) inappropriate break/continue (Parser)
break or continue statement has been
found that is not enclosed in an appropriate control structure. A continue can only
be used inside a while, for, or do
while loop, while break can only be used inside those
loops or a switch statement, for example:
switch(input) {
case 0:
if(output == 0)
input = 0xff;
} /* oops! this should not be here; it closed the switch */
break; /* this should be inside the switch */
(244) “default” case redefined (Parser)
default label is allowed to be in a
switch() statement. You have more than one, for example:
switch(a) {
default: /* if this is the default case... */
b = 9;
break;
default: /* then what is this? */
b = 10;
break;
(245) “default” case not in switch (Parser)
A label has been encountered called default, but it is
not enclosed by a switch statement. A default label is only legal
inside the body of a switch statement.
If there is a switch statement before this default
label, there could be one too many closing braces in the switch
code. That would prematurely terminate the switch statement. See
message 246.
(246) case label not in switch (Parser)
A case label has been encountered, but there is no
enclosing switch statement. A case label can only
appear inside the body of a switch statement.
If there is a switch statement before this
case label, there might be one too many closing braces in the
switch code. That would prematurely terminate the switch
statement, for example:
switch(input) {
case ’0’:
count++;
break;
case ’1’:
if(count>MAX)
count= 0;
} /* oops -- this shouldn’t be here */
break;
case ’2’: /* error flagged here */
(247) duplicate label “*” (Parser)
start:
if(a > 256)
goto end;
start: /* error flagged here */
if(a == 0)
goto start; /* which start label do I jump to? */
(248) inappropriate “else” (Parser)
else keyword has been encountered that cannot be
associated with an if statement. This can mean there is a missing
brace or other syntactic error, for example:
/* here is a comment which I have forgotten to close...
if(a > b) {
c = 0;
/* ... that will be closed here, thus removing the "if" */
else /* my "if" has been lost */
c = 0xff;
(249) probable missing “}” in previous block (Parser)
void set(char a)
{
PORTA = a;
/* the closing brace was left out here */
void clear(void) /* error flagged here */
{
PORTA = 0;
}
(251) array dimension redeclared (Parser)
extern int array[5];
int array[10]; /* oops -- has it 5 or 10 elements? */
(252) argument * conflicts with prototype (Parser)
/* this is supposedly calc’s prototype */
extern int calc(int, int);
int calc(int a, long int b) /* hmmm -- which is right? */
{ /* error flagged here */
return sin(b/a);
}
(253) argument list conflicts with prototype (Parser)
extern int calc(int); /* this is supposedly calc’s prototype */
int calc(int a, int b) /* hmmm -- which is right? */
{ /* error flagged here */
return a + b;
}
(254) undefined *: “*” (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(255) not a member of the struct/union “*” (Parser)
struct {
int a, b, c;
} data;
if(data.d) /* oops -- there is no member d in this structure */
return;
(256) too much indirection (Parser)
A pointer declaration can only have 16 levels of indirection.
(257) only “register” storage class allowed (Parser)
register, for example:
void process(static int input)
(258) duplicate qualifier (Parser)
typedef. Remove the redundant qualifier. For example:
typedef volatile int vint;
/* oops -- this results in two volatile qualifiers */
volatile vint very_vol;
(259) object can’t be qualified both far and near (Parser)
far and
near, for example:
far near int spooky; /* oops -- choose far or near, not both */
(260) undefined enum tag “*” (Parser)
enum tag has not been defined, for example:
enum WHAT what; /* a definition for WHAT was never seen */
(261) struct/union member “*” redefined (Parser)
struct or
union has already been used in this struct or
union, for example:
struct {
int a;
int b;
int a; /* oops -- a different name is required here */
} input;
(262) struct/union “*” redefined (Parser)
struct {
int a;
} ms;
struct {
int a;
} ms; /* was this meant to be the same name as above? */
(263) members can’t be functions (Parser)
struct {
int a;
int get(int); /* should be a pointer: int (*get)(int); */
} object;
(264) bad bitfield type (Parser)
struct FREG {
char b0:1; /* these must be part of an int, not char */
char :6;
char b7:1;
} freg;
(265) integer constant expected (Parser)
struct {
unsigned first: /* oops -- should be: unsigned first; */
unsigned second;
} my_struct;If this was meant to be a structure with bit-fields, then the following illustrates an example:
struct {
unsigned first : 4; /* 4 bits wide */
unsigned second: 4; /* another 4 bits */
} my_struct;
(266) storage class illegal (Parser)
struct {
/* no additional qualifiers can be present with members */
static int first;
} ;
(267) bad storage class (Code Generator)
auto int foo; /* auto not permitted with global variables */
int power(static int a) /* parameters cannot be static */
{
return foo * a;
}
(268) inconsistent storage class (Parser)
extern static int where; /* so is it static or extern? */
(269) inconsistent type (Parser)
int float input; /* is it int or float? */
(270) variable can’t have storage class “register” (Parser)
register qualifier, for example:
register int gi; /* this cannot be qualified register */
int process(register int input) /* this is okay */
{
return input + gi;
}
(271) type can’t be long (Parser)
int and double can be qualified
with long. long char lc; /* what? */
(272) type can’t be short (Parser)
int can be modified with short,
for example: short float sf; /* what? */
(273) type can’t be both signed and unsigned (Parser)
signed and unsigned
cannot be used together in the same declaration, as they have opposite meaning, for
example:
signed unsigned int confused; /* which is it? */
(274) type can’t be unsigned (Parser)
unsigned, for
example: unsigned float uf; /* what? */
(275) “...” illegal in non-prototype argument list (Parser)
/* K&R-style non-prototyped function definition */
int kandr(a, b, ...)
int a, b;
{
(276) type specifier required for prototyped argument (Parser)
A type specifier is required for a prototyped argument. It is not acceptable to just have an identifier.
(277) can’t mix prototyped and non-prototyped arguments (Parser)
int plus(int a, b) /* oops -- a is prototyped, b is not */
int b;
{
return a + b;
}
(278) argument “*” redeclared (Parser)
/* cannot have two parameters called "a" */
int calc(int a, int a)
(279) initialization of function arguments is illegal (Parser)
/* oops -- a is initialized when proc is called */
extern int proc(int a = 9);
(280) arrays of functions are illegal (Parser)
int * farray[](); /* oops -- should be: int (* farray[])(); */
(281) functions can’t return functions (Parser)
A function cannot return a function. It can return a function pointer. A
function returning a pointer to a function could be declared like this: int
(* (name()))(). Note the many parentheses that are necessary to
make the parts of the declaration bind correctly.
(282) functions can’t return arrays (Parser)
A function can return only a scalar (simple) type or a structure. It cannot return an array.
(283) dimension required (Parser)
/* This should be, for example: int arr[][7] */
int get_element(int arr[2][])
{
return array[1][6];
}
(284) invalid dimension (Parser)
int array[0]; // oops -- you cannot have an array of size 0
(285) no identifier in declaration (Parser)
void interrupt(void) /* what is the name of this function? */
{
}
(286) declarator too complex (Parser)
This declarator is too complex for the compiler to handle. Examine the declaration and find a way to simplify it. If the compiler finds it too complex, so will anybody maintaining the code.
(287) arrays of bits or pointers to bit are illegal (Parser)
__bit objects, or a
pointer to bit variable, for example:
bit barray[10]; /* wrong -- no bit arrays */
bit * bp; /* wrong -- no pointers to bit variables */
(288) the type 'void' is applicable only to functions (Parser)
void. Only a function can be void,
for example:
int a;
void b; /* this makes no sense */
(289) the specifier 'interrupt' is applicable only to functions (Parser)
/* variables cannot be qualified interrupt */
interrupt int input;
(290) illegal function qualifier(s) (Parser)
const or volatile. This can indicate that you
have forgotten a star, *, that is indicating that the function
should return a pointer to a qualified object, for example:
const char ccrv(void) /* const * char ccrv(void) perhaps? */
{ /* error flagged here */
return ccip;
}
(291) K&R identifier “*” not an argument (Parser)
int process(input)
int unput; /* oops -- that should be int input; */
{
}
(292) a function is not a valid parameter type (Parser)
A function parameter cannot be a function. It can be a pointer to a
function, so perhaps a * has been omitted from the declaration.
(293) bad size in index_type() (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(294) can’t allocate * bytes of memory (Code Generator, Hexmate)
This is an internal compiler error. Contact Microchip Technical Support with details.
(295) expression too complex (Parser)
This expression has caused overflow of the compiler’s internal stack and should be rearranged or split into two expressions.
(296) out of memory (Objtohex)
This could be an internal compiler error. Contact Microchip Technical Support with details.
(297) bad argument (*) to tysize() (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(298) end of file in #asm (Preprocessor)
#asm block.
This probably means the #endasm is missing or misspelled, for
example:
#asm
MOV r0, #55
MOV [r1], r0
} /* oops -- where is the #endasm */
(300) unexpected end of file (Parser)
int main(void)
{
init();
run(); /* is that it? What about the close brace */
(301) end of file on string file (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(302) can’t reopen “*”: * (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(303) can’t allocate * bytes of memory (line *) (Parser)
The parser was unable to allocate memory for the longest string encountered, as it attempts to sort and merge strings. Try reducing the number or length of strings in this module.
(306) can’t allocate * bytes of memory for * (Code Generator)
This is an internal compiler error. Contact Microchip Technical Support with details.
(307) too many qualifier names (Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(308) too many case labels in switch (Code Generator)
There are too many case labels in this switch statement.
The maximum allowable number of case labels in any one switch
statement is 511.
(309) too many symbols (Assembler, Parser)
There are too many symbols for the assembler’s symbol table. Reduce the number of symbols in your program.
(310) “]” expected (Parser)
process(carray[idx); /* oops --
should be: process(carray[idx]); */
(311) closing quote expected (Parser)
A closing quote was expected for the indicated string.
(312) “*” expected (Parser)
The indicated token was expected by the parser.
(313) function body expected (Parser)
/* the function block must follow, not a semicolon */
int get_value(a, b);
(314) “;” expected (Parser)
while(a) {
b = a-- /* oops -- where is the semicolon? */
} /* error is flagged here */Note: Omitting a semicolon from statements not preceding a close brace or keyword typically results in some other error being issued for the following code which the parser assumes to be part of the original statement.
(315) “{” expected (Parser)
/* oops! no opening brace after the prototype */
void process(char c)
return max(c, 10) * 2; /* error flagged here */
}
(316) “}” expected (Parser)
char carray[4] = { 1, 2, 3, 4; /* oops -- no closing brace */
(317) “(” expected (Parser)
(, was expected here. This
must be the first token after a while , for ,
if , do or asm keyword, for
example:
if a == b /* should be: if(a == b) */
b = 0;
(318) string expected (Parser)
asm statement must be a string
enclosed in parentheses, for example:
asm(nop); /* that should be asm("nop");
(319) while expected (Parser)
while is expected at the end of a
do statement, for example:
do {
func(i++);
} /* do the block while what condition is true? */
if(i > 5) /* error flagged here */
end();
(320) “:” expected (Parser)
case label, or after the
keyword default. This often occurs when a semicolon is accidentally
typed instead of a colon, for example:
switch(input) {
case 0; /* oops -- that should have been: case 0: */
state = NEW;
(321) label identifier expected (Parser)
goto,
for example:
if(a)
goto 20;
/* this is not BASIC -- a valid C label must follow a goto */
(322) enum tag or “{” expected (Parser)
enum, must come either an identifier
that is, or will be, defined as an enum tag, or an opening brace,
for example:
enum 1, 2; /* should be, for example: enum {one=1, two }; */
(323) struct/union tag or “{” expected (Parser)
struct or union keyword, for example:
struct int a; /* this is not how you define a structure */You might mean something like:
struct {
int a;
} my_struct;
(324) too many arguments for printf-style format string (Parser)
/* oops -- missed a placeholder? */
printf("%d - %d", low, high, median);
(325) error in printf-style format string (Parser)
printf() style format string, and it is not
syntactically correct. If not corrected, this will cause unexpected behavior at
runtime, for example:
printf("%l", lll); /* oops -- possibly: printf("%ld", lll); */
(326) long int argument required in printf-style format string (Parser)
long argument is required for this
format specifier. Check the number and order of format specifiers and corresponding
arguments, for example:
printf("%lx", 2); // possibly you meant: printf("%lx", 2L);
(327) long long int argument required in printf-style format string (Parser)
long long argument is required for this format
specifier. Check the number and order of format specifiers and corresponding
arguments, for example:
printf("%llx", 2); // possibly you meant: printf("%llx", 2LL);
(328) int argument required in printf-style format string (Parser)
printf("%d", 1.23); /* wrong number or wrong placeholder */
(329) double argument required in printf-style format string (Parser)
%f or similar, and requires a floating-point expression. Check
for missing or extra format specifiers or arguments to printf.
printf("%f", 44); /* should be: printf("%f", 44.0); */
(330) pointer to * argument required in printf-style format string (Parser)
A pointer argument is required for this format specifier. Check the number and order of format specifiers and corresponding arguments.
(331) too few arguments for printf-style format string (Parser)
printf("%d - %d", low); /* oops! where is the other value to print? */
(332) “interrupt_level” should be 0 to 7 (Parser)
pragma interrupt_level must have an argument from 0
to 7; however, mid-range devices only use level 1. PIC18 devices can use levels 1 or
2. For example:
#pragma interrupt_level 9 /* oops -- the level is too high */
void interrupt isr(void)
{
/* isr code goes here */
}
(333) unrecognized qualifier name after “strings” (Parser)
pragma strings was passed a qualifier that was not
identified, for example:
/* oops -- should that be #pragma strings const ? */
#pragma strings cinst
(334) unrecognized qualifier name after “printf_check” (Parser)
#pragma printf_check was passed a qualifier that
could not be identified, for example:
/* oops -- should that be const not cinst? */
#pragma printf_check(printf) cinst
(335) unknown pragma “*” (Parser)
pragma directive was encountered, for
example:
#pragma rugsused myFunc w /* I think you meant regsused */
(336) string concatenation across lines (Parser)
char * cp = "hi"
"there"; /* this is okay, but is it what you had intended? */
(337) line does not have a newline on the end (Parser)
The last line in the file is missing the newline (operating system dependent character) from the end. Some editors will create such files, which can cause problems for include files. The C standard requires all source files to consist of complete lines only.
(338) can’t create * file “*” (Any)
The application tried to create or open the named file, but it could not be created. Check that all file path names are correct.
(339) initializer in extern declaration (Parser)
extern has an
initializer. This overrides the extern storage class, because to
initialize an object it is necessary to define (i.e., allocate storage for) it, for
example:
extern int other = 99; /* if it’s extern and not allocated
storage, how can it be initialized? */
(340) string not terminated by null character (Parser)
char array is being initialized with a string literal
larger than the array. Hence there is insufficient space in the array to safely
append a null terminating character, for example:
char foo[5] = "12345"; /* the string stored in foo won’t have
a null terminating, i.e.
foo = [’1’, ’2’, ’3’, ’4’, ’5’] */
(343) implicit return at end of non-void function (Parser)
return statement with a value, or
if the function is not to return a value, declare it void, for
example:
int mydiv(double a, int b)
{
if(b != 0)
return a/b; /* what about when b is 0? */
} /* warning flagged here */
(344) non-void function returns no value (Parser)
return statement that does not specify a return value, for
example:
int get_value(void)
{
if(flag)
return val++;
return;
/* what is the return value in this instance? */
}
(345) unreachable code (Parser)
while(1) /* how does this loop finish? */
process();
flag = FINISHED; /* how do we get here? */
(346) declaration of “*” hides outer declaration (Parser)
int input; /* input has filescope */
void process(int a)
{
int input; /* local blockscope input */
a = input; /* this will use the local variable. Is this right? */
(347) external declaration inside function (Parser)
extern declaration. This is
legal but is invariably not desirable as it restricts the scope of the function
declaration to the function body. This means that if the compiler encounters another
declaration, use, or definition of the extern object later in the
same file, it will no longer have the earlier declaration and thus will be unable to
check that the declarations are consistent. This can lead to strange behavior of
your program or signature errors at link time. It will also hide any previous
declarations of the same thing, again subverting the compiler’s type checking. As a
general rule, always declare extern variables and functions outside
any other functions. For example:
int process(int a)
{
/* this would be better outside the function */
extern int away;
return away + a;
}
(348) auto variable “*” should not be qualified (Parser)
An auto variable should not have qualifiers such as
near or far associated with it. Its storage
class is implicitly defined by the stack organization. An auto variable can be
qualified with static, but it is then no longer auto.
(349) non-prototyped function declaration for “*” (Parser)
int process(input)
int input; /* warning flagged here */
{
}This would be better written:
int process(int input)
{
}
(350) unused * “*” (from line *) (Parser)
The indicated object was never used in the function or module being
compiled. Either this object is redundant, or the code that was meant to use it was
excluded from compilation or misspelled the name of the object. Note that the
symbols rcsid and sccsid are never reported as
being unused.
(352) float parameter coerced to double (Parser)
float, the compiler converts this to a double.
This is because the default C type conversion conventions provide that when a
floating-point number is passed to a non-prototyped function, it is converted to
double. It is important that the function declaration be
consistent with this convention, for example:
double inc_flt(f) /* f will be converted to double */
float f; /* warning flagged here */
{
return f * 2;
}
(353) sizeof external array “*” is zero (Parser)
The size of an external array evaluates to zero. This is probably due to the array not having an explicit dimension in the extern declaration.
(354) possible pointer truncation (Parser)
A pointer qualified far has been assigned to a default pointer, or a pointer qualified near, or a default pointer has been assigned to a pointer qualified near. This can result in truncation of the pointer and loss of information, depending on the memory model in use.
(355) implicit signed to unsigned conversion (Parser)
signed char sc;
unsigned int ui;
ui = sc; /* if sc contains 0xff, ui will contain 0xffff for example */will perform a sign extension of the char variable to the longer type. If you do not want this to take place, use a cast, for example:
ui = (unsigned char)sc;
(356) implicit conversion of float to integer (Parser)
double dd;
int i;
i = dd; /* is this really what you meant? */If you do intend to use an expression like this, then indicate that this is so by a cast:
i = (int)dd;
(357) illegal conversion of integer to pointer (Parser)
& address operator, for example:
int * ip;
int i;
ip = i; /* oops -- did you mean ip = &i ? */If you do intend to use an expression like this, then indicate that this is so by a cast:
ip = (int *)i;
(358) illegal conversion of pointer to integer (Parser)
* dereference operator, for example:
int * ip;
int i;
i = ip; /* oops -- did you mean i = *ip ? */If you do intend to use an expression like this, indicate your intention by a cast:
i = (int)ip;
(359) illegal conversion between pointer types (Parser)
long input;
char * cp;
cp = &input; /* is this correct? */This is a common way of accessing bytes within a multi-byte variable. To indicate that this is the intended operation of the program, use a cast:
cp = (char *)&input; /* that’s better */
This warning can also occur when converting between pointers to objects that have the same type, but which have different qualifiers, for example:
char * cp;
/* yes, but what sort of characters? */
cp = "I am a string of characters";
If the default type for string literals is const char
*, then this warning is quite valid. This should be written:
const char * cp;
cp = "I am a string of characters"; /* that’s better */
Omitting a qualifier from a pointer type is often disastrous and almost certainly not what you intend.
(360) array index out of bounds (Parser)
int i, * ip, input[10];
i = input[-2]; /* oops -- this element doesn’t exist */
ip = &input[5];
i = ip[-2]; /* this is okay */
(361) function declared implicit int (Parser)
extern or static, as appropriate. For example:
/* I can prevent an error arising from calls below */
extern void set(long a, int b);
int main(void)
{
/* at this point, a prototype for set() has already been seen */
set(10L, 6);
}
(362) redundant “&” applied to array (Parser)
& has been applied to an array.
Because using the name of an array gives its address anyway, this is unnecessary and
has been ignored, for example:
int array[5];
int * ip;
/* array is a constant, not a variable; the & is redundant. */
ip = &array;
(363) redundant “&” or “*” applied to function address (Parser)
& has been applied to a
function. Because using the name of a function gives its address anyway, this is
unnecessary and has been ignored, for example:
extern void foo(void);
int main(void)
{
void(*bar)(void);
/* both assignments are equivalent */
bar = &foo;
bar = foo; /* the & is redundant */
}
(364) attempt to modify object qualified * (Parser)
const or code cannot
be assigned to or modified in any other way by your program. The effect of
attempting to modify such an object is compiler specific.
const int out = 1234; /* "out" is read only */
out = 0; /* oops -- writing to a read-only object */
(365) pointer to non-static object returned (Parser)
char * get_addr(void)
{
char c;
/* returning this is dangerous; the pointer could be dereferenced */
return &c;
}
(366) operands of “*” not same pointer type (Parser)
The operands of this operator are of different pointer types. This probably means you have used the wrong pointer, but if the code is actually what you intended, use a typecast to suppress the error message.
(367) identifier is already extern; can’t be static (Parser)
extern, possibly
through an implicit declaration. It has now been redeclared static,
but this redeclaration is invalid.
int main(void)
{
/* at this point the compiler assumes set is extern... */
set(10L, 6);
}
/* now it finds out otherwise */
static void set(long a, int b)
{
PORTA = a + b;
}
(368) array dimension on “*[ ]” ignored (Preprocessor)
/* param should be: "int array[]" or "int *" */
int get_first(int array[10])
{ /* warning flagged here */
return array[0];
}
(369) signed bitfields not supported (Parser)
int, the compiler still treats it as unsigned, for example:
struct {
signed int sign: 1; /* oops -- this must be unsigned */
signed int value: 7;
} ;
(370) illegal basic type; int assumed (Parser)
/* here ling is assumed to be int */
unsigned char bar = (unsigned ling) ’a’;
(371) missing basic type; int assumed (Parser)
int
has been assumed. This declaration is not illegal, but it is preferable to include a
basic type to make it clear what is intended, for example:
char c;
i; /* don’t let the compiler make assumptions, use : int i */
func(); /* ditto, use: extern int func(int); */
(372) “,” expected (Parser)
unsigned char a;
/* thinks: chat & b are unsigned, but where is the comma? */
unsigned chat b;
(373) implicit signed to unsigned conversion (Parser)
unsigned type was expected where a
signed type was given and was implicitly converted to
unsigned, for example:
unsigned int foo = -1;
/* the above initialization is implicitly treated as:
unsigned int foo = (unsigned) -1; */
(374) missing basic type; int assumed (Parser)
int., for example:
int i = (signed) 2; /* (signed) assumed to be (signed int) */
(375) unknown FNREC type “*” (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(376) bad non-zero node in call graph (Linker)
The linker has encountered a top level node in the call graph that is referenced from lower down in the call graph. This probably means the program has indirect recursion, which is not allowed when using a compiled stack.
(378) can’t create * file “*” (Hexmate)
This type of file could not be created. Is the file, or a file by this name, already in use?
(379) bad record type “*” (Linker)
This is an internal compiler error. Ensure that the object file is a valid object file. Contact Microchip Technical Support with details.
(380) unknown record type (*) (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(381) record “*” too long (*) (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(382) incomplete record: type = *, length = * (Dump, Xstrip)
This message is produced by the dump or
xstrip utilities and indicates that the object file is not a
valid object file, or that it has been truncated. Contact Microchip Technical
Support with details.
(383) text record has length (*) too small (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(384) assertion failed: file *, line *, expression * (Linker, Parser)
This is an internal compiler error. Contact Microchip Technical Support with details.
(387) illegal or too many -G options (Linker)
There has been more than one linker -g option, or the
-g option did not have any arguments following. The arguments
specify how the segment addresses are calculated.
(388) duplicate -M option (Linker)
The map file name has been specified to the linker for a second time. This should not occur if you are using a compiler driver. If invoking the linker manually, ensure that only one instance of this option is present on the command line.
(389) illegal or too many -O options (Linker)
This linker -o flag is illegal, or another
-o option has been encountered. A -o option to
the linker must be immediately followed by a filename with no intervening space.
(390) missing argument to -P (Linker)
There have been too many -p options passed to the
linker, or a -p option was not followed by any arguments. The
arguments of separate -p options can be combined and separated by
commas.
(391) missing argument to -Q (Linker)
The -Q linker option requires the machine type for an
argument.
(392) missing argument to -U (Linker)
The -U (undefine) option needs an argument.
(393) missing argument to -W (Linker)
The -W option (listing width) needs a numeric
argument.
(394) duplicate -D or -H option (Linker)
The symbol file name has been specified to the linker for a second time. This should not occur if you are using a compiler driver. If invoking the linker manually, ensure that only one instance of either of these options is present on the command line.
(395) missing argument to -J (Linker)
The maximum number of errors before aborting must be specified following
the -j linker option.
(397) usage: hlink [-options] files.obj files.lib (Linker)
Improper usage of the command-line linker. If you are not invoking the linker directly, this could be an internal compiler error, and you should contact Microchip Technical Support with details.
(398) output file can’t be also an input file (Linker)
The linker has detected an attempt to write its output file over one of its input files. This cannot be done, because it needs to simultaneously read and write input and output files.
(400) bad object code format (Linker)
This is an internal compiler error. The object code format of an object file is invalid. Ensure it is a valid object file. Contact Microchip Technical Support with details.
(402) bad argument to -F (Objtohex)
The -F option for objtohex has been supplied an invalid
argument. If you are not invoking this tool directly, this is an internal compiler
error, and you should contact Microchip Technical Support with details.
(403) bad -E option: “*” (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(404) bad maximum length value to -<digits> (Objtohex)
The first value to the OBJTOHEX -n,m HEX
length/rounding option is invalid.
(405) bad record size rounding value to -<digits> (Objtohex)
The second value to the OBJTOHEX -n,m HEX
length/rounding option is invalid.
(406) bad argument to -A (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(407) bad argument to -U (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(408) bad argument to -B (Objtohex)
This option requires an integer argument in either base 8, 10, or 16. If you are not invoking this tool directly, this is an internal compiler error and you should contact Microchip Technical Support with details.
(409) bad argument to -P (Objtohex)
This option requires an integer argument in either base 8, 10, or 16. If you are not invoking this tool directly, this is an internal compiler error and you should contact Microchip Technical Support with details.
(410) bad combination of options (Objtohex)
The combination of options supplied to OBJTOHEX is invalid.
(412) text does not start at 0 (Objtohex)
Code in some things must start at zero. Here it doesn’t.
(413) write error on “*” (Assembler, Linker, Cromwell)
A write error occurred on the named file. This probably means you have run out of disk space.
(414) read error on “*” (Linker)
The linker encountered an error trying to read this file.
(415) text offset too low in COFF file (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(416) bad character (*) in extended TEKHEX line (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(417) seek error in “*” (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(418) image too big (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(419) object file is not absolute (Objtohex)
The object file passed to OBJTOHEX has relocation items in it. This can indicate it is the wrong object file, or that the linker or OBJTOHEX have been given invalid options. The object output files from the assembler are relocatable, not absolute. The object file output of the linker is absolute.
(420) too many relocation items (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(421) too many segments (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(422) no end record (Linker)
This object file has no end record. This probably means it is not an object file. Contact Microchip Technical Support if the object file was generated by the compiler.
(423) illegal record type (Linker)
There is an error in an object file. This is either an invalid object file, or an internal error in the linker. Contact Microchip Technical Support with details if the object file was created by the compiler.
(424) record too long (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(425) incomplete record (Objtohex, Libr)
The object file passed to OBJTOHEX or the librarian is corrupted. Contact Microchip Technical Support with details.
(427) syntax error in list (Objtohex)
There is a syntax error in a list read by OBJTOHEX. The list is read from standard input in response to an option.
(428) too many segment fixups (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(429) bad segment fixups (Objtohex)
This is an internal compiler error. Contact Microchip Technical Support with details.
(430) bad specification (Objtohex)
A list supplied to OBJTOHEX is syntactically incorrect.
(431) bad argument to -E (Objtoexe)
This option requires an integer argument in either base 8, 10, or 16. If
you are invoking objtoexe directly then check this argument.
Otherwise, this can be an internal compiler error and you should contact Microchip
Technical Support with details.
(432) usage: objtohex [-ssymfile] [object-file [exe-file]] (Objtohex)
Improper usage of the command-line tool objtohex. If
you are not invoking this tool directly, this is an internal compiler error and you
should contact Microchip Technical Support with details.
(434) too many symbols (*) (Linker)
There are too many symbols in the symbol table, which has a limit of * symbols. Change some global symbols to local symbols to reduce the number of symbols.
(435) bad segment selector “*” (Linker)
-G) to the linker is
invalid, for example: -GA/f0+10Did you forget the radix?
-GA/f0h+10
(436) psect “*” re-orged (Linker)
This psect has had its start address specified more than once.
(437) missing “=” in class spec (Linker)
A class spec needs an = sign, e.g.,
-Ctext=ROM.
(438) bad size in -S option (Linker)
-S specification is invalid, it
should be a valid number, in decimal, octal, or hexadecimal radix. The radix is
specified by a trailing O, for octal, or H for
HEX. A leading 0x can also be used for hexadecimal. Case in not
important for any number or radix. Decimal is the default, for example:
-SCODE=f000Did you forget the radix?
-SCODE=f000h
(439) bad -D spec: “*” (Linker)
-D specification, giving a delta value
to a class, is invalid, for example:
-DCODEWhat is the delta value for this class? Possibly, you meant something like:
-DCODE=2
(440) bad delta value in -D spec (Linker)
The delta value supplied to a -D specification is
invalid. This value should an integer of base 8, 10, or 16.
(441) bad -A spec: “*” (Linker)
-A specification, giving address ranges
to the linker, is invalid, for example:
-ACODEWhat is the range for this class? Possibly, you meant:
-ACODE=0h-1fffh
(442) missing address in -A spec (Linker)
-A specification, giving address ranges
to the linker, is invalid, for example:
-ACODE=What is the range for this class? Possibly, you meant:
-ACODE=0h-1fffh
(443) bad low address “*” in -A spec (Linker)
-A specification is invalid:
it should be a valid number, in decimal, octal, or hexadecimal radix. The radix is
specified by a trailing O (for octal) or H for
HEX. A leading 0x can also be used for hexadecimal. Case in not
important for any number or radix. Decimal is default, for example:
-ACODE=1fff-3fffhDid you forget the radix?
-ACODE=1fffh-3fffh
(444) expected “-” in -A spec (Linker)
-, between the high and
low addresses in a -A linker option, for example:
-AROM=1000hPossibly, you meant:
-AROM=1000h-1fffh
(445) bad high address “*” in -A spec (Linker)
-A specification is invalid:
it should be a valid number, in decimal, octal, or hexadecimal radix. The radix is
specified by a trailing O, for octal, or H for
HEX. A leading 0x can also be used for hexadecimal. Case in not
important for any number or radix. Decimal is the default, for example:
-ACODE=0h-ffffDid you forget the radix?
-ACODE=0h-ffffh
(446) bad overrun address “*” in -A spec (Linker)
-A specification is
invalid: it should be a valid number, in decimal, octal, or hexadecimal radix. The
radix is specified by a trailing O (for octal) or
H for HEX. A leading 0x can also be used for
hexadecimal. Case in not important for any number or radix. Decimal is default, for
example: -AENTRY=0-0FFh-1FFDid you forget the radix?
-AENTRY=0-0FFh-1FFh
(447) bad load address “*” in -A spec (Linker)
-A specification is invalid:
it should be a valid number, in decimal, octal, or hexadecimal radix. The radix is
specified by a trailing O (for octal) or H for
HEX. A leading 0x can also be used for hexadecimal. Case in not
important for any number or radix. Decimal is default, for example:
-ACODE=0h-3fffh/a000Did you forget the radix?
-ACODE=0h-3fffh/a000h
(448) bad repeat count “*” in -A spec (Linker)
-A specification is
invalid, for example: -AENTRY=0-0FFhxfDid you forget the radix?
-AENTRY=0-0FFhxfh
(449) syntax error in -A spec: * (Linker)
-A spec is invalid. A valid -A
spec should be something like:
-AROM=1000h-1FFFh(450) psect “*” was never defined, or is local (Linker)
This psect has been listed in a -P option, but is not
defined in any module within the program. Alternatively, the psect is defined using
the local psect flag, but with no class flag; and,
so, cannot be linked to an address. Check the assembly list file to ensure that the
psect exists and that it is does not specify the local psect flag.
(451) bad psect origin format in -P option (Linker)
-p option is not a validly formed
decimal, octal, or HEX number, nor is it the name of an existing psect. A HEX number
must have a trailing H, for example:
-pbss=f000Did you forget the radix?
-pbss=f000h
(452) bad “+” (minimum address) format in -P option (Linker)
-p
option is badly formatted, for example:
-pbss=data+f000Did you forget the radix?
-pbss=data+f000h
(453) missing number after “%” in -P option (Linker)
The % operator in a -p option (for
rounding boundaries) must have a number after it.
(454) link and load address can’t both be set to “.” in -P option (Linker)
-Pmypsect=1000h/.
-Pmypsect=./1000hBoth of these options are valid and equivalent. However, the following usage is ambiguous:
-Pmypsect=./.
What is the link or load address of this psect?
(455) psect “*” not relocated on 0x* byte boundary (Linker)
This psect is not relocated on the required boundary. Check the relocatability of the
psect and correct the -p option if necessary.
(456) psect “*” not loaded on 0x* boundary (Linker)
This psect has a relocatability requirement that is not met by the load
address given in a -p option. For example, if a psect must be on a
4K byte boundary, you could not start it at 100H.
(459) remove failed; error: *, * (Xstrip)
The creation of the output file failed when removing an intermediate file.
(460) rename failed; error: *, * (Xstrip)
The creation of the output file failed when renaming an intermediate file.
(461) can’t create * file “*” (Assembler, Code Generator)
This is an internal compiler error. Contact Microchip Technical Support with details.
(464) missing key in avmap file (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(465) undefined symbol “*” in FNBREAK record (Linker)
The linker has found an undefined symbol in the FNBREAK
record for a non-reentrant function. Contact Microchip Technical Support if this is
not handwritten assembler code.
(466) undefined symbol “*” in FNINDIR record (Linker)
The linker has found an undefined symbol in the FNINDIR
record for a non-reentrant function. Contact Microchip Technical Support if this is
not handwritten assembler code.
(467) undefined symbol “*” in FNADDR record (Linker)
The linker has found an undefined symbol in the FNADDR
record for a non-reentrant function. Contact Microchip Technical Support if this is
not handwritten assembler code.
(468) undefined symbol “*” in FNCALL record (Linker)
The linker has found an undefined symbol in the FNCALL
record for a non-reentrant function. Contact Microchip Technical Support if this is
not handwritten assembler code.
(469) undefined symbol “*” in FNROOT record (Linker)
The linker has found an undefined symbol in the FNROOT
record for a non-reentrant function. Contact Microchip Technical Support if this is
not handwritten assembler code.
(470) undefined symbol “*” in FNSIZE record (Linker)
The linker has found an undefined symbol in the FNSIZE
record for a non-reentrant function. Contact Microchip Technical Support if this is
not handwritten assembler code.
(471) recursive function calls: (Linker)
reentrant keyword (if supported with this compiler) or
recode to avoid recursion, for example:
int test(int a)
{
if(a == 5) {
/* recursion cannot be supported by some compilers */
return test(a++);
}
return 0;
}(472) non-reentrant function “*” appears in multiple call graphs: rooted at “*” and “*” (Linker)
reentrant keyword, if this compiler supports it, or recode
to avoid using local variables or parameters, or duplicate the function, for
example:
void interrupt my_isr(void)
{
scan(6); /* scan is called from an interrupt function */
}
void process(int a)
{
scan(a); /* scan is also called from main-line code */
}
(473) function “*” is not called from specified interrupt_level (Linker)
#pragma interrupt_level 1
void foo(void)
{
...
}
#pragma interrupt_level 1
void interrupt bar(void)
{
// this function never calls foo()
}
(474) no psect specified for function variable/argument allocation (Linker)
The FNCONF assembler directive which specifies to the
linker information regarding the auto/parameter block was never seen. This is
supplied in the standard runtime files if necessary. This error can imply that the
correct run-time startup module was not linked. Ensure you have used the
FNCONF directive if the runtime startup module is
hand-written.
(475) conflicting FNCONF records (Linker)
The linker has seen two conflicting FNCONF directives.
This directive should be specified only once and is included in the standard runtime
startup code which is normally linked into every program.
(476) fixup overflow referencing * * (location 0x* (0x*+*), size *, value 0x*) (Linker)
The linker was asked to relocate (fixup) an item that would not fit back into the space after relocation. See the following error message (1356) for more information.
(477) fixup overflow in expression (location 0x* (0x*+*), size *, value 0x*) (Linker)
The linker was asked to relocate (fixup) an item that would not fit back into the space after relocation. See the following error message (1356) for more information.
(478) * range check failed (location 0x* (0x*+*), value 0x* > limit 0x*) (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(479) circular indirect definition of symbol “*” (Linker)
The specified symbol has been equated to an external symbol which, in turn, has been equated to the first symbol.
(480) function signatures do not match: * (*): 0x*/0x* (Linker)
extern int get_value(int in);
/* and in another module: */
/* this is different to the declaration */
int get_value(int in, char type)
{
(481) common symbol “*” psect conflict (Linker)
A common symbol has been defined to be in more than one psect.
(482) symbol “*” is defined more than once in “*” (Assembler)
_next:
MOVE r0, #55
MOVE [r1], r0
_next: ; oops -- choose a different nameThe linker will issue this warning if the symbol (C or assembler) was defined multiple times in different modules. The names of the modules are given in the error message. Note that C identifiers often have an underscore prepended to their name after compilation.
(483) symbol “*” can’t be global (Linker)
This is an internal compiler error. Contact Microchip Technical Support with details.
(484) psect “*” can’t be in classes “*” and “*” (Linker)
class= options to the
PSECT directive, or use of the -C option to
the linker, for example:
psect final,class=CODE
finish:
/* elsewhere: */
psect final,class=ENTRY
(485) unknown “with” psect referenced by psect “*” (Linker)
with flag. The psect it has been placed with does not exist,
for example:
psect starttext,class=CODE,with=rext
; was that meant to be with text?
(486) psect “*” selector value redefined (Linker)
The selector value for this psect has been defined more
than once.
(487) psect “*” type redefined: */* (Linker)
This psect has had its type defined differently by different modules. This probably means you are trying to link incompatible object modules, i.e., linking 386 flat model code with 8086 real mode code.
(488) psect “*” memory space redefined: */* (Linker)
psect spdata,class=RAM,space=0
ds 6
; elsewhere:
psect spdata,class=RAM,space=1
(489) psect “*” memory delta redefined: */* (Linker)
global psect has been defined with two different
delta values, for example:
psect final,class=CODE,delta=2
finish:
; elsewhere:
psect final,class=CODE,delta=1
(490) class “*” memory space redefined: */* (Linker)
A class has been defined in two different memory spaces. Either rename one of the classes or, if they are the same class, place them in the same memory space.
(491) can’t find 0x* words for psect “*” in segment “*” (Linker)
One of the main tasks the linker performs is positioning the blocks (or
psects) of code and data that is generated from the program into the memory
available for the target device. This error indicates that the linker was unable to
find an area of free memory large enough to accommodate one of the psects. The error
message indicates the name of the psect that the linker was attempting to position
and the segment name which is typically the name of a class which is defined by a
-A linker option issued by the compiler driver. Typically psect
names which are, or include, text relate to program code. Names
such as bss or data refer to variable blocks. This
error can be due to two reasons.
First, the size of the program or the program’s data has exceeded the total amount of space on the selected device. In other words, some part of your device’s memory has completely filled. If this is the case, then the size of the specified psect must be reduced.
The second cause of this message is when the total amount of memory needed by the psect being positioned is sufficient, but that this memory is fragmented in such a way that the largest contiguous block is too small to accommodate the psect. The linker is unable to split psects in this situation. That is, the linker cannot place part of a psect at one location and part somewhere else. Thus, the linker must be able to find a contiguous block of memory large enough for every psect. If this is the cause of the error, then the psect must be split into smaller psects if possible.
To find out what memory is still available, generate and look in the map file. Search for the string UNUSED ADDRESS RANGES. Under this heading, look for the name of the segment specified in the error message. If the name is not present, then all the memory available for this psect has been allocated. If it is present, there will be one address range specified under this segment for each free block of memory. Determine the size of each block and compare this with the number of words specified in the error message.
Psects containing code can be reduced by using all the compiler’s optimizations, or restructuring the program. If a code psect must be split into two or more small psects, this requires splitting a function into two or more smaller functions (which can call each other). These functions can need to be placed in new modules.
Psects containing data can be reduced when invoking the compiler
optimizations, but the effect is less dramatic. The program can need to be rewritten
so that it needs less variables. If the default linker options must be changed, this
can be done indirectly through the driver using the driver -Wl,
option. If a data psect cannot be positioned, then you typically need to reduce the
total size of variables being used.
For example, after receiving the message:
Can’t find 0x34 words (0x34 withtotal) for psect text in segment CODE (error)
look in the map file for the ranges of unused memory.
UNUSED ADDRESS RANGES
CODE 00000244-0000025F
00001000-0000102f
RAM 00300014-00301FFB
In the CODE segment, there is 0x1c (0x25f-0x244+1)
bytes of space available in one block and 0x30 available in another block. Neither
of these are large enough to accommodate the psect text which is
0x34 bytes long. Notice that the total amount of memory available is larger than
0x34 bytes. If the function that is encoded into the text psect can
be split into two smaller functions, there is a chance the program will link
correctly.
(492) attempt to position absolute psect “*” is illegal (Linker)
This psect is absolute and should not have an address specified in a
-P option. Either remove the abs psect flag,
or remove the -P linker option.
(493) origin of psect “*” is defined more than once (Linker)
The origin of this psect is defined more than once. There is most likely
more than one -p linker option specifying this psect.
(494) bad -P format “*/*” (Linker)
-P option given to the linker is malformed. This
option specifies placement of a psect, for example:
-Ptext=10g0hPossibly, you meant:
-Ptext=10f0h
(495) use of both “with=” and “INCLASS/INCLASS” allocation is illegal (Linker)
It is not legal to specify both the link and location of a psect as within a class, when that psect was also defined using a with psect flag.
(497) psect “*” exceeds max size: *h > *h (Linker)
The psect has more bytes in it than the maximum allowed as specified
using the size psect flag.
(498) psect “*” exceeds address limit: *h > *h (Linker)
The maximum address of the psect exceeds the limit placed on it using
the limit psect flag. Either the psect needs to be linked at a
different location or there is too much code/data in the psect.
(499) undefined symbol: (Assembler, Linker)
The symbol following is undefined at link time. This could be due to spelling error, or failure to link an appropriate module.