5.6 Assembly List Files
An assembly list file is a human-readable listing, showing the opcodes that are present in the final output and the addresses at which they are located.
The assembler will produce an assembly list file if instructed using the
-Wa,-a option. From the MPLAB X IDE, this option can be
specified by selecting the Generate the ASM listing file
checkbox in the category in the Project Properties dialog. When using the MPLAB
Extension for VS Code, a similar checkbox exists in category.
There is one assembly list file produced for each assembly source file.