1.14 Bootloader Linker and Build Options
Compiler, Linker and Post Build Options for the Bootloader and Application Projects
Since the bootloader often requires specialized build features, extra build options are often required. These settings are automatically enabled in the most recent versions of MPLABx.
- Basic Verification Linker Settings
-
If the user is not enabling any Code Protect or Codeguard settings, then no linker command line changes are required and the user can skip to the Application Post Build Options below
- Code Protect / Code Guard settings
-
When the user selected Code Protect Bootloader, the device is configured to use Codeguard. This feature requires special linker options to place the code in the correct place. The three added features are listed below along with the command line that needs to be added to the project
- Bootloader Project Linker Settings
-
-
–add-flags-code=boot Forces all code in this project placed in the boot section.
-
–add-flags-const=boot Forces all constants in this project placed in the boot section.
-
-D__USE_BFA Allows the boot section to be placed according to the security mode and not default to normal system map.
This linker command should automatically be added to the project for the user. However, they can be added manually by following the below steps.
-
Go to Project Properties
-
Go to XC16->xc16-ld
-
Under additional options add the following: –add-flags-code=boot,–add-flags-const=boot,-D__USE_BFA
-
- ECDSA Verification with Code Protect / Code Guard settings
-
When the user selected Code Protect Bootloader, the device is configured to use Codeguard. This feature requires special linker options to place the code in the correct place. Below are the linker settings for the bootloader.
- Application Project Post Build Settings
-
As the final part of the build process, the application code needs to be signed and converted to a hex format to download. This process is the same for all verification methods and is shown below.
Windows Post Build Command
cd mcc_generated_files/boot && postBuild.bat $(MP_CC_DIR) $(ProjectDir) $(ImageDir) $(ImageName) $(IsDebug)
Linux Post Build Command
cd mcc_generated_files/boot && ./postBuild.sh $(MP_CC_DIR) $(ProjectDir) $(ImageDir) $(ImageName) $(IsDebug)
- Adding Post Build step to Application Project
-
-
Go to Project Properties
-
Select the 'Building' left navigation node.
-
Check the box next to 'Execute this line after the build'.
-
- Application Side Linker Workaround
-
Due to XC16-2324 and XC16-2333, it is possible for link-time or run-time issues in specific situations when using this bootloader solution. The following workarounds are required on the application side only when the project has the all of the following settings:
- Device > 64KB
- Code Protect / Code Guard enabled
- XC-16 (any version) or XC-DSC 3.00
Workaround #1 (Recommended): Update to XC-DSC 3.10 or newer. It is recommended to update to the latest compiler when possible.
Workaround #2: When it is not possible to update the version of the compiler in use for the project, the following manual workaround will resolve this potential issue.- Copy the device linker file into the project. The location of the golden linker file on
the system depends on the compiler versions and Device Family Packs (DFPs) installed. The
easiest way to find the most current linker file is to first build the project with the
default settings. At the very end of the build process in the Output window, there will be
a line that shows the linker file used for the build as show below. Copy this linker file
and place in the root of the project folder.
- "Info: Loading file: <FILE PATH>/gld/<device_name>.gld”
- Modify the linker file. Open the copied
version of the linker file in a text/code editor. Locate the first SECTIONS declaration and
add the following line inside of the SECTIONS{} declaration at the top.
.application_header 0x<BOOT_CONFIG_APPLICATION_IMAGE_APPLICATION_HEADER_ADDRESS>: { KEEP(*(.application_header)); } >programNOTE: Replace BOOT_CONFIG_APPLICATION_IMAGE_APPLICATION_HEADER_ADDRESS with the resolved value defined in boot_config.h. These instructions and the exact line to copy with the resolved value already injected can be found in application_header.S in 16-bit Bootloader version 1.25.1 and later.
When complete, it should look similar to the following:
Save the modified linker file.SECTIONS { .application_header 0x<BOOT_CONFIG_APPLICATION_IMAGE_APPLICATION_HEADER_ADDRESS>: { KEEP(*(.application_header)); } >program #if !defined(__CORESIDENT) || defined(__DEFINE_RESET) .reset : { SHORT(ABSOLUTE(__reset)); SHORT(0x04); SHORT((ABSOLUTE(__reset) >> 16) & 0x7F); SHORT(0); } >reset #endif - Add the modified linker file to the project. In the "Projects" pane in MPLAB X, right click on the "Linker Files" folder. Select "Add Existing Item" Browse to the modified linker file modified in step 2.