3.6.1 Chip Erase
As it refers to ERASE_FAILED, a status bit that does not exist in the UPDI, a clarification has been made to the Chip Erase section. Functional changes are shown in bold.
Follow these steps to issue a chip erase:
        - Enter the Chip Erase key by using
                    the 
KEYinstruction. See Key Activation Signatures for the CHIPERASE signature. - Optional: Read the Chip Erase (CHIPERASE) bit in the ASI Key Status (UPDI.ASI_KEY_STATUS) register to see that the key is successfully activated.
 - Write the signature to the Reset Request (RSTREQ) bit in the ASI Reset Request (UPDI.ASI_RESET_REQ) register, which will issue a System Reset.
 - Write 
0x00to the ASI Reset Request (UPDI.ASI_RESET_REQ) register to clear the System Reset. - Read the NVM Lock Status (LOCKSTATUS) bit from the ASI System Status (UPDI.ASI_SYS_STATUS) register.
 - The chip erase is done when the
                    LOCKSTATUS bit is ‘
0’. If the LOCKSTATUS bit is ‘1’, return to step 5. - Check the Chip Erase Key Failed (ERASE_FAILED) bit in the ASI System Status (UPDI.ASI_SYS_STATUS) register to verify if the chip erase was successful.
 - If the
                            ERASE_FAILED bit is ‘
0’, the chip erase was successful. 
After a successful chip erase, the lock bits will be cleared, and the UPDI will have full access to the system. Until the lock bits are cleared, the UPDI cannot access the system bus, and only CS-space operations can be performed.
CAUTION: During chip erase, the
            BOD is forced into ON state by writing to the Active (ACTIVE) bit field from the Control
            A (BOD.CTRLA) register and uses the BOD Level (LVL) bit field from the BOD Configuration
            (FUSE.BODCFG) fuse and the BOD Level (LVL) bit field from the Control B (BOD.CTRLB)
            register. If the supply voltage VDD is below that threshold level, the device
            is unavailable until VDD is increased adequately. See the BOD section
            for more details.