5.2.6.1 Analog-to-Digital Conversion
Once the programmed start-up time (ADC_MR.STARTUP) has elapsed, ADC conversions are sequenced by three operating times:
- Tracking time—the time for the ADC to charge its input sampling capacitor to the input voltage (depends on the impedance of the analog driver connected to the package pin). When several channels are converted to Continuous mode (i.e., without waiting for a trigger event), the inherent tracking time is 6 ADC clock cycles. However, the tracking time can be increased using the TRACKTIM field in the Mode register (ADC_MR) and the TRACKX4 bit in the Extended Mode register (ADC_EMR).
- ADC inherent conversion time—the time for the ADC to convert the sampled analog voltage. This time is constant and is defined from start of conversion to end of conversion.
- Channel conversion period—the effective time between the end of the
current channel conversion and the end of the next channel conversion.
Figure 5-2. Sequence of Consecutive ADC Conversions with TRACKTIM = 0 Figure 5-3. Sequence of Consecutive ADC Conversions with TRACKTIM = 4 and TRACKX4 = 1