9.1 MCC Generated Code
To generate this project using MPLAB Code Configurator (MCC), follow the next steps:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open MCC from the toolbar (more information about how to install the MCC plug-in can be found here).
- Go to Project Resources →
System → System Module and make the following configurations:
- Oscillator Select: HFINTOSC
- HF Internal Clock: 1 MHz
- Clock Divider: 1
- In the Watchdog Timer Enable field in the WWDT tab, WDT Disabled has to be selected
- In the Programming tab, Low-Voltage Programming Enable has to be checked
- From the Device Resources window, add
TMR2, TMR4 and make the following configurations:
Timer2 Configuration:
- Enable Timer: checked
- Control Mode: Roll over pulse
- Ext. Reset Source: TMR4_postscaled
- Start/Reset Option: Starts at
T2ON =
1and TMR2_ers =0 - Timer Clock tab
- Clock Source: LFINTOSC
- Clock Prescaler: 1:64
- Postscaler: 1:1
- Set 100 ms period in the
Timer Period tab
- Enabled Timer Interrupt: checked
-
Timer4 Configuration:
- Enable Timer: checked
- Control mode: One shot
- Ext. Reset Source: T4INPPS pin
- Start/Reset Option: Starts at
TMR4_ers =
0and Resets at TMR4_ers =1 - Timer Clock tab:
- Clock Source: LFINTOSC
- Clock Prescaler: 1:64
- Postscaler: 1:1
- Set 500 ms period in the Timer Period tab
- Open Pin Manager → Grid
View window, select UQFN40 in the MCU package field and select the
I/O pins outputs to enable the internal signal access to the I/O.
Figure 9-1. Pin Mapping
- Click Pin Module in the Project Resources, set the custom name for RE0 to LED0 and select Output box. For RC7 pin, select WPU.
- Click Generate in the Project Resources tab.
- The Interrupt function that will
toggle LED0 at Timer2 period will need to be added before
mainfunction:void TMR2_interrupt(void) { /* Toggle LED0 at the Timer2Period frequency */ LED0_Toggle(); } void main(void) { // Initialize the device SYSTEM_Initialize(); TMR2_SetInterruptHandler(TMR2_interrupt); // Enable the Global Interrupts INTERRUPT_GlobalInterruptEnable(); // Enable the Peripheral Interrupts INTERRUPT_PeripheralInterruptEnable(); while (1) { // Add your application code } }