3.1 MCC Generated Code
To generate this project using MPLAB Code Configurator (MCC), follow the next steps:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open MCC from the toolbar (more information about how to install the MCC plug-in can be found here).
- Go to Project Resources →
System → System Module and make the following configurations:
- Oscillator Select: HFINTOSC
- HF Internal Clock: 1 MHz
- Clock Divider: 1
- In the Watchdog Timer Enable field in the WWDT tab, WDT Disabled has to be selected
- In the Programming tab, Low-Voltage Programming Enable has to be checked
- From the Device Resources window, add
TMR0 and do the following configurations:
Timer0 Configuration:
- Enable Timer: checked
- Timer Clock tab
- Clock Source: LFINTOSC
- Clock Prescaler: 1:32
- Postscaler: 1:1
- Timer mode: 16-bit
- Enable Synchronization: unchecked
- Timer period: 10s
- Enable Timer Interrupt: checked
- Open Pin Manager → Grid
View window and select UQFN40 in the MCU package field and
make the following pin configuration:
- Set Port E pin 0 (RE0) as output
Figure 3-1. Pin Mapping - Click Pin Module in the Project Resources and set the custom name for RE0 to LED0.
- Click Generate in the Project Resources tab.
- In the
main.cfile generated by MCC, change or add the following code:- Enable the Global and Peripheral interrupts
- Light up LED0, wait 100 ms, turn off LED0 and put the microcontroller to Sleep
-
void main(void) { // Initialize the device SYSTEM_Initialize(); // Enable the Global Interrupts INTERRUPT_GlobalInterruptEnable(); // Enable the Peripheral Interrupts INTERRUPT_PeripheralInterruptEnable(); while (1) { LED0_SetLow(); __delay_ms(100); LED0_SetHigh(); SLEEP(); } }