11.1 MCC Generated Code
To generate this project using MPLAB Code Configurator (MCC) the next steps need to be followed:
- Create a new MPLAB X IDE project for PIC18F47Q10.
- Open the MCC from the toolbar (information about how to install the MCC plug-in can be found here).
- Go to Project Resources →
System → System Module and make the following configurations:
- Oscillator Select: HFINTOSC
- HF Internal Clock: 4 MHz
- Clock Divider: 1
- In the Watchdog Timer Enable field in the WWDT tab, WDT Disabled has to be selected
- In the Programming tab, Low-Voltage Programming Enable has to be checked
- From the Device Resources window, add
TMR2, MSSP1 and make the following configurations:
Timer2 Configuration:
- Enable Timer: checked
- Timer Clock tab
- Clock Source: HFINTOSC
- Clock Prescaler: 1:64
- Postscaler: 1:1
- Set 50 µs period in the Timer Period tab
MSSP1 Configuration:
- Serial Protocol: SPI
- Mode: Master
- SPI Mode: SPI Mode 0
- Input Data Sampled At: Middle
- Clock Source Selection: TMR2/2
- Actual Clock Frequency (Hz): 10000.00
- Open Pin Manager → Grid
View window, select UQFN40 in the MCU package field, and make the
following pin configurations:
- Set Port C pin 6 (RC6) as output for Slave Select 1 (SS 1)
- Set Port C pin 7 (RC7) as output for Slave Select 2 (SS 2)
The SCK, SDO and SDI pins appear alongside the MSSP1 peripheral and have their direction preset.
Figure 11-1. Pin Mapping - Click Pin Module in the Project
Resources and set the custom names SS pins:
- Rename RC6 to Slave1
- Rename RC7 to Slave2
- Click Generate in the Project Resources tab.
- In the
main.cfile generated by MCC, add the following code:- Control of Slave devices
- Data transmission
uint8_t writeData = 1; /* Data that will be transmitted */ uint8_t receiveData; /* Data that will be received */ void main(void) { // Initialize the device SYSTEM_Initialize(); while (1) { SPI1_Open(SPI1_DEFAULT); Slave1_SetLow(); receiveData = SPI1_ExchangeByte(writeData); Slave1_SetHigh(); SPI1_Close(); SPI1_Open(SPI1_DEFAULT); Slave2_SetLow(); receiveData = SPI1_ExchangeByte(writeData); Slave2_SetHigh(); SPI1_Close(); } }