Reversal of Read to Write

The host initiates the communication by a read command and finishes it by a write command.

The figure below describes the REPEATED START and the reversal from Read mode to Write mode.

Figure 45-36. Repeated Start and Reversal from Read Mode to Write Mode
Note: TXCOMP is only set at the end of the transmission. This is because after the REPEATED START, SADR is detected again.