1 Harmony 3 Driver and System Service Application Examples for PIC32CZ CA80 Family
The following applications are provided to demonstrate the typical or interesting usage
models of one or more drivers, system services and RTOS.
Name | Description |
---|---|
Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
FAT File System using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
FAT File System using SD Card Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
FAT File System using SDMMC Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDMMC driver |
FAT File System using SST26 Media | This application shows an example of using the FAT File System to access SQI based SST26 flash media |
FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
I2C Driver Asynchronous - Multi-client | This example application demonstrates the multi-client feature of the asynchronous mode of the I2C driver by communicating with an external EEPROM and a temperature sensor |
I2C EEPROM AT24 Driver - EEPROM Read Write | This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM |
SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
SPI EEPROM AT25 Driver - EEPROM Read Write | This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM |
Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |
USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |