3.2.6 Error Response Details
When a MDFU client detects an error during the update, it is important that the client is able to communicate information about the error to the host.
The mechanism that the client uses to report error conditions to the host is the response (see Responses). When an error is detected, the client can report back a Response Status which indicates that an error has occurred along with a response data payload that contains more information about the error.
The following sections provide detailed definitions of the error responses including their status codes and data payload definitions.