1 Approval Information
| Country | Regulatory Agency / Reference | Approval Number | Regulatory Information (Module) | Regulatory Information (End Product) |
|---|---|---|---|---|
| Algeria | ANF | 280/H/ANF/2021 |
Trademark: Microchip Technology Inc. Model: RN4678 Serial Number: MAC Address on module label CE Marking: Available on module “Made in” remark available on module packaging label | N/A |
| Argentina | ENACOM | RAMATEL Registration Number: C-26028 |
If the product is too small, it is recommended to follow the
instruction.
|
The external label must be composed of the module RAMATEL registration number, preceded by the legend “CONTAINS”, using one of the following models: |
| Bahrain | TRA | DLM/1416/15571 | Follow CE | Follow CE |
| Bolivia | ATT | ATT-DJ-RA-H-TL LP 87/2021 | N/A | N/A |
| Botswana | BOCRA | BOCRA/TA/2020/5876 |
Label can be put on the manual or packaging |
BTA REGISTERED No.: BOCRA/TA/2020/5876 Label must have a minimum height of 2 mm. Follow BOCRA guidelines for end product. |
| Brazil | ANATEL | ANATEL: 07091-21-08759 |
|
|
| Canada | ISED | 12246A-BM78SPPS5M2 |
IC:12246A-BM78SPPS5M2 HVIN: BM78SPPS5M2 Label must be on the module |
Exterior label must use wording such as the following or similar: Contains IC:12246A-BM78SPPS5M2 |
| China | SRRC | CMIIT ID: 2015DJ7133 |
CMIIT ID: 2015DJ7133 Label must be on the module |
CMIIT ID: 2015DJ7133 The end product also needs to show "本设备包含型号核准代码为: CMIIT ID: 2015DJ7133 的无线电发射模块 “ on the product label. |
| Costa Rica | SUTEL | 00279-SUTEL-DGC-2021 | N/A | N/A |
| Ethiopia | ECA | 1599/2021 | N/A | N/A |
| Europe | CE | CE |
Label must be on the module |
Label must be on the product |
| Honduras | CONATEL | 2912/2021 | N/A | N/A |
| Indonesia | KOMINFO | 76512/SDPPI/2021 |
SDPPI Label can be affixed on unit or packaging. QR code that needs to be enclosed on the packaging |
SDPPI Label can be affixed on unit or packaging. QR code that needs to be enclosed on the packaging |
| Israel | MOC | 51-77745 |
MOC cert. no.:51-77745 Label can be put on the manual or packaging |
End product's ID. Place the label on the end product. |
| Japan | MIC | 202-SMD070 |
Label must be on the module |
Contains Transmitter Module The diameter of Japan Approved Mark must be min. > 3 mm. |
| Jordan | TRC | TRC/23/9021/2021 | N/A | N/A |
| Kenya | CA | CA/LCS/1600/GEN/Vol.1 | N/A | N/A |
| Korea | KCC | MSIP-CRM-mcp-BM78SPPS5MC2 |
Label can be put on the manual or packaging if the module is too small. |
and
|
| Kuwait | CITRA | 4778 | N/A | N/A |
| Malaysia | SIRIM QAS | 124481 |
Label can be put on the manual if there is no enough space on the product itself. | End product need to get SIRIM certificate and stick system MCMC label |
| Mexico | IFT | RCPMIRN21-1240 |
IFT: RCPMIRN21-1240 La operación de este equipo está sujeta a las siguientes dos condiciones: (1) es posible que este equipo o dispositivo no cause interferencia perjudicial y (2) este equipo o dispositivo debe aceptar cualquier interferencia, incluyendo la que pueda causar su operación no deseada. Label can be put the manual or packaging |
RCPMIRN21-1240 La operación de este equipo está sujeta a las siguientes dos condiciones: (1) es posible que este equipo o dispositivo no cause interferencia perjudicial y (2) este equipo o dispositivo debe aceptar cualquier interferencia, incluyendo la que pueda causar su operación no deseada. Place the label on the end product. |
| Nicaragua | TELCOR | NCG-CE-21-038 | N/A | N/A |
| Nigeria | NCC | NCC/TSNI/WN/TA/CERT/4083/2021 |
Label can be put on the manual or packaging |
Follow NCC guidelines for the end product. |
| Oman | TRA | TRA/TA-R/10901/21 |
Label can be put on the manual or packaging |
(End product’s ID) |
| Paraguay | CONATEL | 2020-12-I-0946 |
Label can be put on the manual or packaging |
|
| Qatar | ICT | CRA/SM/2021/S-0006992 | N/A | N/A |
| Russia | FAC | 8859 | Label can be put on the manual or packaging | Label can be put on the manual or packaging |
| South Africa | ICASA | TA-2021/0187 |
Label can be put on the manual or packaging |
|
| Taiwan | NCC | CCAN15LP0511T6 |
Label can be put on the manual or packaging |
Label must be on the product. No size requirement, but it needs to be clearly visible. This exterior label can use wording such as the following: Contains Transmitter Module:
or similar wording. |
|
UAE (United Arab Emirates) | TRA | ER97457/21 |
Label can be put on the manual or packaging |
End product’s TRA certification number and Dealer’s number. Follow TRA guidelines for the end product. |
| UKCA | CE | CE |
Label must be on the module |
The UKCA marking must be at least 5 mm in height |
| Uruguay | URSEC | VU20210210-002193 | N/A | N/A |
| USA | FCC | A8TBM78ABCDEFGH |
FCC ID: A8TBM78ABCDEFGH Label must be on the module |
The outside of final products that contains this module device must display a label referring to the enclosed module. This exterior label can use wording such as the following: FCC ID: A8TBM78ABCDEFGH or Contains FCC ID:A8TBM78ABCDEFGH |
| Venezuela | CONATEL | PCD0003 | N/A | N/A |