1 Harmony 3 Peripheral Library Application Examples for PIC32CZ CA80 Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more peripheral libraries.
| Name | Description |
|---|---|
| AC Sleepwalking | This example application shows how to use the AC Peripheral library to perform a single shot comparison in standby sleep mode periodically and wake up the device when the comparator output toggles |
| ADC Blocking | This example application shows how to use the ADC Peripheral library in blocking mode to convert analog input on a ADC channel |
| ADC DMA Scan | This example application shows how to use the ADC Peripheral library in scan mode to convert multiple analog input on a ADC channels and transfer the ADC result using DMA |
| ADC Interrupt | This example application shows how to use the ADC Peripheral library in interrupt mode to convert multiple analog inputs |
| CAN Blocking | This example application shows how to use the CAN module to transmit and receive normal CAN messages in polling mode |
| CAN FD Blocking | This example application shows how to use the CAN module to transmit and receive CAN FD messages in polling mode |
| CAN FD Interrupt | This example application shows how to use the CAN module to transmit and receive CAN FD messages in interrupt mode |
| Clock Configuration | This example application shows how to configure the clock system to run the device at maximum frequency. It also outputs a prescaled clock signal on a GPIO pin for measurement and verification |
| DMA CRC-32 Generation | This example application demonstrates how to use the DMA peripheral to compute 32-bit Cyclic Redundancy Checksum (CRC) |
| DMAC Linked List Transfer | This example application demonstrates how to use the DMA peripheral to copy multiple blocks of memory using DMA linked lists |
| DMAC Memory Transfer | This example application demonstrates how to use the DMAC peripheral to do a memory to memory transfer |
| DMAC USART Echo | This example application demonstrates USART transfer with DMA to receive 10 bytes and echo back the received bytes |
| DMAC USART Pattern Matching | This example application demonstrates how to use DMA pattern matching to abort DMA transfer when a specific character is encountered |
| DSU CRC32 Generate | This example application demonstrates how to use the DSU Peripheral library to compute 32-bit Cyclic Redundancy Checksum (CRC) |
| EIC Interrupt | This example application demonstrates how to generate interrupt using the EIC on switch press and indicate it through an LED |
| EVSYS Trigger | This example application demonstrates how to use the EVSYS Peripheral library to setup autonomous, low-latency and configurable communication between peripherals |
| FCR CRC32 Generate | This example application demonstrates how to use the FCR Peripheral library to compute 32-bit Cyclic Redundancy Checksum (CRC) |
| FCW Read Write | This example application demonstrates how to use the FCW to erase and program the internal Flash memory |
| FREQM Measurement | This example application demonstrates how to use the FREQM peripheral to measure the frequency of the internal RC Oscillator |
| MCRAMC Erase On Tamper Detect | This example application demonstrates how to test the SRAM using the MCRAMC ECC feature on internal SRAM memory.. |
| MPU Cache Coherency | This example shows how to maintain cache coherency by allocating DMA buffers in non-cacheable SRAM region defined by MPU |
| PM Wakeup Using EIC | This application demonstrates entering the low power modes and exiting it using the EIC |
| PM Wakeup Using RTC | This example demonstrates entering the low power modes and exiting it using the RTC |
| PORT Polling | This example application demonstrate how to poll the switch input, and indicate the switch status using the LED |
| RSTC Reset Cause | This example shows how to use the RSTC peripheral to indicate the cause of the device reset |
| RTC Alarm Interrupt | This example shows how to use the RTC to configure the time and generate the alarm |
| RTC Periodic Interrupt | This example application shows how to use the RTC to generate periodic interrupts |
| SERCOM I2C EEPROM Emulation (I2C Client) | This example application demonstrates how to use the SERCOM peripheral in client mode |
| SERCOM I2C EEPROM Read Write | This example application demonstrates how to use the SERCOM peripheral to write and read from the I2C serial EEPROM memory |
| SERCOM SPI EEPROM Read Write | This example application demonstrates how to use the SERCOM SPI peripheral to write and read from the SPI serial EEPROM memory |
| SERCOM SPI Interrupt | This example application shows how to use SERCOM SPI PLIB with external loop back to write and then read back an array of data in interrupt mode |
| SERCOM SPI Host Read Write Test Application | This is a SPI Host test application which is provided to demonstrate communication between SPI host and the corresponding SPI client application available under - apps/sercom/spi/slave/spi_write_read/firmware |
| SERCOM SPI Client Read Write | This example application demonstrates how to use the SERCOM SPI peripheral in client mode |
| SERCOM USART Blocking | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer block of data in a blocking manner |
| SERCOM USART Interrupt | This example application demonstrates how to use the SERCOM peripheral in USART mode to transfer data in a non-blocking manner |
| SERCOM USART Ring Buffer | This example application demonstrates how to use the SERCOM peripheral in USART ring buffer mode to transfer data in a non-blocking manner |
| SQI Flash Read Write | This example application demonstrates how to use the SQI Peripheral library to perform erase, write and read operation with the on-board SST26 SQI Serial Flash memory |
| Systick Periodic Interrupt | This example shows how to use the SysTick to generate periodic interrupts |
| TCC Capture Mode | This example shows how to use the TCC module in capture mode to measure duty cycle and frequency of an external input |
| TCC Compare Mode | This example shows how to use the TCC module in compare mode to generate different waveforms |
| TCC PWM Generation | This example application shows how to use the TCC to generate a 2 or 3 phase PWM signals for motor control with dead time |
| TCC Timer Mode | This example shows how to use the TCC module in timer mode to generate periodic interrupt |
| Temperature Sensor Measurement Calibration | This example application shows how to use the ADC Peripheral library in blocking mode to convert the internal bandgap temperature to a temperature |
| TRAM Erase On Tamper Detect | This example application shows how to configure and use tamper detect feature of RTC and TrustRam |
| TRNG Random Number | This example shows how to use the TRNG Peripheral library to generate and read a random number |
| WDT Timeout | This example shows how to generate a Watchdog timer reset by emulating a deadlock |