4.5 UART Mode Switch (PB2)
- When the host MCU pulls the UART mode switch pin from low to high (rising edge), the RNBD350 module switches to Data mode.
- When the host MCU pulls the UART mode switch pin from high to low (falling edge), the RNBD350 module switches to Command mode.
- When the host MCU uses the RN command to switch the mode, the host MCU keeps the UART mode switch pin to the original setting.
Note: By default, the UART mode switch functionality is not
assigned to the PB2 pin. The user can enable this feature using the
SR,<hex16> command, for example,
SR,0002. For more details, refer to Set Application Options (SR,<hex16>).