7 MCC Content Manager
The MCC Content Manager (CMT) allows users to select specific versions of the component modules and libraries to be used for their MCC projects.
Refer to the MCC Content Manager Reference for more information.
The MCC Melody Content Manager, supports content management and
versioning at a component level.
- This means that component modules of a project can be updated on its own, separate from the other modules. For example, if you have a working project, except for a bug on the ADC driver. Now, rather than needing to update all the other drivers in your system, like the UART and Timers, you will be able to update just the ADC.
- This component level content versioning granularity will be especially useful in the latter stages of your project development, as you near production. At this stage, when almost everything is working perfectly, one may want to change one modules one needs to, due to either bugs or needed features.