Silicon Errata Issues
The following errata issues apply to the PIC32CX BZ6 family of devices.
- Cells with an ‘X’ indicate the issue is present in this revision of the silicon.
- Cells with a dash (‘—’) indicate the issue does not exist for this revision of the silicon.
- Blank cells indicate the issue is corrected or does not exist in this revision of the silicon.
Analog-to-Digital Converter (ADC)
Glitches in ADC Conversion Result
When the ADC control clock is asynchronous with the system clock, the conversion result may have glitches if a new conversion result updates while the CPU reads ADCDATAx.
Work Around
The user must accurately read ADCBUFx before the next conversion begins. If the ADC is operated in the Asynchronous mode, ensure that each converted value is read immediately after the ready bit is set. Achieve this either by implementing a tight polling loop or by using low-latency interrupts.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Analog Comparators (AC)
Improper Comparison Operation in Standby Sleep Mode
A comparison in Single-Shot mode will not be completed when entering in Standby Sleep mode with RUNSTDBY = 0.
Work Around
Set RUNSTBDY = 1 before entering in Standby mode or wait for standby exit to start a new comparison.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Configurable Custom Logic (CCL)
PAC Error when Writing to CCL.CTRLA.SWRST Bit
Writing to the Software Reset bit in the Control A register (CTRLA.SWRST) of the CCL triggers a Peripheral Access Controller (PAC) protection error.
Work Around
Clear the CCL PAC error each time a CCL software Reset is executed.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
LUT Output is Corrupted after Enabling the CCL when using Sequential Logic
When the LUT is disabled (LUTCTRL0.ENABLE = 0) to clear the
flip-flop or latch output and then enabled again, the sequential logic remains
under Reset.
Work Around
Write to CTRL.ENABLE again after the LUT is enabled (after LUTCTRL0.ENABLE =
1).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Controller Area Network (CAN)
Debug Message Handling State Machine Not Resetting
In case CCCR.INIT bit is set by writing to the CCCR register or when the M_CAN enters Bus Off state, the debug message handling state machine stays in its current state, as signaled by RXF1S.DMS, instead of being reset to the Idle state. If RXF1S.DMS = 3, the output m_can_dma_req remains active. Setting CCCR.CCE does not change RXF1S.DMS.
This behavior is limited to when the debug on CAN Support feature is active. Regular operation is not affected. In regular operation, the debug message handling state machine always remains in the Idle state.
Work Around
If the debug message handling state machine stops while RXF1S.DMS = 1 or RXF1S.DMS = 2, the user can reset it to the Idle state either by performing hardware reset or by receiving debug messages after resetting CCCR.INIT to zero.
If the debug message handling state machine stops while RXF1S.DMS = 3 with m_can_dma_req active, the user can reset it to the Idle state either by performing a hardware reset or by activating the input m_can_dma_ack.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Message Order Inversion when Transmitting with Same Message ID
Several Tx buffers are configured with the same Message ID. Transmission of these Tx buffers is requested sequentially with a delay between the individual Tx requests. Depending on the delay between the individual Tx requests, it can happen that when multiple Tx buffers are configured with the same Message ID, the Tx buffers are not transmitted in the order of the Tx buffer number (lowest number first).
Work Around
First, write the group of Tx messages with the same Message ID to the Message RAM, and then request the transmission of all these messages concurrently by a single write access to TXBAR.
Use the Tx FIFO instead of the dedicated Tx buffers for the transmission of several messages with the same Message ID in a specific order. For more details, refer to the Section 3.5.3 Tx FIFO of the M_CAN Controller Area Network User’s Manual (Revision 3.3.1).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Interrupt Access to Reserved Area
When the reserved register space is accessed, the IR.ARA bit is not asserted and it returns zero.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Direct Memory Access Controller (DMAC)
Fetch Error on Linked Descriptors
When at least one channel using linked descriptors is already active, enabling a channel with no linked descriptor or having one of the already active channels using linked descriptors fetch the enabled second descriptor (index 1) of the channel may cause a channel Fetch Error (FERR). These errors may occur if a channel is enabled during the link request of another channel and if the channel number of the enabled channel is lower than that of the already active channel.
Work Around
When enabling a channel while other channels using linked descriptors are already active, the channel number of the new channel to enable must be greater than the other channel numbers.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Corrupted DMA Writeback Descriptor
Writeback descriptors can be corrupted on an active channel where there is an ongoing transfer while another channel is being disabled or suspended.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Event System (EVSYS)
Spurious Overrun Interrupts
In the Synchronous mode, spurious overrun interrupts can happen when the generic clock for a channel is always CHANNEL.ONDEMAND = 0.
Work Around
Set generic clock On Demand feature by setting CHANNEL.ONDEMAND = 1.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Software Event
The BUSYCH flag never resets upon software events in synchronous or resynchronized path modes with event detection on falling edges.
If a software event occurs when the EVSYS is set to synchronous or resynchronized path modes (CHANNELn.PATH = 0x0/0x1) with event detection set to falling edges (CHANNELn.EDGSEL = 0x2), the CHSTATUS.BUSYCHn flag is set but never returns to 0. As a result, it is impossible to determine whether the event user for this channel is ready to accept new events.
Work Around
Generate software events for this user through a dedicated channel configured with event detection set to rising edges (CHANNELn.EDGSEL = 0x1).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Spurious Overrun
The Overrun Interrupt flag may be incorrectly set upon software events in the Synchronous/Resynchronized Path modes with event detection on both rising and falling edges.
If a software event occurs when the EVSYS is set to Synchronous/Resynchronized Path modes (CHANNELn.PATH = 0x0/0x1) with event detection set to both rising and falling edges (CHANNELn.EDGSEL = 0x3), spurious overrun interrupts may occur (INTFLAG.OVRn).
Work Around
Generate software events for the event user through a dedicated channel configured with event detection set on rising edges (CHANNELn.EDGSEL = 0x1).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
External Interrupt Controller (EIC)
Asynchronous Edge Detection
When asynchronous edge detection is enabled and the system is in Standby Sleep mode, only the first edge is detected. Edges following the first edge of the waveform are ignored until the system wakes up.
Work Around
Use asynchronous edge detection with the debouncer enabled. The recommendation is to set DPRESCALER.PRESCALER and DPRESCALER.TICKON to achieve the lowest frequency possible. To reduce power consumption, set the EIC GCLK frequency as low as possible or select the 32KHz_LPCLK clock (with EIC CTRLA.CKSEL set).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Spurious NMI Interrupts
If the NMI is configured in the Synchronous Edge Detection mode (NMICTRL.NMISENSE = 1, 2, or 3; NMICTRL.NMIASYNCH = 0), spurious NMI interrupts may occur after a software Reset (CTRLA.SWRST = 1).
Work Around
- Configure one dummy EIC external interrupt x (EXTINTx) in the Edge Detection mode.
- Enable the EIC (CTRLA.ENABLE =
1). - Wait for synchronization to complete (SYNCBUSY.ENABLE =
0). - Configure the NMI in the Edge Detection mode.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
General-Purpose Input/Output (GPIO)
GPIO Port Value Unstable in Debug and Freeze Mode
The issue occurs when a signal changes on a GPIO pad at the same time that the MPLAB® In-Circuit Debugger (ICD) freezes the GPIO peripheral. In this case, reading the port register results in unstable values for the pads that changed.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
GPIO Change Notification Interrupt not Firing After Sleep
CNEN0x = 110 or 101. The
device does not wake up on a Pin state change.- When
CNEN0x = 110, interrupt-on-change for a negative edge transition is enabled for PORTx[n]. - When
CNEN0x = 101, interrupt-on-change for a positive edge transition is enabled for PORTx[n].
Work Around
When CNEN0x = 110, interrupt-on-change for a negative edge
transition is enabled for PORTx[n]. Keep the PORT value high before entering
the Sleep mode so that the negative edge can be detected.
When CNEN0x = 101, interrupt-on-change for a positive edge
transition is enabled for PORTx[n]. Keep the PORT value low before entering
the Sleep mode so that the positive edge can be detected.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Peripheral Access Controller (PAC)
PAC Protection Error in FREQM
FREQM reads on the Control B register (FREQM.CTRLB) to generate a PAC protection error.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Quadrature Encoder Interface (QEI)
Interval Timer (INTTMRx) Does Not Clear on Invalid QEI State Transition
In QEI mode, the INTTMR register is not reset when an invalid quadrature state transition occurs (that is, a direct 0<>3 change, where both phase inputs appear to change simultaneously).
Work Around
None.
Affected Silicon Revisions
| A0 | |||||||
|---|---|---|---|---|---|---|---|
| X |
RAM Error Correction Code (RAMECC)
4 Bytes Not Retained at Address 0x20000018
When SRAM is configured for memory retention, 4 bytes of memory cannot be retained.
Work Around
For ease-of-use, retention memory for deep sleep applications or similar applications should start at SRAM offset of 32 bytes.
Affected Silicon Revisions
| A0 | |||||||
|---|---|---|---|---|---|---|---|
| X |
Real-Time Counter and Calendar (RTCC)
Tamper Input Filter Majority Debouncing Not Working
Majority debouncing, as part of the RTCC tamper detection, does not work when enabled by setting the Debouncer Majority Enable bit, CTRLB.DEBMAJ.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
False Tamper Detection
Enabling the RTCC tamper detection feature can cause the RTCC to report a false tamper detection.
Work Around
Use any one of the following workarounds:
- Configure TAMPER detection to ONLY falling edge.
- If the user software has to use TAMPER detection as the rising edge, it must ignore the first tamper interrupt generated after enabling the RTCC tamper detection.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Periodic Event Generation when CTRLA.PRESCALER is OFF
When CTRLA.PRESCALER is set to OFF and either CTRLB.RTCOUT is set or one of the TAMPCTRL.DEBNCn bits is set, the RTCC prescaler behaves like CTRLA.PRESCALER = DIV1. The periodic events and periodic interrupts are generated.
Work Around
Clear the EVTCTRL.PEREOn bits to avoid unwanted event generation, and clear the INTENCLR.PERn bits to avoid unwanted interrupt generation.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
INFLAG.TAMPER Not Resetting
When DMA is enabled (CTRLB.DMAEN = 1), the INTFLAG.TAMPER bit does not reset after reading the TIMESTAMP register.
Work Around
Clear the INTFLAG.TAMPER bit by writing a 1 to this bit when the timestamp value is read by the DMA.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SYNCBUSY Register in Deep Sleep Mode
Entering the Deep Sleep mode without waiting for the synchronization completion of SYNCBUSY.ENABLE and SYNCBUSY.COUNTSYNC may freeze these bits status.
Work Around
The user must always configure and enable the RTCC before enabling the Deep Sleep mode.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Periodic Daily Event Generated One Second Earlier
For prescaler values above DIV1, the system must assert the periodic delay event at the end of the prescaler period to generate it on the last second of the day. Since the prescaler overflow does not qualify the periodic delay event, the system generates the event at the beginning of the prescaler period, causing it to occur one second earlier than specified.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
ACTL Detection not Gated by rtc_enable
When the RTC is configured in ACTL mode with an external tamper pin and the RTC CTRLA.ENABLE bit is not set, a tamper can be detected and a timestamp captured. The TAMPID register and the INTFLAG.TAMPER bit may, but are not always, be set.
Work Around
When the RTC is configured for tamper detection in ACTL mode with an external pin, after setting the CTRLA.ENABLE control bit, the user must wait for 10 RTC clock periods.
Then the user clears the TAMPID register, clear the INTFLAG.TAMPER bit, and performs a dummy read of the TIMESTAMP register to remove the Lock condittion on the TIMESTAMP register. After these operations, the RTC tamper is configured and running.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Write Corruption
- COUNT register in COUNT32 mode
- COUNT register in COUNT16 mode
- CLOCK register in CLOCK mode
Work Around
- Use a 32-bit write access for the COUNT register in COUNT32 mode and the CLOCK register in CLOCK mode.
- Use a 16-bit write access for the COUNT register in COUNT16 mode.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Tamper Detection Timestamp
If an external Reset occurs during tamper detection, the TIMESTAMP register is not updated when the next tamper detection is triggered.
Work Around
- SRAM
- GPx register in the RTC
- BKUPx register in the RTC
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
General Purpose Register
General Purpose registers n (GPn) are reset on tamper detection even if GPTRST = 0.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
COUNTSYNC
When COUNTSYNC is enabled, the first COUNT value is not correctly synchronized and is therefore incorrect.
Work Around
After enabling COUNTSYNC, read the COUNT register repeatedly until its value changes from the first value read. After this, all subsequent reads from the COUNT register are valid.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Root of Trust (ROT)
Storage Root Key (SRK) Not Supported
The Storage Root Key (SRK) feature is not supported. The ROOT_KEY_LCK[1:0] lock bits (SECCFG bits 9:8) and the SRK holding register are non-functional.
Work Around
None
Affected Lot ID - Date Code
For example, “2645” indicates that the device was assembled in Calendar Week (CW) 45 of 2026.
Serial Communication Interface (SERCOM)
SERCOM-I2C: Repeated Start
When the Quick command is enabled (CTRLB.QCEN = 1), the software can issue a repeated Start by writing to either CTRLB.CMD or ADDR.ADDR bit fields. If, under these conditions, the SCL Stretch mode is CTRLA.SCLSM = 1, a bus error is generated.
Work Around
Use the Quick Command mode (CTRLB.QCEN = 1) only if the SCL Stretch mode (CTRLA.SCLSM) is set to 0.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C: Client in DATA32B Mode Stalled Bus
When SERCOM is configured as an I2C client in the 32-bit Data mode (DATA32B = 1) and the I2C host reads from the I2C client (client transmitter) and outputs its NACK (indicating no more data is needed), the I2C client still receives a DRDY interrupt.
If the CPU does not write new data to the I2C client DATA register, the I2C client pulls the SDA line, resulting in a permanent bus stall.
Work Around
Use any one of the following workarounds:
- Write dummy data to the Data register when the host sends a NACK signal.
- Use command #2 (
SERCOMx->I2CS.CTRLB.CMD = 2) when the host sends a NACK signal.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C: Client Auto ACK is Not Usable
The I2C client’s AACKEN feature is not usable when doing a repeated start.
Work Around
Do not use the AACKEN feature; instead, implement an AMATCH handler.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C: Client Error Interrupt INTFLAG.ERROR Repeated Start
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C: I2C in Client Mode
Work Around
1 to each bit when they are set:- LENERR
- SEXTOUT
- LOWTOUT
- COLL
- BUSERR
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C: Client Mode with DMA
Work Around
Configure the DMA transfer size to match the number of data bytes to be received by the I2C host. The DMA cannot be used if the number of data bytes to be received by the host is unknown.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-USART: Data Transmission in Debug Mode
In the USART Operating mode, if DBGCTRL.DBGSTOP = 1, the data transmission is not halted after entering the Debug mode.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-USART: Two Stop Bits Mode Not Supported in LIN Operation
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-USART: Collision Detection
1), the SERCOM does not abort the current transfer as expected if a collision is detected and the SERCOM APB (PBx_CLK) clock is lower than the SERCOM generic clock.Work Around
The SERCOM APB (PBx_CLK) clock must always be higher than the SERCOM generic clock to support collision detection.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-USART: Error Interrupts
Work Around
Configure the SERCOM-USART to wake up on RX complete and check for any PERR or FERR Interrupt flags upon wake-up.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-USART: Flow Control in 32-Bit Extension Mode
0 or 1. Work Around
Use 8-bit mode when using Hardware Flow Control feature.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-USART: SERCOM USART in TX Mode Only
0 and the receiver is disabled (CTRLB.RXEN = 0), the clock request to the SERCOM generic clock generator feeding the SERCOM remains asserted during Standby Sleep mode, leading to unexpected overconsumption. Work Around
Configure CTRLA.RXPO and CTRLA.TXPO to use the same SERCOM pad for RX and TX, or add an external pull-up on the RX pin.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-SPI: 32-Bit Extension Mode Additional Bytes
When the 32-bit Extension mode is enabled and the data to be sent is not in multiples of 4 bytes, which means the length counter must be enabled, additional bytes are sent over the line.
Work Around
- Write the Inter-Character Spacing bits (CTRLC.ICSPACE) to a non-zero-value.
- Do not use the length counter in firmware by keeping the data to be sent in multiples of 4 bytes.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-SPI: Client Data Preload
1) before entering Standby Sleep mode may lead to increased power consumption. Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-SPI: Data Preload
1), the client transmitter may discard some data if the host cannot keep the Client Select (SS) pin low until the end of the transmission. Work Around
In SPI Client mode, the Client Select pin (SS) must be kept low by the host until the end of the transmission in case of using the Client Data Preload feature (CTRLB.PLOADEN = 1).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-SPI: Hardware Client Select Control
1), the Client Select (SS) pin goes high after each byte transfer, even if new data is ready to be sent. Work Around
Set CTRLB.MSSEN to 0 and handle the Client Select (SS) pin in software.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-SPI: SPI Host Mode
In SPI Host mode with CTRLB.MSSEN = 0, the INTFLAG.TXC flag may be asserted earlier than expected if new data is written to the DATA register close to the end of the previous byte transmission. This may cause the application to desert the Chip Select line before the SPI transfer is complete.
Work Around
- Insert a delay of at least 8 SPI clock cycles after the last DATA write before deserting the Chip Select line.
- Enable inter-character spacing by setting CTRLC.ICSPACE = 1, which inserts a one SCK cycle delay between transmitted bytes.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C Client: I2C DRDY Raised when no Data is to be Fed
The RXNACK status bit is invalid during the first I2CS_DRDY interrupt handler.
Work Around
Use a software flag to track when to ignore RXNACK (equivalent to having it true), and reset this flag in the I2CS_AMATCH interruption handler (this workaround inapplicable with AACKEN = 1).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C Client: SCL/SDA Transition Time
The minimum transition time for SCL/SDA is not met in Fast-mode Plus (1 MHz).
Work Around
| Product/Interface | Voltage Range | IOLmin |
|---|---|---|
| All SERCOM (except SERCOM2) | 2.97 < VDDIO < 3.63 | 16.3 mA |
| 1.9 < VDDIO < 2.97 | 9.3 mA | |
| SERCOM2 | 2.97 < VDDIO < 3.63 | 20mA |
| 1.9 < VDDIO < 2.97 | 13mA |
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
SERCOM-I2C Host Mode: Second DMA Packet Corrupted When LENEN = 1
When the SERCOM is enabled and configured as an I2C master with LENEN set to 1, and data packets are transferred via DMA, the transmission of the second packet gets corrupted (first byte is not transmitted) and fails to proceed.
Work Around
Disable DMA when any packet of data is transferred to SERCOM, and enable it again once the SW has written to the ADDR register.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Timer/Counter (TC)
SYNCBUSY Flag on PERBUF/CCBUFx Register
When clearing the STATUS.PERBUFV/STATUS.CCBUFVx flag, the SYNCBUSY flag is released before restoring the PERBUF/CCBUFx register to its appropriate value.
Work Around
Clear the STATUS.PERBUFV/STATUS.CCBUFVx flag twice successively to ensure that the system restores the PERBUF/CCBUFx register value before updating it.
Affected Silicon Revisions
| A0 | |||||||
|---|---|---|---|---|---|---|---|
| X |
Corrupted Re-trigger Event Waveform Output
If a Re-trigger event (EVCTRL.EVACTn = 1, RETRIGGER) occurs at the Channel Compare Match [n] time, the next waveform output [n] is corrupted.
Work Around
Use two channels to store their two successive (n and n+1) CC register values and combine their related waveform outputs to make signal redundancy.
Affected Silicon Revisions
| A0 | |||||||
|---|---|---|---|---|---|---|---|
| X |
Timer/Counter for Control Applications (TCC)
Dithering Mode with External Re-trigger Events
Using the TCC in the Dithering mode with external re-trigger events can lead to an unexpected stretch of right-aligned pulses or shrink of left-aligned pulses.
Work Around
Do not use re-trigger events or actions when the TCC module is configured in the Dithering mode.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
LUPD Feature in Down-Counting Mode
When the TCC is used in the Down-counting mode, the transfer of the PERBUF register value to the PER register is delayed by one counter cycle; therefore, do not use the LUPD feature with the PER register.
Work Around
In the Down-counting mode, write period value directly to the PER register instead of writing to the PERBUF register. Alternatively, the Up-counting mode in the TCC can be used if the LUPD feature is required.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Incompatible with EVSYS in SYNC/RESYNC Mode
The TCC peripheral is not compatible with an EVSYS channel in the SYNC or RESYNC mode.
Work Around
Use the TCC with an EVSYS channel in the ASYNC mode.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
2RAMP Mode with Hi-resolution Reference Multiple Restarts
In the two Ramp modes (RAMP2, RAMP2A, RAMP2C, and RAMP2CS), a re-trigger is not supported in the Dithering mode.
Work Around
None.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Corrupted Re-trigger Event Waveform Output
If a Re-trigger event (EVCTRL.EVACTn = 1, RETRIGGER) occurs at the Channel Compare Match [n] time, the next Waveform Output [n] is corrupted.
Work Around
Use two channels to store their two successive (n and n+1) CC register values and combine their related waveform outputs to make signal redundancy.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
RAMP2 Feature in Down-Counting Mode
The Timer/Counter Counting-down mode (CTRLBCLR.DIR = CTRLBSET.DIR = 1) is not supported in RAMP2 operations (RAMP2, RAMP2A, RAMP2C, and RAMP2CS).
Work Around
Use the Timer/Counter Up-counting mode (CTRLBCLR.DIR = CTRLBSET.DIR = 0).
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |
Watchdog Timer (WDT)
Run Mode Watchdog Counter is Not Cleared Before Standby Sleep Instruction
When the interval between clearing the WDT (in other words, clearing the Run mode watchdog counter) and the sleep instruction is less than one WDT clock cycle, the Run mode watchdog counter is not cleared. When using Low-Power RC Oscillator (LPRC) as a clock source, the interval is one LPRC clock. Since the watchdog timer is in the LPRC domain, which is much slower than the CPU clock, the sleep instruction is executed even before clearing the Run mode watchdog counter. Hence, the Run mode watchdog counter remains frozen at its last count instead of clearing to 0.
While in the Standby Sleep mode, the Sleep mode watchdog counter increments. At the end of the Watchdog Timer Postscaler (WDTPS), it generates a Non-Maskable Interrupt (NMI), which causes the CPU to wake up.
After wake-up, the user expects that because the WDT is cleared just before going to sleep, an entire WDT period is available before the WDT needs to be cleared again. However, because the Run mode counter is not cleared before going into sleep, the WDT Reset occurs earlier than expected.Work Around
- Add a delay of more than one WDT Clock (LPRC clock) between clearing of the WDT and execution of sleep instruction.
- Execute the WDT clear instruction as soon as the CPU wakes up.
Affected Silicon Revisions
| A0 | ||||||
|---|---|---|---|---|---|---|
| X |