36.4.1.2 General Call Addressing Support
The I2C Specification reserves the address
0x00 as the
General Call address. The General Call address is used to address all client modules
connected to the bus at the same time. When a host issues a General Call, all client
devices should, in theory, respond with an ACK. The General
Call Enable (GCEN) bit determines whether client hardware will respond to a
General Call address. When GCEN is set (GCEN = 1), client hardware will
respond to a General Call with an ACK, and when GCEN is clear
(GCEN = 0), the General Call is ignored, and the client responds with a
NACK. When the module receives a General Call, the ADRIF
bit is set and the address is stored in I2CxADB0. If the ADRIE bit is set, the module will generate an interrupt and stretch the
clock after the 8th falling edge of SCL. This allows the client to determine the
acknowledgment response to return to the host (see figure below).
Important: When using the General
Call addressing feature, loading the I2CxADR0/1/2/3 registers with the
0x00 address is not recommended. Additionally, client hardware only
supports General Call addressing in 7-bit Addressing modes.