2.1 PIC32CM LE00/LS00/LS60
Click on the following links to check various collaterals:
PIC32CM Lx Videos
Sl. No | Type/ Focus Area | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | Getting Started with Tools | N/A | A step-by-step guide explaining:
MPLAB Harmony v3 is configurable through the MCC. Refer to items 6 and 7 for specific instructions to use the MCC. | How to Set-up the Tools Required to Get Started with Harmony v3 |
2 | Getting Started with Tools | PIC32CM LE00 Curiosity Pro Evaluation Kit (EV80P12A) | Introduces the PIC32CM LE00 Curiosity Pro Evaluation Kit and explains the key features of the board. | PIC32CM LE00 Curiosity Pro Evaluation Kit Overview |
3 | Getting Started with application | PIC32CM LE00 Curiosity Pro Evaluation Kit (EV80P12A) | Explains how to create a simple
application on the PIC32CM LE00 using the MCC. This application demonstrates how to toggle an LED by pressing the switch on a timeout basis and viewing the LED toggling rate on the serial terminal. | Getting Started with PIC32CM LE00 Curiosity Pro Evaluation Kit |
4 | Getting Started with Device/ Kit | PIC32CM LS60 Curiosity Pro
Evaluation Kit
(EV76R77A) or PIC32CM LS00 Curiosity Pro Evaluation Kit (EV12U44A) | Introduces TrustZone®-based security
on the PIC32CM LSx Microcontrollers and shows how to create a simple
TrustZone®-based application using the MCC. The application has two projects pertaining to Secure and Non-Secure modes of the PIC32CM LS60/LS00 that work together on the same MCU. It offers security isolation between the trusted and the non-trusted resources in the device. | Getting Started With the TrustZone®-based Security on PIC32CM LSx |
5 | Getting Started with Software Tools | N/A | Explains how to use the MCC Content Manager | MPLAB® Code Configurator Content Manager |
6 | Getting started with Docs | N/A | Introduces the Quick Docs package to help develop applications using Microchip's 32-bit products using the MPLAB Harmony v3 software framework. | Harmony Quick Docs Package |
7 | Getting started with Solutions | N/A | Introduces the MPLAB Harmony Reference Apps package and describes its typical application types and download methods. | Harmony Reference Applications Package |
8 | Overview of the PIC32CM LS00 Curiosity Pro Evaluation kit | PIC32CM LS00 Curiosity Pro Evaluation kit (EV12U44A) | The video explains robust security features like secure boot, Crypto accelerator & Arm® TrustZone® Technology, paired with enhanced peripherals like PTC, Op Amps, ADC, DAC, and Analog comparators. With an Arduino® Uno connector, microBUS socket, and expansion headers, this kit offers limitless development possibilities. | PIC32CM LS00 Curiosity Pro Evaluation Kit Overview |
9 | Overview of the PIC32CM LS60 Curiosity Pro Evaluation kit | PIC32CM LS60 Curiosity Pro Evaluation kit (EV76R77A) | The video says industry’s first ultra-low power microcontroller that brings together a JIL ‘High’ rated secure subsystem and Arm® TrustZone in one package. The MCU integrates TrustFLEX ECC608 secure subsystem & Arm® TrustZone® Technology in one package. | PIC32CM LS60 Curiosity Pro Evaluation Kit |
PIC32CM Lx Training Modules
Sl. No | Type/ Focus Area | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | Getting Started with Device/ Kit | PIC32CM LE00 Curiosity Pro
Evaluation Kit (EV80P12A)
or PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) or PIC32CM LS00 Curiosity Pro Evaluation Kit (EV12U44A) | This training module shows how to
create an application to get started with the SAM L10 using the
MPLAB Harmony v3 software framework. This training module content
can be easily ported for the PIC32CM LE00/ LS00/ LS60. Though the training module is based on the MHC, similar steps and flow can be used to create a project using the MCC. | Getting Started with Harmony v3 Peripheral Libraries on SAM L10 |
2 | Getting started with tools | N/A | Shows how to create a new MPLAB® Code Configurator (MCC) Harmony v3 project from scratch. | Create a new MPLAB Harmony v3 project using MCC |
3 | Getting started with tools | N/A | Shows how to open an existing project and use it with the MCC. | MCC - Open an Existing MPLAB® Harmony v3 Project |
4 | Getting started with tools | N/A | Shows how to install the MPLAB® Code Configurator (MCC) plugin and how to download the MPLAB Harmony v3 framework.. | MPLAB® Code Configurator Overview with MPLAB Harmony Content |
5 | Getting started with tools | This training uses the SAM D5x/E5x. The same training can be used as a reference for other MCUs. | Shows how to create a new MPLAB Harmony v3 project using the MCC. | Create a new MPLAB Harmony v3 project using MCC |
6 | Application Specific | PIC32CM LE00 Curiosity Pro
Evaluation Kit (EV80P12A)
or PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) or PIC32CM LS00 Curiosity Pro Evaluation Kit (EV12U44A) | Shows how to create a low-power
application on a SAM L1x, showcasing the current measurement on Idle
and Standby Sleep modes. The current consumption data is shown on
the data visualizer. The same training module methodology can be ported to the PIC32CM Lx MCU. | Low Power Application on SAM L10 |
7 | Product Feature | PIC32CM LE00 Curiosity Pro
Evaluation Kit (EV80P12A)
or PIC32CM LS60 Curiosity Pro Evaluation Kit(EV76R77A) or PIC32CM LS00 Curiosity Pro Evaluation Kit (EV12U44A) | Shows how to create an Arm® TrustZone® feature application on the SAM L11 microcontroller (MCU) using the MPLAB Harmony v3 software framework. | Arm® TrustZone® Getting Started Application on SAM L11 MCUs |
8 | Secure Boot on PIC32CM LS60 Curiosity Pro Evaluation Kit | PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) | This tutorial shows how to use the Secure Boot feature on the PIC32CM LS60 microcontroller (MCU) using ATECC608B to create a Secure Bootloader and an application that is loaded using the Secure Bootloader. This tutorial helps you get started in developing secure applications on PIC32CM LS60 MCUs using Microchip's Trust Platform Design Suite (TPDS) and MPLAB Harmony v3 software framework. | Secure Boot on PIC32CM LS60 Curiosity Pro Evaluation Kit using MPLAB® Harmony v3 Software Framework |
9 | Low Power Application on a PIC32CM LE00 MCU | PIC32CM LE00 Evaluation Kit (EV80P12A) | This tutorial shows how to create a low power application on a PIC32CM LE00 MCU using the MPLAB® Harmony v3 software framework. | Low Power Application on PIC32CM LE00 (Cortex M23) MCUs Using MPLAB® Harmony v3 Peripheral Libraries |
10 | Arm® TrustZone® Getting Started | PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) | This tutorial shows how to create an Arm® TrustZone® technology feature application on a PIC32CM LS60 microcontroller (MCU) using MPLAB® Harmony v3 software framework. | Arm® TrustZone® Getting Started Application on PIC32CM LS60 (Arm Cortex®-M23) MCUs |
PIC32CM Lx Virtual/On-Demand Training
More virtual trainings are available at Microchip University. Click on the following links for more details:
- Introduction To MPLAB® X IDE
- MPLAB® X Tips and Tricks
- Overview of the Microchip Code Configurator (MCC) Content Manager (CM)
- MPLAB® Code Configurator (MCC) For Simplified Embedded Software Development
- ARM® Cortex®-M Architecture Overview
- Getting Started with Writing Code for the Microchip ARM® Cortex® Microcontrollers
- MPLAB® Harmony v3 Fundamentals
- Simple Applications Using the MPLAB® Harmony v3 Peripheral Libraries
- Creating Advanced Embedded Applications with 32-bit MCUs/MPUs using the MPLAB® Harmony v3 Software Framework
- FreeRTOS Simplified: A Beginner's Guide to Develop and Debug FreeRTOS Applications
PIC32CM Lx Technical Briefs
Sl. No | Type/ Focus Area | Description | Link |
---|---|---|---|
1 | Getting Started | TB3231: This document
explains how to create a simple application on SAM MCU using the
MPLAB Harmony v3 modules. This application sends a “Hello World!”
string to a console running on a computer. Though this document is explained on one MCU, it can be ported for other MCUs. Note: MPLAB Harmony v3
is configurable through the MCC. Refer to items 3 and 4 in PIC32CM Lx
Videos for specific instructions to use the
MCC. | Link |
2 | Getting Started | TB3232: This document explains how to set up the tools required to get started with the MPLAB Harmony v3 software development framework. | Link |
3 | Getting Started | TB3304: How to Add a New Configuration to an Existing MPLAB Harmony v3 Project | Link |
4 | Getting Started | TB3305: How to Use the MPLAB Harmony v3 Project Manifest Feature | Link |
5 | Getting Started | TB3290: MPLAB Harmony v3 Synchronous Drivers and Their Usage in FreeRTOS Based Applications | Link |
6 | Getting Started | TB3269: The Differences Between MPLAB Harmony v3 Synchronous and Asynchronous Drivers and When to Use Them | Link |
7 | Getting Started | TB3291: The Difference Between MPLAB Harmony v3 PLIBs and Drivers, and When to Use Them | Link |
8 | Getting Started | TB3253: How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project | Link |
9 | Getting Started | TB3246: How to Use the MPLAB Harmony v3 Debug System Service | Link |
10 | Peripheral Feature | TB3306: Dual Developer Application Development Use Case with TrustZone on SAM L11 Using MPLAB Harmony v3 | Link |
11 | Low Power | TB3318: Peripheral Power Consumption in Standby Mode for SAM L10/L11 Family of Devices | Link |
12 | Peripheral Feature | TB3222: EEPROM Emulation for Flash-Only Devices | Link |
13 | MCU Feature | TB3183: What is Sleepwalking? How it Helps to Reduce Power Consumption? | Link |
14 | Getting Started | TB3342: Creating the First Application on PIC32CM LSx Microcontrollers Using MPLAB Harmony v3 with MPLAB Code Configurator (MCC) | Link |
15 | Getting Started | TB3355: How to Use the MPLAB® Data Visualizer with 32-bit MCU based Curiosity Nano Evaluation Kits | Link |
PIC32CM Lx Application Notes
Sl. No | Type/ Focus Area | Description | Link |
---|---|---|---|
1 | Getting Started | AN4511: Getting Started with the PIC32CM LE00/LS00/LS60 Curiosity Pro Board | Link |
2 | IoT, Connectivity | AN4152 - PIC32CM LS00/LS60 Ultra Low-Power Secure LoRa Demonstration | Link |
3 | Migration | AN4495: MPLAB Harmony v3 Project Migration application note discusses the migration of an existing MPLAB Harmony v3 based project developed on a particular hardware (microcontroller or development board) platform to another one of Microchip's 32-bit hardware platforms of the user's choice. | Link |
4 | Migration | AN3346: Introduction to MPLAB and Harmony v3 for Atmel Studio and ASF Users | Link |
PIC32CM Lx Application Demonstrations
Sl. No | Type | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | Getting started | PIC32CM LE00 Curiosity Pro | Getting Started Extended Application on PIC32CM LE00 Curiosity Pro Evaluation Kit | Link |
2 | Getting started feature | PIC32CM LS00 Curiosity Pro | TrustZone Getting Started on PIC32CM LS00 Curiosity Pro Evaluation Kit | Link |
3 | Getting started feature | PIC32CM LS60 Curiosity Pro | TrustZone Getting Started on PIC32CM LS60 Curiosity Pro Evaluation Kit | Link |
4 | AWS Secure Cloud Connect | PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) | This specific development board can be pre-provisioned for AWS IoT Core; The application demonstrates MQTT data transfer of light and temperature sensor data from IO1Xpro to AWS IoT core. | Link |
5 | Secure IoT Gateway | PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) | This application demonstrates the anti-cloning feature on the PIC32CM LS60 microcontroller (MCU) using ATECC608B secure element. The application has three projects pertaining to Secure and Non-Secure modes of PIC32CM LS60 that work between the Host and Client devices (PIC32CM LS60/LE00) and offers security isolation between the trusted and the non-trusted resources in the device. | Link |
6 | Smart Lock | PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A) | The application showcases key-less secure access control and monitoring of a deadbolt through multiple methods. | Link |
More application demonstrations are available at Microchip's MPLAB Harmony GitHub repositories. Refer to the following links:
- More application demonstrations on PIC32CM LS60 Curiosity Pro Evaluation Kit and other Development Boards/Kits having the same part number (PIC32CM5164LS60100)
- More application demonstrations on PIC32CM LS00 Curiosity Pro Evaluation Kit and other Development Boards/Kits having the same part number (PIC32CM5164LS00100)
- More application demonstrations on PIC32CM LE00 Curiosity Pro Evaluation Kit and other Development Boards/Kits having the same part number (PIC32CM5164LE00100)
PIC32CM Lx Reference Designs/ Solutions
Sl. No | Type | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | PTC, MCU feature | PIC32CM LE00 ULP Water-Tolerant Touch Reference Design (EV55S83A) | Water Tolerant Demonstration Application | Link |
2 | MCU Feature | Smart Home Lock Reference Design Kit (BN33J40A) | Showcases keyless secure access control and monitoring of a mechanical lock through capacitive touch keypad or a smartphone app. | Link |
3 | MCU Feature | Secure IoT Gateway | The Secure IoT Gateway application provides a secure, pre-configured, compact and managed solution for Internet of Things (IoT) applications. It is designed to provide robust security and connectivity for devices operating on the edge of the network. | Link |
PIC32CM Lx Key Links
- PIC32CM LS60 Curiosity Pro Evaluation Kit (EV76R77A)
- PIC32CM LS00 Curiosity Pro Evaluation Kit (EV12U44A)
- PIC32CM LE00 Curiosity Pro Evaluation Kit (EV80P12A)
- PIC32CM LE00 ULP Water-Tolerant Touch Reference Design (EV55S83A)
- PIC32CM Lx Family of Microcontrollers (MCUs)
- PIC32CM LS00 Curiosity Nano+ Touch Evaluation Kit (EV41C56A)
- MPLAB Harmony Landing Page
- MPLAB Harmony v3 GitHub Reference Application Repository
- MPLAB Harmony v3 GitHub Quick Docs Repository
- Microchip Reference Designs Page