6.2 PIC32MZ DA
Click on the following links to check the various collaterals:
PIC32MZ DA Videos
Sl. No | Type/ Focus Area | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | Getting Started with Tools | N/A | A step-by-step guide explaining:
MPLAB Harmony v3 is configurable through the MCC. Refer to items 3 and 4 for specific instructions for using the MCC. | How to Set-up the Tools Required to Get Started with Harmony v3 |
2 | Getting Started with device/kit | PIC32MZ DA Curiosity Development Board (EV87D54A) | Introduces the PIC32MZ DA Curiosity
Development Kit and explains how to create a simple application on
Microchip's PIC32MZ DA, that is based on a MIPS Core 32-bit
microcontroller using the MPLAB Harmony v3 MHC. Introduces the PIC32MZ DA Curiosity Development Kit and explains how to create a simple application on Microchip's PIC32MZ DA, that is based on a MIPS™ Core 32-bit microcontroller using the MPLAB Harmony v3 MHC. MPLAB Harmony v3 is configurable through the MCC. Refer to items 3 and 4 for specific instructions for using the MCC. | Getting Started with the PIC32MZ DA Curiosity Development Kit |
3 | Getting Started with S/W Tools | N/A | Explains how to use the MCC Content Manager. | MPLAB® Code Configurator Content Manager |
4 | Getting Started with S/W Tools | The video covers DM320209 and EV76S68A, the same content can be replicated for the PIC32MZ DA Curiosity Development Board (EV87D54A) | Explains how to create a new MPLAB Harmony v3 project using the MCC and shows how to migrate an MHC-based project to a MCC based project. | Getting Started with Harmony v3 Using Code Configurator |
5 | Getting started with Docs | N/A | Introduces the Quick Docs package to help develop applications using Microchip's 32-bit products using the MPLAB Harmony v3 software framework. | Harmony Quick Docs Package |
6 | Getting started with Solutions | N/A | Introduces the MPLAB Harmony Reference Apps package and describes its typical application types and download methods. | Harmony Reference Applications Package |
PIC32MZ DA Training Modules
Sl. No | Type/ Focus Area | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | Getting Started with Device/ Kit | PIC32MZ DA Curiosity Development Board (EV87D54A) | Shows how to create an application
to get started with PIC32MZ EF using the MPLAB Harmony v3 software
framework. The training module is based on the MHC. Similar steps and flow can be used to create a project using the MCC. The same training module example/ flow can be ported to the PIC32MZ DA following the same steps. | Getting Started with Harmony v3 Peripheral Libraries on PIC32MZ EF MCUs |
2 | Getting Started with Device/ Kit | PIC32MZ DA Curiosity Development Board (EV87D54A) | This training module shows how to
create an application to get started with the PIC32MZ EF using the
MPLAB Harmony v3 software framework drivers and middleware with
FreeRTOS. The training module is based on the MHC, similar steps and flow can be used to create a project using the MCC. The same training module example or flow can be ported to the PIC32MZ DA following the same steps. | Getting Started with Harmony v3 Drivers and Middleware on PIC32MZ EF MCUs using FreeRTOS |
3 | Getting started with tools | N/A | This training module shows how to create a new MPLAB® Code Configurator (MCC) Harmony v3 project from scratch. | Create a new MPLAB Harmony v3 project using MCC |
4 | Getting started with tools | N/A | This training module shows how to open an existing project and use it with the MCC. | MCC - Open an Existing MPLAB® Harmony v3 Project |
5 | Getting started with tools | N/A | This page will show how to install the MPLAB® Code Configurator (MCC) plugin, and how to download MPLAB Harmony v3 framework. | MPLAB® Code Configurator Overview with MPLAB Harmony Content |
6 | Getting started with tools | This training is uses the SAM D5x/E5x. The same training can be used as a reference for other MCUs. | This tutorial shows how to create a new MPLAB Harmony v3 project using the MCC. | Create a new MPLAB Harmony v3 project using MCC |
7 | Migration | This training is uses the PIC32MZ EF. The same training can be used for other MCUs. | This tutorial shows how to update and configure an existing MPLAB Harmony Configurator (MHC)-based MPLAB Harmony v3 project to a MPLAB Code Configurator (MCC)-based project. | Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project |
PIC32MZ DA Virtual/On-Demand Training
- Introduction To MPLAB® X IDE
- MPLAB® X Tips and Tricks
- Overview of the Microchip Code Configurator (MCC) Content Manager (CM)
- MPLAB® Code Configurator (MCC) For Simplified Embedded Software Development
- MPLAB® Harmony v3 Fundamentals
- Simple Applications Using the MPLAB® Harmony v3 Peripheral Libraries
- Creating Advanced Embedded Applications with 32-bit MCUs/MPUs using the MPLAB® Harmony v3 Software Framework
- FreeRTOS Simplified: A Beginner's Guide to Develop and Debug FreeRTOS Applications
PIC32MZ DA Technical Briefs
Sl. No | Type/ Focus Area | Description | Link |
---|---|---|---|
1 | Getting Started | TB3259: This document
explains how to create a simple application on a PIC32 MCU using the
MPLAB Harmony v3 modules. This application sends a “Hello World!”
string to a console running on a computer. This document is explained on one MCU, it can be ported for other MCUs. Note: Microchip is
moving from the MHC to the MCC. Refer to items 3 and 4 in the
Videos table. | Link |
2 | Getting Started | TB3232: This document explains how to set up the tools required to get started with the MPLAB Harmony v3 software development framework. | Link |
3 | Getting Started | TB3304: How to Add a New Configuration to an Existing MPLAB Harmony v3 Project | Link |
4 | Getting Started | TB3305: How to Use the MPLAB Harmony v3 Project Manifest Feature | Link |
5 | Getting Started | TB3290: MPLAB Harmony v3 Synchronous Drivers and Their Usage in FreeRTOS bBsed Applications | Link |
6 | Getting Started | TB3269: The Differences Between MPLAB Harmony v3 Synchronous and Asynchronous Drivers and When to Use Them | Link |
7 | Getting Started | TB3291: The Difference Between MPLAB Harmony v3 PLIBs and Drivers, and When to Use Them | Link |
8 | Cache | TB3308: Handling Cache Coherency Issues at Runtime Using Cache Maintenance Operations on PIC32MZ MCUs Using MPLAB Harmony v3 | Link |
9 | DMA CRC | TB3196: How to Use the DMA CRC Generator on PIC32 Devices | Link |
10 | Getting Started | TB3296: Multiplexed and Remappable Functionalities on I/O pins on PIC32M Devices Using MPLAB Harmony v3 | Link |
11 | Getting Started | TB3253: How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project | Link |
PIC32MZ DA Application Notes
Sl. No | Type/ Focus Area | Description | Link |
---|---|---|---|
1 | Migration | AN4495: MPLAB Harmony v3 Project Migration application note discusses the migration of an existing MPLAB Harmony v3 based project developed on a particular hardware (microcontroller or development board) platform to another one of Microchip's 32-bit hardware platforms of the user's choice. | Link |
2 | Migration | AN3388: MPLAB Harmony v3 Application Development Guide for MPLAB Harmony v2 Users | Link |
3 | Bootloader | AN3703: Live Update Application on PIC32MZ MCUs Using MPLAB Harmony v3 | Link |
PIC32MZ DA Application Demonstrations
Sl. No | Type | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | Getting Started | PIC32MZ DA Curiosity Development Board (EV87D54A) | Getting Started Application with the PIC32MZ DA Curiosity Development Kit. | Link |
2 | Audio, Graphics | PIC32MZ DA Curiosity Development Board (EV87D54A) | SD Card USB Audio Player on a PIC32MZ DA Curiosity Development Kit + High-Performance 4.3" WQVGA Display Module with maXTouch® Technology using Legato Graphics. | Link |
More application demonstrations are available at Microchip's MPLAB Harmony GitHub repositories. Refer to the following link:
PIC32MZ DA Reference Designs/Solutions
Sl. No | Type | Hardware Board/ Kit Used | Description | Link |
---|---|---|---|---|
1 | HMI, Graphics | PIC32MZ DA Curiosity Development Board (EV87D54A) | Graphical User Interface Demonstrations: MPLAB Harmony v3 has various demonstration examples for creating an intuitive and reliable GUI in applications. | Ref design Link
and |
2 | Graphics, IoT | PIC32MZ DA Curiosity Development Board (EV87D54A) PIC32MZ Embedded Graphics with External DRAM (DA) Starter Kit (DM320008) PIC32MZ Embedded Graphics with External DRAM (DA) Starter Kit (Crypto)(DM320008-C) | This reference design demonstrates a round display user interface that is more attractive for users and differentiates it from a rectangular display. Integrating a MiWi protocol module on the board combines an attractive user interface with broad IoT communication capability in a small package. | Link |