6.3 PIC32MK
Click the following links to check the various collaterals:
PIC32MK Videos
| Sl. No | Type/Focus Area | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting Started with Tools | N/A | A step-by-step guide is provided
below to explain the following:
MPLAB Harmony v3 is configurable through the MCC. Refer to items 3 and 4 for specific instructions to use the MCC. | How to Set-up the Tools Required to Get Started with Harmony v3 |
| 2 | Getting Started with device/ kit | PIC32MK MCM Curiosity Pro Development Board (EV31E34A) | Introduces the PIC32 MK MCM Curiosity Pro Development Board and explains how to create a simple application on Microchip's PIC32 MK MCM 32-bit microcontroller using the MPLAB Code Configurator. | Getting Started on the PIC32MK MCM Curiosity Pro |
| 3 | Getting Started with Software Tools | N/A | Explains how to use the MCC Content Manager. | MPLAB® Code Configurator Content Manager |
| 4 | Getting Started with Software Tools | The video covers DM320209 and EV76S68A. The same content can be replicated for the PIC32MK MCM Curiosity Pro Development Board (EV31E34A). | Explains how to create a new MPLAB Harmony v3 project using the MCC and shows how to migrate an MHC-based project to a MCC based project. | Getting Started with MPLAB Harmony v3 Using Code Configurator |
PIC32MK Training Modules
| Sl. No | Type/Focus Area | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting Started with Device/Kit | PIC32MK MCM Curiosity Pro Development Board (EV31E34A) | Shows how to create an application
to get started with PIC32MK GP MCUs using the MPLAB Harmony v3
software framework. This training module is developed for PIC32MK GP Development Kit. The same flow can be reused for the PIC32MK MCM Curiosity Pro Development Board (EV31E34A). | Getting Started with MPLAB Harmony v3 Peripheral Libraries on PIC32MK GP MCUs |
| 2 | Getting started with tools | N/A | Shows how to create a new MPLAB® Harmony v3 project using MPLAB Code Configurator (MCC) from scratch. | Create a new MPLAB Harmony v3 project using MCC |
| 3 | Getting started with tools | N/A | Shows how to open an existing project and use it with the MCC. | MCC - Open an Existing MPLAB® Harmony v3 Project |
| 4 | Getting started with tools | N/A | Shows how to install the MPLAB Code Configurator (MCC) plug in, and how to download the MPLAB Harmony v3 framework. | MPLAB® Code Configurator Overview with MPLAB Harmony Content |
| 5 | Getting started with tools | This training uses the SAM D5x/E5x. The same training can be used as a reference for other MCUs. | Shows how to create a new MPLAB Harmony v3 project using the MCC. | Create a new MPLAB Harmony v3 project using MCC |
| 6 | Migration | This training uses the PIC32MZ EF. The same training can be used for other MCUs. | Shows how to update and configure an existing MPLAB Harmony Configurator (MHC)-based MPLAB Harmony v3 project to a MPLAB Code Configurator (MCC)-based project. | Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project |
PIC32MK Virtual/On-Demand Training
More virtual trainings are available at Microchip University. Click the following links for more details:
- Introduction To MPLAB® X IDE
- MPLAB® X IDE Tips and Tricks
- Overview of the Microchip Code Configurator (MCC) Content Manager (CM)
- MPLAB® Harmony v3 Fundamentals
- Simple Applications Using the MPLAB® Harmony v3 Peripheral Libraries
- Creating Advanced Embedded Applications with 32-bit MCUs/MPUs using the MPLAB® Harmony v3 Software Framework
- FreeRTOS Simplified: A Beginner's Guide to Develop and Debug FreeRTOS Applications
- Class B Diagnostic Libraries For Functional Safety
PIC32MK Technical Briefs
| Sl. No | Type/Focus Area | Description | Link |
|---|---|---|---|
| 1 | Getting Started | TB3259: This document explains how to
create a simple application on a PIC32 MCU using the MPLAB Harmony
v3 modules. This application sends a “Hello World!” string to a
console running on a computer. This document explains one MCU, it can be ported for other MCUs. Note: Microchip is
moving from the MHC to the MCC. Refer to items 3 and 4 in the
Videos table. | Link |
| 2 | Getting Started | TB3232: This document explains how to set up the tools required to get started with the MPLAB Harmony v3 software development framework. | Link |
| 3 | Getting Started | TB3304: How to Add a New Configuration to an Existing MPLAB Harmony v3 Project | Link |
| 4 | Getting Started | TB3305: How to Use the MPLAB Harmony v3 Project Manifest Feature | Link |
| 5 | Getting Started | TB3290: MPLAB Harmony v3 Synchronous Drivers and Their Usage in FreeRTOS Based Applications | Link |
| 6 | Getting Started | TB3269: The Differences Between MPLAB Harmony v3 Synchronous and Asynchronous Drivers and When to Use Them | Link |
| 7 | Getting Started | TB3291: The Difference Between MPLAB Harmony v3 PLIBs and Drivers, and When to Use Them | Link |
| 8 | ADC | TB3319: How to Perform ADC Conversions with DMA Data Transfers on PIC32MK Devices Using MPLAB Harmony v3 | Link |
| 9 | DMA CRC | TB3196: How to Use the DMA CRC Generator on PIC32 Devices | Link |
| 10 | Getting Started | TB3296: Multiplexed and Remappable Functionalities on I/O pins on PIC32M Devices Using MPLAB Harmony v3 | Link |
| 11 | Getting Started | TB3253: How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project | Link |
PIC32MK Application Notes
| Sl. No | Type/Focus Area | Description | Link |
|---|---|---|---|
| 1 | Migration | AN4495: MPLAB Harmony v3 Project Migration application note discusses the migration of an existing MPLAB Harmony v3-based project developed on a particular hardware (microcontroller or development board) platform to another one of Microchip's 32-bit hardware platforms of the user's choice. | Link |
| 2 | Migration | AN3388: MPLAB Harmony v3 Application Development Guide for MPLAB Harmony v2 Users | Link |
PIC32MK Application Demonstrations
| Sl. No | Type | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting started | PIC32MK GP Development Kit (DM320106) | Getting Started Application Demonstration on a PIC32MK General Purpose (GP) Development Board using MPLAB Harmony v3. | Link |
| 2 | Getting Started | PIC32MK MCM Curiosity Pro Development Board (EV31E34A) | Getting Started Application on the PIC32MK MCM Curiosity Pro Development Board. | Link |
| 3 | Getting Started Extended | PIC32MK MCM Curiosity Pro Development Board (EV31E34A) | Getting Started Extended Application on the PIC32MK MCM Curiosity Pro Development Board. | Link |
More application demonstrations are available at Microchip's MPLAB Harmony GitHub repositories. Refer to the following link:
PIC32MK Reference Designs/Solutions
| Sl. No | Type | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Motor Control |
dsPICDEM MCLV-3 Development Board High Voltage (DM330023-3) dsPICDEM MCLV-2 Development Board Low Voltage ( DM330021-2) and PIC32MK MCM Motor Control Plug In Module (MA320211) or PIC32MK1024 Motor Control Plug In Module (MA320024) | Motor Control for Appliances: There are multiple demonstration examples, which are pre-configured to run on the various motor control development boards, which makes it easy for prototyping motor drive applications. | Reference Design Link |
| 2 | Motor Control | PIC32MK MCA Curiosity Pro Development Board (EV15D86A) PIC32MK MCJ Curiosity Pro Development Board (DT100113) PIC32MK MCM Curiosity Pro Dual-USB Development Kit (EV31E34A) | The PIC32MK MCM multi-motor control solution demonstrates how to use a PIC32MK MCM to drive up to three motors. | Link |