3.1 PIC32CK SG/GC
Click the following links to view the various collaterals:
PIC32CK SG/GC Videos
| Sl.No | Type/Focus Area | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting Started with Tools | N/A | A step-by-step guide is provided
below to explain the following:
Refer to items 2 and 3 for specific instructions to use the MCC. | How to Set-up the Tools Required to Get Started with MPLAB Harmony v3 |
| 2 | Getting Started with Software Tools | N/A | Explains how to use the MCC Content Manager. | MPLAB® Code Configurator Content Manager |
| 3 | Getting Started with Software Tools | Though the video covers DM320209 and EV76S68A, the same content can be replicated for PIC32CK SG Curiosity Ultra Development Board | Explains how to create a new MPLAB Harmony v3 project using the MCC and shows how to migrate an MHC-based project to an MCC-based project. | Getting Started with MPLAB Harmony v3 Using MCC |
| 4 | Getting started with Solutions | N/A | Introduces the MPLAB Harmony v3 Reference Applications package and describes its typical application types and download methods. | MPLAB Harmony Reference Applications Package |
| 5 | TrustZone Getting started with PIC32CK SG |
PIC32CK SG Curiosity Ultra Development Board (EV33A17A) | This video introduces the PIC32CK SG Curiosity Ultra Development Board using MPLAB Harmony and MCC. The project demonstrates TrustZone by separating Secure and Non-Secure applications. | Getting Started with TrustZone using PIC32CK SG01 |
| 6 | Build Smarter with PIC32CK SG/GC using MPLAB Harmony/MCC: Connectivity, Security and Safety |
PIC32CK SG Curiosity Ultra Development Board (EV33A17A) PIC32CK GC Curiosity Ultra Development Board (EV44P93A) | This video provides insights into the PIC32CK SG/GC family of 32-bit MCUs powered by the Arm Cortex-M33 processor. With advanced connectivity, robust security features, such as an integrated HSM, and functional safety support, these microcontrollers are ideal for automotive, industrial, medical, and communication applications. | 32-bit MCU Digest|Build Smarter with PIC32CK SG/GC using MPLAB Harmony/MCC: Connectivity, Security & Safety |
PIC32CK SG/GC Training Modules
| SL.No | Type/Focus Area | Hardware Board/Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | Getting Started with Tools | N/A | Shows how to create a new MPLAB® Harmony v3 project using MPLAB Code Configurator (MCC) from scratch. | Create a new MPLAB Harmony v3 project using MCC |
| 2 | Getting Started with Tools | N/A | Shows how to open an existing project and use it with the MCC. | MCC - Open an Existing MPLAB® Harmony v3 Project |
| 3 | Getting Started with Tools | N/A | Shows how to install the MPLAB Code Configurator (MCC) plug in, and how to download the MPLAB Harmony v3 framework. | MPLAB® Code Configurator Overview with MPLAB Harmony Content |
| 4 | Getting Started with Tools | This training uses the SAMD5x/E5x. The same training can be used as a reference for other MCUs. | Shows how to create a new MPLAB Harmony v3 project using the MCC. | Create a new MPLAB Harmony v3 project using MCC |
| 5 | Migration | This training uses the PIC32MZ EF. The same training can be used for other MCUs. | Shows how to update and configure an existing MPLAB Harmony Configurator (MHC)-based MPLAB Harmony v3 project to a MPLAB Code Configurator (MCC)-based project. | Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC based Project |
| 6 | Getting Started | PIC32CK SG01 Curiosity Ultra Development Board (EV33A17A) | This application demonstrates the TrustZone feature on the PIC32CK SG01 microcontroller (MCU). The application has two projects pertaining to Secure and Non-Secure modes of PIC32CK SG01 that work together on the same MCU and offers security isolation between the trusted and the non-trusted resources in the device. | Arm® TrustZone® Technology Getting Started Application on PIC32CK SG01 (Cortex®-M33) MCUs |
PIC32CK SG/GC Virtual/On-Demand Training
More virtual trainings are available at Microchip University. Click the following links for more details:
- Introduction To MPLAB® X IDE
- MPLAB® X IDE Tips and Tricks
- Overview of the Microchip Code Configurator (MCC) Content Manager (CM)
- Arm® Cortex®-M Architecture Overview
- Getting Started with Writing Code for the Microchip Arm® Cortex® Microcontrollers
- MPLAB® Harmony v3 Fundamentals
- Simple Applications Using the MPLAB® Harmony v3 Peripheral Libraries
- Creating Advanced Embedded Applications with 32-bit MCUs/MPUs using the MPLAB® Harmony v3 Software Framework
- FreeRTOS Simplified: A Beginner's Guide to Develop and Debug FreeRTOS Applications
- Class B Diagnostic Libraries For Functional Safety
PIC32CK SG/GC Technical Briefs
| Sl. No | Type/Focus Area | Description | Link |
|---|---|---|---|
| 1 | Getting Started | TB3231: This document explains how to
create a simple application on a SAM MCU using the MPLAB Harmony v3
modules. This application sends a “Hello World!” string to a console
running on a computer. Though this document is explained on one MCU, and it can be ported to other MCUs. | Link |
| 2 | Getting Started | TB3232: This document explains how to set up the tools required to get started with the MPLAB Harmony v3 software development framework. | Link |
| 3 | Getting Started | TB3304: How to Add a New Configuration to an Existing MPLAB Harmony v3 Project | Link |
| 4 | Getting Started | TB3305: How to Use the MPLAB Harmony v3 Project Manifest Feature | Link |
| 5 | Getting Started | TB3290: MPLAB Harmony v3 Synchronous Drivers and Their Usage in FreeRTOS Based Applications | Link |
| 6 | Getting Started | TB3269: The Differences Between MPLAB Harmony v3 Synchronous and Asynchronous Drivers and When to Use Them | Link |
| 7 | Getting Started | TB3291: The Difference Between MPLAB Harmony v3 PLIBs and Drivers, and When to Use Them | Link |
| 8 | Getting Started | TB3227: Clock System Configuration and Usage on SAM C2x (Cortex M0+) Devices | Link |
| 9 | Getting Started | TB3253: How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project | Link |
| 10 | Getting Started | TB3246: How to Use the MPLAB Harmony v3 Debug System Service | Link |
| 11 | Peripheral Feature | TB3243: How to Wake-up Fast from an External Event on Cortex M0+ Based MCUs | Link |
| 12 | Peripheral Feature | TB3230: Various Timers on SAM Devices | Link |
| 13 | Peripheral Feature | TB3222: EEPROM Emulation for Flash-Only Devices | Link |
| 14 | MCU Feature | TB3183: What is Sleepwalking? How it helps to reduce the power consumption? | Link |
| 15 | Peripheral Feature | TB3170: How the Event System Helps to Lower CPU Load and Power Consumption in Cortex™-M0+ Microcontrollers | Link |
| 16 | Getting Started | TB3358: Creating the First Application on PIC32CK GC Microcontrollers Using MPLAB Harmony v3 with MPLAB Code Configurator (MCC) | Link |
| 17 | Peripheral Feature | TB3367: ADC Sequencing Using DMA and EVENT System on PIC32C and SAM MCUs Using MPLAB Harmony v3 and MCC | Link |
PIC32CK SG/GC Application Notes
| Sl. No | Type/Focus Area | Description | Link |
|---|---|---|---|
| 1 | Migration | AN4495: MPLAB Harmony v3 Project Migration application note discusses the migration of an existing MPLAB Harmony v3-based project developed on a particular hardware (microcontroller or Development Board) platform to another one of Microchip's 32-bit hardware platforms of the user's choice. | Link |
| 2 | Feature specific | AN4383: 32-bit Microcontroller Wafer-Level Chip-Scale Package (WLCSP) | Link |
| 3 | Migration | AN3346: Introduction to MPLAB Harmony v3 for Atmel Studio and ASF Users | Link |
| 4 | Peripheral Feature | AN5807: SERCOM USART on Microchip Cortex Devices (SAM and PIC32C) | Link |
PIC32CK SG/GC Application Demonstrations
| Sl. No | Type/Focus Area | Hardware Kit Used | Description | Link |
|---|---|---|---|---|
| 1 | TrustZone Getting Started | PIC32CK SG Curiosity Ultra Development Board (EV33A17A) | This application demonstrates the TrustZone feature on the PIC32CK SG01 microcontroller (MCU). The application has two projects pertaining to Secure and Non-Secure modes of PIC32CK SG01 that work together on the same MCU and offers security isolation between the trusted and the non-trusted resources in the device. | Link |
| 2 | TrustZone Getting Started Drivers | PIC32CK SG Curiosity Ultra Development Board (EV33A17A) | TrustZone Getting Started on PIC32CK SG01 Curiosity Ultra Development Board using MPLAB Harmony v3 Drivers | Link |
| 3 | TrustZone Getting Started FreeRTOS | PIC32CK SG Curiosity Ultra Development Board (EV33A17A) | Trustzone Getting Started with MPLAB Harmony v3 Drivers on the PIC32CK SG MCU Using FreeRTOS. | Link |
| 4 | Getting Started | PIC32CK GC01 Curiosity Ultra Development Board (EV44P93A) | Getting Started on the PIC32CK GC01 Curiosity Ultra Development Board. | Link |
PIC32CK SG/GC Key Links
- PIC32CK SG/GC Family of Microcontrollers (MCUs)
- PIC32CK SG Curiosity Ultra Development Board (EV33A17A)
- PIC32CK GC Curiosity Ultra Development Board (EV44P93A)
- MPLAB Harmony v3 Landing Page
- MPLAB® Harmony v3 Reference Applications for PIC32CK MCUs
- Microchip Reference Designs Page
- Rapid Prototyping with 32-bit MCUs