1.4 I2C EEPROM AT24 Driver - EEPROM Read Write
This example application shows how to use the AT24 driver to perform read and write operations on AT24 series of EEPROM.
Description
This example uses the AT24 driver to communicate with I2C based AT24CM02 series EEPROMs to perform write and read operations in Bare-Metal environment.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file.
Path of the application within the repository is apps/driver/i2c_eeprom/at24/at24_eeprom_read_write.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| pic32ak_gc_curiosity.X | MPLABX project for Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| pic32ak_gc_curiosity.X | Curiosity Platform Development Board and PIC32AK1216GC41064 General Purpose Dual In-Line Module (DIM) |
Setting Up Curiosity Development Board
- To run the demo, the following additional hardware are required:
- One EEPROM 3 Click board
- Insert EEPROM 3 Click board into the mikroBUS A header of Curiosity Board
- Insert the GP DIM on to DIM slot of Curiosity Board
- Connect the PKoB (J24) on the board to the computer using a USB type-C cable
Running the Application
- Build and program the application using its IDE