4.4 Creating a New MCC Harmony Project
- To create a new project, open MPLAB X IDE and click on File>New
Project.
Figure 4-5. New Project - In the “New Project” pop-up,
click on Microchip Embedded>Application Project(s)>Next.
Figure 4-6. Choose Project - In Select Device window,
select the device from drop down and click Next.
Figure 4-7. Select Device - In Select Compiler window,
Select the latest compiler and click Next.
Figure 4-8. Select Compiler - In Select Project Name and
Folder window, enter the project name and select the project location, and
click Finish.
Figure 4-9. Select Project Name and Folder - Locate the Harmony Framework path and
click Next.
- Now MPLAB X Code Configurator Content
Manager will be launched automatically.
- Click Finish.
Figure 4-10. MCC Required Content - Project Graph window of the
Configurator may have predefined components.
Figure 4-11. Project Graph - Project and Device
resources.
Figure 4-12. Project and Device resources
- Click Finish.