43.6.2 Channel Sequencer
The channel sequencer automatically performs the operations defined by each channel
context. The channel sequencer is enabled when the Context Scan Enable (CSEN) bit is set (CSEN =
1
), and the scan sequence is
executed when the GO bit is set by software or by the reception of an
auto-conversion trigger.The sequence includes all channel contexts that are enabled via the context’s Channel
Scan Enable (CHEN) bit. A context channel is included in the scan sequence
when the CHEN bit is set (CHEN =
1
). If all context channels’ CHEN bits
are clear (CHEN = 0
), the GO
bit is immediately cleared and no conversions or interrupts will occur.A sequence always begins with Context 1, as long as its CHEN bit is enabled. If Context 1’s CONT bit is set (CONT =
1
), the sequencer will scan Context
1 and continue scanning until the threshold test invokes the ADC Channel Threshold
Interrupt flag (ADCHxIF). If the ADC Stop On Interrupt (SOI) bit is set (SOI = 1
) and the channel threshold
interrupt occurs, the scanner will proceed to check Context 1’s ADC Scan Stop On
Interrupt (SSI) bit to determine whether to proceed to the next channel
context. If SSI is set (SSI = 1
), the scanner will clear the GO
bit and the scanner will stop. If the SSI bit is clear (SSI = 0
), the
scanner proceeds to the next channel context that has the CHEN bit set.If Context 1’s CONT bit is set, the SOI bit is clear (SOI =
0
) and the scanner will repeatedly
scan Context 1 until software clears the GO
bit.Important: If a context’s CONT bit is set and both the SOI and SSI bits are clear, the scanner will repeatedly scan that context
indefinitely without scanning any further channels.
If Context 1’s CONT bit is clear (CONT =
0
), the sequencer
will scan Context 1, and when the conversion completes, the channel threshold test is
performed. If ADCH1IF is set, the sequencer checks Context 1’s SSI bit to determine whether to proceed to the next channel context. If SSI
is set, the sequencer clears GO
and the scanner stops. If the SSI bit is clear, the sequencer will proceed to the next
channel that has the CHEN bit set.The scan sequence ends when any context’s channel threshold interrupt occurs and that
context’s SSI bit
is set. If the sequencer has scanned all enabled channels and no interrupt occurs or no
context’s SSI bit is set, the sequencer will return to Context 1 (or the first enabled
channel context) and repeat the scanning process until software clears the GO
bit.
Important: The final channel in a
sequence need to set the Threshold Interrupt Mode Select (TMD) bits to “Interrupt regardless of the threshold test results” (TMD =
111
) and set the SSI bit. These settings allow the scanner to stop after the scan sequence
has completed.The figure below illustrates the operation of the channel sequencer.
Note:
- If all channels are disabled
(ADCSEL[1..4].CHEN =
0
), the scanner stops, but the GO bit remains set. No interrupts will occur. If software relies on a hardware clear of GO to continue code execution, the program will stall indefinitely. - ADC computation modes (Average, Burst Average, etc.) are included in the ‘Perform ADC Operation’ block.