5.2 Creating an Application for PIC® Devices
This section demonstrates how to configure a bootable application configuration for 8-bit PIC® devices.
Description: With the bootloader code built and configured to the needed specifications, configure the target application to work alongside the bootloader instead of erasing the bootloader code from the device and programming the new target application over it. MPLAB X IDE allows the user to set various project configuration properties to match the bootloader configuration. The first step for completing this task is to create a blinking LED project.
-
Create a new MPLAB X IDE project.
Figure 5-39. New Application Project - MCC opens up automatically when a new
project is created. If not, click the MCC button in the menu bar to start the
MPLAB Code Configurator.
Figure 5-40. Open MCC - To keep the build configuration
clean, it is suggested to create at least two project configurations for your
application. One that can be used to prototype your application functionality and
another configuration that builds that application in the manner needed to bootload
it.
Figure 5-41. Open the Project Properties Navigate to Project Properties>Manage Configurations...
With the ‘default’ configuration highlighted, click the Duplicate button, and then Rename the new configuration to ‘bootable’. Click OK.
Figure 5-42. Create the New ‘bootable’ Configuration Set the ‘bootable’ configuration as the active project by click Set Active and then click OK to close the menu.
Figure 5-43. Activate the ‘bootable’ Configuration -
Configure the on-board LED by setting the RF3 pin. Set the Custom Name to LED.
Figure 5-44. LED Configuration -
Configure the on-board Switch by setting the RB4 pin. Set the Custom Name to BTN and enable Weak Pull-ups.
Figure 5-45. BTN Configuration - Add the Delay driver from
Device Resources>Drivers>Timer to the project.
Figure 5-46. Delay Driver -
Press the Generate button in the Project Resources tab to generate the project code.
Important: Make sure to match the Clock Control and Configuration Bits settings to the bootloader project settings.Figure 5-47. Generate Application Code -
For a blinking LED application, add the following code to
main.c
in Source Files under the project folder. Thedelay.h
header file must also be included in the main file.// if the BTN is pressed, reset the device. if (BTN_GetValue() == 0U) { RESET(); } LED_Toggle(); DELAY_milliseconds(200U);
Figure 5-48. Update the Application Code - Add the following code at the top of
the
main.c
file before the main function. This reserves the last bytes to hold the Checksum value. The address presented below in the__at()
is PROGMEM_SIZE - 2, since the Checksum hash size used is two bytes and we are locating the end of the application to be the end of Flash. This address may be different for your device.Note: For Checksum, CRC16 and Check State Flag verification schemes, the hash size is two bytes. For CRC32, the hash size is four bytes.Checksum Verification Scheme
#include <stdint.h> #ifdef __XC8__ #include <xc.h> #endif volatile const uint16_t #ifdef __XC8__ __at(0x1FFFE) #endif applicationFooter __attribute__((used, section("application_footer"))) = 0xFFFF;
CRC32 Verification Scheme
#include <stdint.h> #ifdef __XC8__ #include <xc.h> #endif volatile const uint32_t #ifdef __XC8__ __at(0x1FFFC) #endif applicationFooter __attribute__((used, section("application_footer"))) = 0xFFFFFFFF;
CRC16 Verification Scheme
#include <stdint.h> #ifdef __XC8__ #include <xc.h> #endif volatile const uint16_t #ifdef __XC8__ __at(0x1FFFE) #endif applicationFooter __attribute__((used, section("application_footer"))) = 0xFFFF;
Check State Flag Verification Scheme
#include <stdint.h> #ifdef __XC8__ #include <xc.h> #endif volatile const uint8_t #ifdef __XC8__ __at(0x1FFFE) #endif applicationFooter __attribute__((used, section("application_footer"))) = 0x55;
Figure 5-49. Add Verification Settings in main.c
-
Configure the project properties. Go to File>Project Properties and select PIC18F57Q43 Curiosity Nano under Connected Hardware Tool, DFP version under Packs and the XC8 version under Compiler Toolchain.
Figure 5-50. Set Project Properties - Configure the linker setting for the
used verification scheme.
Compiler and Linker Settings
The following section is intended to provide an explanation of the compiler and linker settings utilized in the PIC18F57Q43 end application project. The example below uses the Checksum verification scheme for demonstration.
- Navigate to the
Project Properties>XC8 Linker>Additional
options. Enter the application start address into the
Codeoffset and enter the algorithm information into the
Checksum box that corresponds with the below verification scheme
Table 5-1. Checksum Example Project Setting Input Codeoffset 0x2000 Checksum 2000-1FFFD@1FFFE,width=-2,algorithm=2
For the above Checksum option, the algorithm arguments can be understood as:
Argument Start-End@Store,width=-Width,algorithm=-Algorithm,offset=Offset,polynomial=Polynomial Start Address 2000 in the above example is the start address of the hash calculation. Changing the start address of the application will require this value to also be changed. End Address 1FFFD in the above example is the end address of the hash calculation. Changing the end address of the application partition will require this value to also be scaled. You must never include the location of the hash data in the calculation of the check sum. This value must be lower than the Store Address. Store Address 1FFFE is the location of the check sum data after hexmate perform the calculation. This address must not be considered for being included in the check sum calculation and must always be greater than the Address 1. Data Width -2 in the above command represents a 2 byte check sum size that will be stored in little endian byte order Hexmate Algorithm 2 in the above command is the algorithm being used for the hexmate operation. Refer to the Hexmate documentation for more information on the algorithm descriptions. CRC Polynomial The polynomial entry is not shown in the above example but it is used to set the polyniomial used for the CRC16 and CRC32 verification algorithms. Refer to the Verification Schemes section for more information. CRC Offset The offset entry is not shown in the above example but it is used to set the remainder value used in the CRC16 and CRC32 calculations. - Refer to the table below
for the Checksum setting for each verification scheme:
Verification Scheme Checksum Algorithm CRC16 2000-1FFFD@1FFFE,width=-2,algorithm=5,offset=FFFF,polynomial=1021 CRC32 2000-1FFFB@1FFFC,width=-4,algorithm=-5,offset=FFFFFFFF,polynomial=04C11DB7 Checksum 2000-1FFFD@1FFFE,width=-2,algorithm=2 Warning: For PIC16 devices, you must include,code=3F
to the end of all of the commands listed above. Example: 2000-1FFFD@1FFFE,width=-2,algorithm=2,code=3FFigure 5-51. Project Properties - Checksum Configuration
Open File>Project Properties. Add the below settings to the XC8 Linker>Fill Flash Memory. These steps enable the mentioned constant to fill all the unused memory space in the generated hex file. Set the Memory address range to:
0x<Application Start Address>:0x<End of Flash Memory>
.Important: For PIC16 devices, the value in the Constant field must be 0x3FFF and the addresses are the word addresses.Figure 5-52. XC8 Linker - Fill Flash Memory - Navigate to the
Project Properties>XC8 Linker>Additional
options. Enter the application start address into the
Codeoffset and enter the algorithm information into the
Checksum box that corresponds with the below verification scheme
- Click Apply and OK to close the project properties. Then, click Clean and Build to the build the project hex file.
With the bootloader client and the application projects created, the image file
can be generated by using the Firmware Image Builder ( pyfwimagebuilder) tool by combining the
bootloader_configuration.toml
file and the application hex
file.
pyfwimagebuilder build -i PIC18F57Q43_App.X.production.hex -c bootloader_configuration.toml -o output.img

End Application Programming
The newly-generated application image can be transferred to the target device using the Microchip Device Firmware Update (pymdfu) tool.
pymdfu update --tool serial --image output.img --baudrate 9600 --port COM48