4.1 Firmware Image Builder (pyfwimagebuilder)
Introduction
The Image Builder (pyfwimagebuilder) is a Command Line
Interface (CLI) that converts the application hex file (*.hex
) into
another format (*.img
) that is directly understood by the
bootloader client. The image builder tool also requires
bootloader_configuration.toml
that is generated by the MCC
Melody 8-Bit MDFU Client library. bootloader_configuration.toml
file contains various device parameters that are added to the generated image file
and are used by the bootloader client to identify the device that is used to create
the application. A few examples of device parameters are: Device ID, Flash row size,
application start address, memory unlock keys, etc. These parameters in the image
file help the bootloader client to perform initial image verification by extracting
the Device ID information and comparing it with the Device ID of the target
device.
pyfwimagebuilder Workflow
- Open the Windows Command Prompt.
-
Install the pyfwimagebuilder using the command:
pip install pyfwimagebuilder
-
Execute the below command to generate the embedded application image file:
pyfwimagebuilder build [-i input.hex] [-c bootloader_configuration.toml] [-o output.img]