| EIC Interrupt | This example application
                                demonstrates how to generate interrupt using the EIC on switch press
                                and indicate it through an LED | 
| PORT Polling | This example application
                                demonstrate how to poll the switch input, and indicate the switch
                                status using the LED | 
| SERCOM USART Blocking | This example application
                                demonstrates how to use the SERCOM peripheral in USART mode to
                                transfer block of data in a blocking manner | 
| SERCOM USART Interrupt | This example application
                                demonstrates how to use the SERCOM peripheral in USART mode to
                                transfer data in a non-blocking manner | 
| Systick Periodic Interrupt | This example shows how to use the
                                SysTick to generate periodic interrupts |