2 Microchip MPLAB® Harmony 3 Release Notes
BSP Release v3.20.1
New Features
- None
Bug Fixes
- Updated BSP for LED_RED PORT PIN to PC14 in SAM9X75 Curiosity Board.
Known Issues
- None
BSP Release v3.20.0
New Features
This release adds support for the following development kits:
Bug Fixes
- None
Known Issues
- None
BSP Release v3.19.0
New Features
This release adds support for the following development kits:
- SAM9x75 Curiosity Development Board
- PIC32MZ W1 WFI32IOT Board
- WBZ451HPE Curiosity Development board
Bug Fixes
- Fixed Vbus issue for PIC32CK_SG01 Curiosity Board
Known Issues
- None
BSP Release v3.18.0
New Features
This release adds support for the following development kits:
Known Issues
- None
BSP Release v3.17.0
New Features
This release adds support for the following development kits:
Bug Fixes
- None
Known Issues
- None
BSP Release v3.16.1
New Features
- None
Bug Fixes
- Corrected file names from upper case to lower case for Linux compatibility in pic32mk_mca_pim_mc, pic32mk_mcf_pim_mc, pic32mk_mcm_pim_mc, sam_e54_pim_mc and sam_e70_pim_mc BSP.
Known Issues
- None
BSP Release v3.16.0
New Features
- Added board specific name to allow code customizations based on BSP.
Known Issues
- None
BSP Release v3.15.0
New Features
This release adds support for the following development kits:
Known Issues
- None
BSP Release v3.15.0-E2
New Features
This engineering release adds support for the following development kits:
- PIC32CK-GC01 Curiosity Ultra Board
- PIC32CK-SG01 Curiosity Ultra Board
Known Issues
- Same as v3.14.0
BSP Release v3.15.0-E1
New Features
- Added support for the PIC32CZ-C80 Curiosity Ultra Board
Known Issues
- Same as v3.14.0
BSP Release v3.14.0
New Features
Added support for the following development kits:
- PIC32MK MCA Motor Control Plug In Module
- DSPICDEM™ MCHV-3 Development Board for PIC32MK1024 Motor Control Plug In Module
- DSPICDEM™ MCHV-3 Development Board for ATSAME54 Motor Control Plug In Module
- DSPICDEM™ MCHV-3 Development Board for ATSAME70 Motor Control Plug In Module
- DSPICDEM™ MCHV-3 Development Board for PIC32MK MCM Motor Control Plug In Module
- SAM9X60 Curiosity Development Board
Known Issues
- BSP LEDs related macros will not be generated if Pin Manager is launched before adding BSP to the project graph. As a workaround, add BSP to the project graph first before launching Pin manager.
BSP Release v3.13.0
New Features
Added support for the following development kits:
- PIC32CM JH01 Curiosity Pro Evaluation Kit
- PIC32MK MCA Curiosity Pro Board
- PIC32CX BZ2 Curiosity Board
- SAMRH707F18 Evaluation Kit
- SAMA7G54 Evaluation Kit
Known Issues
- BSP LEDs related macros will not be generated if Pin Manager is launched before adding BSP to the project graph. As a workaround, add BSP to the project graph first before launching Pin manager.
BSP Release v3.12.0
New Features
- Added support for the CEC1736 Evaluation Board.
Known Issues
- BSP LEDs related macros will not be generated if Pin Manager is launched before adding BSP to the project graph. As a workaround, add BSP to the project graph first before launching Pin manager.
BSP Release v3.11.1
New Features
- None.
Bug Fixes
- Corrected the module path name in SAM E70 PIM, SAM E54 PIM, PIC32MK MCM PIM and PIC32MK MCF PIM BSPs.
- Corrected the message ID used for communicating between the PMSM FOC component and PIC32MK MCF PIM BSP.
Known Issues
- There are no known issues.
BSP Release v3.11.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.10.0
New Features
Added support for the following development kits:
- SAM E51 Curiosity Nano Evaluation Kit
- PIC32 WFI32E Curiosity Board
- WLR089 Xplained Pro Evaluation Kit
- PIC32MM Curiosity Development Board
- PIC32MM USB Curiosity Development Board
- SAM-IOT WG Development Board
- PIC32CM MC00 Curiosity Nano Evaluation Kit
- PL360G55CF Evaluation Board
- PL485 Evaluation Kit
- PL360G55CB Evaluation Board
- SAMR34 Xplained Pro Evaluation Kit
Known Issues
- There are no known issues.
BSP Release v3.9.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.8.2
New Features
- Minor updates to BSP.
Known Issues
- There are no known issues.
BSP Release v3.8.1
New Features
- Updated supported product families.
Known Issues
- There are no known issues.
BSP Release v3.8.0
New Features
Added support for the following development kits:
- SAMA5D27 SOM1 Kit1
Known Issues
- There are no known issues.
BSP Release v3.7.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.6.1
New Features
- Updated PIC32MK MCJ BSP.
Known Issues
- There are no known issues.
BSP Release v3.6.0
New Features
Added support for the following development kits:
- SAM HA1G16A Xplained Pro
- PIC32MZ W1 Curiosity Board
- PIC32MK MCM Curiosity Pro
Known Issues
- There are no known issues.
BSP Release v3.5.0
New Features
Added support for the following development kits:
- SAM DA1 Xplained Pro Evaluation Kit
- SAM D11 Xplained Pro Evaluation Kit
- SAM D10 Xplained Mini Evaluation Kit
- PIC32MX Ethernet Starter Kit II
- PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit
- PIC32MZ Embedded Graphics with Stacked DRAM (DA) Starter Kit (Crypto)
- PIC32MZ Embedded Graphics with External DRAM (DA) Starter Kit
- PIC32MZ Embedded Graphics with External DRAM (DA) Starter Kit (Crypto)
- PIC32MK MCJ Curiosity Pro Board
- PIC32MK GPL Curiosity Pro Board
- SAM RH71 Evaluation Kit
Known Issues
- There are no known issues.
BSP Release v3.4.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.3.0
New Features
Added support for the following development kits:
- MPLAB Starter Kit for PIC32MX1XX/2XX
- PIC32MX1/2/5 Starter Kit
- PIC32MX274 XLP Starter Kit
- SAM E54 Curiosity Ultra Kit
- Curiosity PIC32MX470 Development Board
- Curiosity PIC32MZEF Development Board
- PIC32MZ Embedded Graphics with External DRAM (DA) Starter Kit (Crypto)
- SAM L21 Xplained Pro Evaluation Kit
- SAM L22 Xplained Pro Evaluation Kit
- PIC32 USB Starter Kit III
- SAM9X60 Evaluation Kit
Known Issues
- There are no known issues.
BSP Release v3.2.1
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.2.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.1.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.
BSP Release v3.0.0
New Features
Added support for the following development kits:
Known Issues
- There are no known issues.