1.2.6.1 Binary to C Array script help

Downloading the host script

To clone or download these host tools from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using MCC content manager

Path of the tool within the repository is tools/btl_bin_to_c_array.py

Setting up the Host PC

  • The Script is compatible with Python 3.x and higher

Description

  • This script should be used to convert the binary file to a C style array containing Hex output that can be directly included in target application code

  • It is mainly used when programming the application using the host_app_nvm application in I2C/CAN Bootloader

  • If size of the input binary file is not aligned to device erase boundary it appends 0xFF to the binary to make it aligned and then generates the Hex output

  • User must specify the binary file to convert (-b), hex output file (-o) and the device (-d)

btl_bin_to_c_array

Usage Examples

Below is the syntax to show help menu for the script

python <harmony3_path>/bootloader/tools/btl_bin_to_c_array.py --help
btl_bin_to_c_array_help_menu

Below is the syntax and an example on how to convert the binary file to a C style array containing Hex output

python <harmony3_path>/bootloader/tools/btl_bin_to_c_array.py -b <binary_file> -o <hex_file> -d <device>
python <harmony3_path>/bootloader/tools/btl_bin_to_c_array.py -b <harmony3_path>/bootloader_apps_i2c/apps/i2c_bootloader/test_app/firmware/sam_d20_xpro.X/dist/sam_d20_xpro/production/sam_d20_xpro.X.production.bin -o <harmony3_path>/bootloader_apps_i2c/apps/i2c_bootloader/host_app_nvm/firmware/src/test_app_images/image_pattern_hex_sam_d20_xpro.h -d samd2x