1.1.3 UART Bootloader Configurations

For MCUs

Bootloader Specific User Configurations

For CORTEX-M based MCUs

uart_bootloader_mcc_config_sam

For MIPS based MCUs

uart_bootloader_mcc_config_pic32m
  • Bootloader Peripheral Used:

    • Specifies the communication peripheral used by bootloader to receive the application
    • The name of the peripheral will vary from device to device
  • Bootloader NVM Memory Used:

    • Specifies the memory peripheral used by bootloader to perform flash operations
    • The name of the peripheral will vary from device to device
  • Bootloader Size (Bytes):

    • Specifies the maximum size of flash required by the bootloader
    • This size is calculated based on Bootloader type and Memory used
    • This size will vary from device to device and should always be aligned to device erase unit size
  • Enable Bootloader Trigger From Firmware:

    • This Option can be used to Force Trigger bootloader from application firmware after a soft reset. It does so by reserving the specified number of bytes in SRAM from the start of the RAM. The reserved memory is updated by the application with a pre-defined pattern. The bootloader firmware in the bootloader_Trigger() routine, can check the reserved memory for the pre-defined pattern and enter bootloader mode if the pattern matches.

    • Number Of Bytes To Reserve From Start Of RAM:

      • This option adds the provided offset to RAM Start address in bootloader linker script.
      • Application firmware can store some pattern in the reserved bytes region from RAM start for bootloader to check at reset in bootloader_Trigger() function
  • Use Dual Bank For Safe Flash Update:

    • Used to configure bootloader to use Dual banks of device to upload the application
    • This option is visible only for devices supporting Dual flash banks

Bootloader System Configurations

uart_bootloader_mcc_config_system
  • Application Start Address (Hex):
    • Start address of the application which will programmed by bootloader
    • This value is filled by bootloader when its loaded which is equal to the bootloader size. It can be modified as per user need
    • This value will be used by bootloader to Jump to application at device reset

Note

  • For optimizing the code Bootloader component disables generation of default interrupt and exception files as shown below

  • Enabling these interrupts explicitly may still not work as bootloader uses custom startup file which has its own Interrupt table populating only the reset handler

uart_bootloader_mcc_config_interrupt_disable

For MPUs

Bootloader Specific User Configurations

Bootloader with SD/eMMC media

mpu_uart_bootloader_config_with_sd

Bootloader with Serial Flash media

mpu_uart_bootloader_config_with_serial_flash

Bootloader with NAND Flash media

mpu_uart_bootloader_config_with_nand_flash
  • Bootloader Peripheral Used:

    • Specifies the communication peripheral used by bootloader to receive the application
    • The name of the peripheral will vary from device to device
  • Application Binary Image Path:

    • Application binary image name harmony.bin (by default)
  • Application Start Address (Hex):

    • Start address of the application on which bootloader will load and execute application
    • This value will be used by bootloader to load and jump to application at device reset
  • Bootloader Memory Used (For Serial/NAND Flash):

    • Specifies the Flash Driver used by bootloader to receive the application
    • The name of the Flash Driver will vary from device to device
  • External Memory App Image Address (Hex)(For Serial/NAND Flash):

    • External Memory App Image Address (0x00200000) on which bootloader will program the application image
    • This value will also be used by bootloader to load the application from external memory to the DDR memory and execute it.
  • External Memory Metadata Address (Hex)(For Serial/NAND Flash):

    • External Memory Metadata Address (0x00180000) on which bootloader will program the size of application binary
    • This value will be used by bootloader to read the application image from external memory

MPLAB X Settings(For MPUs)

  • Specifying post build option to automatically generate the Harmony 3 bootloader binary file from ELF file once the build is complete
${MP_CC_DIR}/xc32-objcopy -Obinary ${ImageDir}/${ConfName}.X.${IMAGE_TYPE}.elf ${ImageDir}/harmony_bootloader.bin
mpu_uart_bootloader_mplabx_project_properties