1.3.6.4 Bootloader SHA Binary Generation Script Help
Downloading the host script
To clone or download these host tools from Github,go to the main page of this repository and then click Clone button to clone this repo or download as zip file. This content can also be download using MCC content manager
Path of the tool within the repository is tools/btl_sha_bin_gen.py
Setting up the Host PC
- The Script is compatible with Python 3.x and higher
Description
This script should be used to generate a binary with 32 Byte SHA-256 embedded in it
It takes a binary as an input and generates a SHA-256 Hex Digest on the binary file for the size mentioned and embeds the generated SHA-256 value at the end and creates a new binary file
This script is mostly applicable for generating a bootloader binary with SHA-256 at the end of bootloader region for trustZone Devices when Secure boot feature is enabled through Fuse
The Secure boot feature is enabled by setting the BOOTOPT bit of BOCOR Row for trustZone devices.
- Note: Only BOOTOPT=1 (SHA-256) is supported by script
If BOOTOPT is set to 1 in BOCOR Row fuse bit (0xFFE81001), then at reset the BOOTROM code generates a SHA-256 on the Bootloader region (BOOTPROT) and compares with SHA-256 value written at last 32 Bytes of BOOTPROT region. If there is a mismatch then device will not Bootup
If the above check fails, then bootloader be must re-programmed using the debugger or programmer utility
Memory Layout

The SHA-256 digest is computed on the whole BOOTPROT region, which is composed by the Secure Flash (BOOT region) and the Non-Secure Callable Flash (BOOT region)
The digest reference value for this area is stored at the end of the Secure Flash (BOOT region), just before the Non-Secure Callable Flash (BOOT region)
- The BNSC region is optional and can be zero
Note: The last 32 Bytes where the SHA-256 is stored are not included in the computation.
SHA-256 = ((Secure Flash Boot Region - 32 Bytes) + BNSC)

Usage Examples
Generate the bootloader binary from MPLAB X for bootloader project by disabling fuse settings and enabling the post build script
Make sure you send the device configuration file which has BOOTOPT set to 1 along with thegenerated bootloader sha binary
Below is the syntax to show help menu for the script
python <harmony3_path>/bootloader/tools/btl_sha_bin_gen.py --help
Below is the syntax and an example on how to generate a bootloader binary with SHA-256 and No BNSC region
python <harmony3_path>/bootloader/tools/btl_dev_cfg_gen.py -v -d <device_name> -b <BOOTPROT_size_in_bytes> -n <BNSC_size_in_bytes> -f <Bootloader_binary_path> -o <ouput_binary_path>python btl_sha_bin_gen.py -v -d pic32cm -b 2048 -f <harmony3_path>/bootloader_apps_uart/apps/trustZone/bootloader/Secure/firmware/pic32cm_ls60_cpro_Secure.X/dist/pic32cm_ls60_cpro/production/pic32cm_ls60_cpro_Secure.X.production.bin -o btl_sha.bin