1.4.2.1 Bootloader Trigger Methods
Bootloader can be invoked in number of ways:
-. Bootloader will run automatically if there is no valid application firmware. - Firmware is considered valid if the first word at application start address is not 0xFFFFFFFF
- Normally this word contains initial stack pointer value for MCUs, so it will never be **0xFFFFFFFF** unless device is erased.
- Bootloader application can implement the bootloader_Trigger() function which will be called during system initialization
A GPIO pin can be used as an external trigger to invoke bootloader at startup.
Bootloader can run on application (internal) request if the configured number of bytes from start of SRAM are equal to some trigger pattern (For MCUs).
Example Implementation of bootloader_Trigger()
#define BTL_TRIGGER_PATTERN 0x5048434D static uint32_t *ramStart = (uint32_t *)BTL_TRIGGER_RAM_START; bool bootloader_Trigger(void) { /* Check for Bootloader Trigger Pattern in first 16 Bytes of RAM to enter * Bootloader. */ if (BTL_TRIGGER_PATTERN == ramStart[0] && BTL_TRIGGER_PATTERN == ramStart[1] && BTL_TRIGGER_PATTERN == ramStart[2] && BTL_TRIGGER_PATTERN == ramStart[3]) { ramStart[0] = 0; return true; } /* Check for Switch press to enter Bootloader */ if (SWITCH_Get() == 0) { return true; } return false; }
Application code to trigger bootloader (For OTA bootloader and bootloaders for MPU devices)
bool bootloader_Trigger(void) { /* Check for Switch press to enter Bootloader */ if (SWITCH_Get() == 0) { return true; } return false; }
Application code to trigger bootloader
void invoke_bootloader(void) { uint32_t *sram = (uint32_t *)BTL_TRIGGER_RAM_START; sram[0] = 0x5048434D; sram[1] = 0x5048434D; sram[2] = 0x5048434D; sram[3] = 0x5048434D; NVIC_SystemReset(); }