1.1.1.5 MPU Bootloader memory layout
MPU Bootloader persistent storage layout
For SD/eMMC media
- The SD/eMMC media uses FAT-FS file system to store the Bootloader, Application and AT91bootstrap images.
For NAND/Serial Flash media
The placement of the AT91bootstrap, Bootloader and the application in flash memory should be such that the application will not overwrite the Bootloader/AT91bootstrap, and the Bootloader can properly program the application when it is downloaded.
The application code can be placed anywhere after the bootloader end address. The application start address should be aligned to Erase Unit Size of the device
As the Bootloader code requires the application start address to be mentioned at compile time, it should match in both the application and bootloader
The size of application image stores into Metadata region (address : 0x00180000) in the Flash memory

MPU Bootloader execution memory layout
- The following table shows Bootloader and Application start address in DDR memory for all MPU devices
| Devices | Bootloader | Application |
|---|---|---|
| SAMA5D2 | 0x26F00000 | 0x21000000 |
| SAM9X60 | 0x23F00000 | 0x21000000 |
| SAM9X7 | 0x23F00000 | 0x21000000 |
| SAMA7G5 | 0x66F00000 | 0x61000000 |
For example, SAMA5D2 DDR execution memory layout is shown in the diagram as below