1.9.2 OTA Bootloader execution flow
OTA Bootloader - Dual Bank
On device reset after systme initialize, The Bootloader task starts executing from while(1) super loop
It retrieves the Control Block (Metadata) from inactive bank
- If any error in reading the Control Block (Metadata) it directly jumps Run application
It checks if the Meta Data read is valid.
If valid
- Checks if the blockUpdated flag is set. If set it jumps to Update Control Block (Metadata) step Or continues to Trigger Check
If Invalid
- It continues to Trigger Check
Trigger Check
- If there are no conditions to enter the firmware upgrade mode, the Bootloader jumps to Run application
- Refer to Bootloader Trigger Methods for different conditions to enter firmware upgrade mode
Update Control Block (Metadata)
The following fields are updated in the Control Block (Metadata), then it swaps bank and then triggers reset to Run application
Clears the blockUpdated flag
Set imageType to active
Set status to valid
Run Application
The application start address used to jump to application space can be
Application start address generated during compile time Or
Application start address retrieved from valid Control Block (Metadata)
Calls SYS_DeInitialize() function to release resources used
Jumps to application space to run the updated application

OTA Bootloader - External Memory
On device reset after systme initialize, The Bootloader task starts executing from the SYS_Tasks()
Once the OTA driver is ready, it retrieves the Control Block (Metadata) from serial memory
- If any error in reading the Control Block (Metadata) it directly jumps Run application
It checks if the Meta Data read is valid.
If valid
- Checks if the blockUpdated flag is set. If set it jumps to Programming step Or continues to Trigger Check
If Invalid
- It continues to Trigger Check
Trigger Check
- If there are no conditions to enter the firmware upgrade mode, the Bootloader jumps to Run application
- Refer to Bootloader Trigger Methods for different conditions to enter firmware upgrade mode
Programming
Starts reading the application binary from serial memory and perform erase/program operations on internal flash
Once programming is completed, it generates CRC32 on programmed space of internal flash and verifies it against the CRC32 value stored in Meta data
Once verification is complete it clears the blockUpdated flag in the Control Block (Metadata) and triggers reset to Run application
Run Application
The application start address used to jump to application space can be
Application start address generated during compile time Or
Application start address retrieved from valid Control Block (Metadata)
Calls SYS_DeInitialize() function to release resources used
Jumps to application space to run the updated application