1.2.1.2 Basic Memory layout for MIPS based MCUs
Bootloader placement for various PIC32M product families
The bootloader is placed in Boot Flash Memory (BFM) or Program Flash Memory (PFM) based on the size of the bootloader and available Boot flash memory on the device.
If the bootloader fits into the available BFM, it is placed in BFM. The user application can use the complete area of the program Flash memory.
If the bootloader does not fit into the available BFM, its reset handler is placed in BFM and rest of code is placed in PFM. The user application can use the remaining area of the program Flash memory.
The bootloader exceptions have to be placed at the _ebase_address of bootloader memory region
The application exceptions have to be placed at the _ebase_address of application memory region
The following table shows the available Boot Flash memory and the placement of different bootloaders by product family.
Note:
The Boot Flash and Program Flash memory end addresses may vary from device to device. Refer to respective Data sheets for details of Flash memory layout.

Basic Memory layout