1.8.4.1 Bootloader linker configurations for MIPS based MCUs
Bootloader placement for various PIC32M product families
The bootloader is placed in Boot Flash Memory (BFM) or Program Flash Memory (PFM) based on the size of the bootloader and available Boot flash memory on the device.
If the bootloader fits into the available BFM, it is placed in BFM. The user application can use the complete area of the program Flash memory.
If the bootloader does not fit into the available BFM, it is placed in PFM. The user application can use the remaining area of the program Flash memory.
The following table shows the available Boot Flash memory and the placement of different bootloaders by product family.

Bootloader linker script settings
Bootloader library uses a custom linker script which is generated through MCC
The values populated in the linker script are based on the Bootloader component MCC configurations
The vector address of a given interrupt is calculated using Exception Base (EBASE) CPU register and the _ebase_address should be aligned to 4KB boundary
Note: The below sections provides overview of changes done to bootloader linker scripts when compared to default linker script. The address location and size may vary based on the specific device used
For Bootloaders placed in Boot Flash Memory (PIC32MZ and PIC32MK Devices)
The bootloader start address by default will be start of Boot flash memory (0xBFC00000). This is the default startup location for all PIC32M devices
The Initial 4KB from Bootloader start address are used by Reset Handler and cache_init section followed by rest of bootloader code.
Length of the bootloader is calculated based on the bootloader being added to MCC
XC32 Compiler calculates offset from the EBASE address and initializes the value of interrupt vector offset (OFFx) register. The offset register is combined with EBASE register using a bitwise OR operator to obtain the interrupt vector address that the CPU will jump to when the corresponding interrupt occurs.
Generated linker scripts as explained above is shown here as an example
Bootloader length <bootloader_length> in the below snippet is auto generated based on the bootloader component added in MCC
Note: Cache related sections are not applicable for PIC32MK Devices
PROVIDE(_vector_spacing = 0x0001); PROVIDE(_ebase_address = 0x9FC01000); _RESET_ADDR = 0xBFC00000; _BEV_EXCPT_ADDR = 0xBFC00380; _DBG_EXCPT_ADDR = 0xBFC00480; _SIMPLE_TLB_REFILL_EXCPT_ADDR = _ebase_address + 0; _CACHE_ERR_EXCPT_ADDR = _ebase_address + 0x100; _GEN_EXCPT_ADDR = _ebase_address + 0x180; kseg0_program_mem (rx) : ORIGIN = 0x9FC01000, LENGTH = <bootloader_length> kseg1_boot_mem : ORIGIN = 0xBFC00000, LENGTH = 0x480 kseg1_boot_mem_4B0 : ORIGIN = 0xBFC004B0, LENGTH = 0x1000 - 0x4B0 ... config_BFC0FF40 : ORIGIN = 0xBFC0FF40, LENGTH = 0x4 config_BFC0FF44 : ORIGIN = 0xBFC0FF44, LENGTH = 0x4 config_BFC0FF48 : ORIGIN = 0xBFC0FF48, LENGTH = 0x4 ... ... SECTIONS { .config_BFC0FF40 : { KEEP(*(.config_BFC0FF40)) } > config_BFC0FF40 .config_BFC0FF44 : { KEEP(*(.config_BFC0FF44)) } > config_BFC0FF44 ... ... } /* Boot Sections */ .reset _RESET_ADDR : { KEEP(*(.reset)) KEEP(*(.reset.startup)) } > kseg1_boot_mem .cache_init : { *(.cache_init) *(.cache_init.*) } > kseg1_boot_mem_4B0 ... /* Interrupt vector table with vector offsets */ .vectors _ebase_address + 0x200 : { /* Symbol __vector_offset_n points to .vector_n if it exists, * otherwise points to the default handler. The * vector_offset_init.o module then provides a .data section * containing values used to initialize the vector-offset SFRs * in the crt0 startup code. */ . = ALIGN(4) ; __vector_offset_0 = (DEFINED(__vector_dispatch_0) ? (. - _ebase_address) : __vector_offset_default); KEEP(*(.vector_0)) ... ... /* Default interrupt handler */ . = ALIGN(4) ; __vector_offset_default = . - _ebase_address; KEEP(*(.vector_default)) } > kseg0_program_mem
For Bootloaders placed in Program Flash Memory (PIC32MK Devices)
The bootloader start address by default will be start of Boot flash memory (0xBFC00000). This is the default startup location for all PIC32M devices
As the entire bootloader cannot be placed in BFM, Only the bootloader Reset Handler is placed in BFM. Rest of the bootloader code along with exceptions and vector table will be placed from start of Program Flash memory
XC32 Compiler calculates offset from the EBASE address and initializes the value of interrupt vector offset (OFFx) register. The offset register is combined with EBASE register using a bitwise OR operator to obtain the interrupt vector address that the CPU will jump to when the corresponding interrupt occurs.
To provide maximum flexibility in placement of interrupt vectors:
- The _ebase_address is placed at start of Program flash memory (Example : 0x9D000000) like the default linker script
Generated linker scripts as explained above is shown here as an example
- Bootloader length <bootloader_length> in the below snippet is auto generated based on the bootloader component added in MCC
PROVIDE(_vector_spacing = 0x0001); PROVIDE(_ebase_address = 0x9D000000); _RESET_ADDR = 0xBFC00000; _BEV_EXCPT_ADDR = 0xBFC00380; _DBG_EXCPT_ADDR = 0xBFC00480; _SIMPLE_TLB_REFILL_EXCPT_ADDR = _ebase_address + 0; _GEN_EXCPT_ADDR = _ebase_address + 0x180; kseg0_program_mem (rx) : ORIGIN = 0x9D000000, LENGTH = <bootloader_length> kseg1_boot_mem : ORIGIN = 0xBFC00000, LENGTH = 0x480 kseg1_boot_mem_4B0 : ORIGIN = 0xBFC004B0, LENGTH = 0x1000 - 0x4B0 ... config_BFC03F40 : ORIGIN = 0xBFC03F40, LENGTH = 0x4 config_BFC03F44 : ORIGIN = 0xBFC03F44, LENGTH = 0x4 config_BFC03F48 : ORIGIN = 0xBFC03F48, LENGTH = 0 SECTIONS { .config_BFC03F40 : { KEEP(*(.config_BFC03F40)) } > config_BFC03F40 .config_BFC03F44 : { KEEP(*(.config_BFC03F44)) } > config_BFC03F44 ... ... } /* Boot Sections */ .reset _RESET_ADDR : { KEEP(*(.reset)) KEEP(*(.reset.startup)) } > kseg1_boot_mem ... /* Interrupt vector table with vector offsets */ .vectors _ebase_address + 0x200 : { /* Symbol __vector_offset_n points to .vector_n if it exists, * otherwise points to the default handler. The * vector_offset_init.o module then provides a .data section * containing values used to initialize the vector-offset SFRs * in the crt0 startup code. */ . = ALIGN(4) ; __vector_offset_0 = (DEFINED(__vector_dispatch_0) ? (. - _ebase_address) : __vector_offset_default); KEEP(*(.vector_0)) ... ... /* Default interrupt handler */ . = ALIGN(4) ; __vector_offset_default = . - _ebase_address; KEEP(*(.vector_default)) } > kseg0_program_mem
For Bootloaders placed in Boot Flash Memory (PIC32MX and PIC32MM Devices)
The bootloader start address by default will be start of Boot flash memory (0xBFC00000). This is the default startup location for all PIC32M devices
The Initial memory from Bootloader start address are used by Reset Handler and then followed by rest of bootloader code.
Length of the bootloader is calculated based on the bootloader being added to MCC
The _ebase_address holds the start address of vector table and it must be placed at 4KB boundary after the Reset Handler section
Generated linker scripts as explained above is shown here as an example.
- Bootloader length <bootloader_length> in the below snippet is auto generated based on the bootloader component added in MCC
PROVIDE(_vector_spacing = 0x0001); PROVIDE(_ebase_address = 0x9FC01000); _RESET_ADDR = 0xBFC00000; _BEV_EXCPT_ADDR = 0xBFC00380; _DBG_EXCPT_ADDR = 0xBFC00480; _DBG_CODE_ADDR = 0xBFC02000; _DBG_CODE_SIZE = 0xFF0; _GEN_EXCPT_ADDR = _ebase_address + 0x180; kseg0_program_mem (rx) : ORIGIN = 0x9FC00500, LENGTH = <bootloader_length> kseg1_boot_mem : ORIGIN = 0xBFC00000, LENGTH = 0x490 ... config3 : ORIGIN = 0xBFC02FF0, LENGTH = 0x4 config2 : ORIGIN = 0xBFC02FF4, LENGTH = 0x4 SECTIONS { .config_BFC02FF0 : { KEEP(*(.config_BFC02FF0)) } > config3 .config_BFC02FF4 : { KEEP(*(.config_BFC02FF4)) } > config2 } /* Boot Sections */ .reset _RESET_ADDR : { KEEP(*(.reset)) KEEP(*(.reset.startup)) } > kseg1_boot_mem ... .vector_0 _ebase_address + 0x200 + ((_vector_spacing << 5) * 0) : { KEEP(*(.vector_0)) } > kseg0_program_mem ASSERT (_vector_spacing == 0 || SIZEOF(.vector_0) <= (_vector_spacing << 5), "function at exception vector 0 too large") .vector_1 _ebase_address + 0x200 + ((_vector_spacing << 5) * 1) : { KEEP(*(.vector_1)) } > kseg0_program_mem ASSERT (_vector_spacing == 0 || SIZEOF(.vector_1) <= (_vector_spacing << 5), "function at exception vector 1 too large") ... ...
For Bootloaders placed in Program Flash Memory (PIC32MX and PIC32MM Devices)
The bootloader start address by default will be start of Boot flash memory (0xBFC00000). This is the default startup location for all PIC32M devices
As the entire bootloader cannot be placed in BFM, Only the bootloader Reset Handler is placed in BFM. Rest of the bootloader code will be placed from start of Program Flash memory
The _ebase_address is placed at start of Program flash memory (Example : 0x9D000000)
Generated linker scripts as explained above is shown here as an example.
- Bootloader length <bootloader_length> in the below snippet is auto generated based on the bootloader component added in MCC
PROVIDE(_vector_spacing = 0x0001); PROVIDE(_ebase_address = 0x9D000000); _RESET_ADDR = 0xBFC00000; _BEV_EXCPT_ADDR = 0xBFC00380; _DBG_EXCPT_ADDR = 0xBFC00480; _DBG_CODE_ADDR = 0x9FC00490; _DBG_CODE_SIZE = 0x760; _GEN_EXCPT_ADDR = _ebase_address + 0x180; kseg0_program_mem (rx) : ORIGIN = 0x9D000000, LENGTH = <bootloader_length> kseg1_boot_mem : ORIGIN = 0xBFC00000, LENGTH = 0x490 ... config3 : ORIGIN = 0xBFC00BF0, LENGTH = 0x4 config2 : ORIGIN = 0xBFC00BF4, LENGTH = 0x4 SECTIONS { .config_BFC00BF0 : { KEEP(*(.config_BFC00BF0)) } > config3 .config_BFC00BF4 : { KEEP(*(.config_BFC00BF4)) } > config2 } /* Boot Sections */ .reset _RESET_ADDR : { KEEP(*(.reset)) KEEP(*(.reset.startup)) } > kseg1_boot_mem ... .vector_0 _ebase_address + 0x200 + ((_vector_spacing << 5) * 0) : { KEEP(*(.vector_0)) } > kseg0_program_mem ASSERT (_vector_spacing == 0 || SIZEOF(.vector_0) <= (_vector_spacing << 5), "function at exception vector 0 too large") .vector_1 _ebase_address + 0x200 + ((_vector_spacing << 5) * 1) : { KEEP(*(.vector_1)) } > kseg0_program_mem ASSERT (_vector_spacing == 0 || SIZEOF(.vector_1) <= (_vector_spacing << 5), "function at exception vector 1 too large") ... ...
Using Both Boot Flash Panels on PIC32MZ device
For PIC32MZ devices, with two 80 KB Boot Flash panels, bootloader may or may not fit entirely in one Boot Flash panel.
In order to fit some of the Bootloaders, the linker script makes the two Boot Flash panels look like one contiguous Boot Flash memory. Unimplemented areas are blocked using a fill command to the linker
kseg0_program_mem (rx) : ORIGIN = 0x9FC01000, LENGTH = 0x2FF00 - 0x1000 /* Bootloader needs to be placed in both the Boot Flash Panels (lower and upper boot alias). Below region is used to fill 0xFF in reserved space between these two panles. */ protected_reg : ORIGIN = 0x9FC14000, LENGTH = 0x20000-0x14000 ... ... SECTIONS { .fill1 : { FILL(0xFF); . = ORIGIN(protected_reg) + LENGTH(protected_reg) - 1; BYTE(0xFF) } > protected_reg }
Note
Device configuration bits should be updated by bootloader only
The bootloader linker script is generated using generic templates for the device family. Generated linker script should be modified if there any changes or modifications to the specific device being used.