24.5.3.1.2 Modifying a Descriptor in a List
In order to add descriptors to a linked list, the following actions must be performed:
- Enable the Suspend interrupt for the DMA channel.
 - Enable the DMA channel.
 - Reserve memory space in SRAM to configure a new descriptor.
 - Configure the new descriptor:
 - Clear the VALID bit for the existing list and for the descriptor which has to be updated.
 - Read DESCADDR from the Write-Back memory.
- If the DMA has not already fetched
                  the descriptor which requires changes (i.e., DESCADDR is wrong):
- Update the DESCADDR location of the descriptor from the List
 - Optionally clear the Suspend block action
 - Set the descriptor VALID bit to '1'
 - Optionally enable the Resume software command
 
 - If the DMA is executing the same
                  descriptor as the one which requires changes:
- Set the Channel Suspend software command and wait for the Suspend interrupt
 - Update the next descriptor address (DESCRADDR) in the write-back memory
 - Clear the interrupt sources and set the Resume software command
 - Update the DESCADDR location of the descriptor from the List
 - Optionally clear the Suspend block action
 - Set the descriptor VALID bit to '1'
 
 
 - If the DMA has not already fetched
                  the descriptor which requires changes (i.e., DESCADDR is wrong):
 - Go to step 4 if needed.