4.9.3.1 diag_result_t

enum diag_result_t

Contains return codes for the diagnostic tests.

DIAG_PASS

0x81U - Indicates that no Fault was detected by the diagnostic  

DIAG_FAIL

0x42U - Indicates that a Fault was detected by the diagnostic  

DIAG_INVALID_ARG

0x24U - Indicates that the diagnostic was not run successfully due to one or more invalid input arguments when calling the function  

DIAG_UNDEFINED

0x7EU - Indicates that the result of the diagnostic is undefined due to incorrect usage of the API  

DIAG_NVM_STORE_ERROR
0xBDU - Indicates that the NVM controller reported an error when attempting to write a value to nonvolatile memory  

Note:

The enum values are chosen with a specific bit pattern to not overlap with the March diagnostic data backgrounds and avoid accidentally reporting an incorrect result.