2.1 Preliminary Steps
Perform the following before you begin the installation:
- Apply AC power to the PD-9501-10GS, using an operational AC cable with an appropriate ground connection
- Connect an output Ethernet cable to the DATA & POWER OUT port
- Verify that a power-ready Ethernet compatible device is connectedWarning: Do not use a crossover cable between the PD-9501-10GS output port and the load device.
- The PD-9501-10GS can be placed on a desktop. Before placing the PD-9501-10GS:
- Do not cover PD-9501-10GS or block the airflow to the PoE with any foreign objects
- Keep the PD-9501-10GS away from excessive heat and humidity and free from vibration and dust
- Ensure that the cable length from Ethernet network source to the terminal does not exceed 100 meters (330 feet). The PoE is not a repeater and does not amplify the Ethernet data signal.
- Use a splitter if desired; ensure that the splitter is connected close to the terminal and not on the PD-9501-10GS
- No on/off switch exists; simply plug the PD-9501-10GS into an AC power source