2.2.5 Embedded SDK
The Embedded SDK contains the C/C++ source code files for the APIs used to build a Knowledge Pack. Select the Source “Format” when downloading a Knowledge Pack to get the Embedded SDK.

The Embedded SDK is a set of instructions for transforming sensor data into feature vectors that can be classified using a classification algorithm. These instructions can be grouped into six categories. This document describes the requirements implementing a function for each of the categories in depth.
-
Sensor Transforms: Act on a single sample of sensor data directly as a pre-processing step
-
Sensor Filters: Modifies a sensor in place and performs some sort of filtering (i.e., moving average)
-
Segmentation: Looks at the ring buffer and indicates the start of a segment and the length of the segment. Returns 1 when it has found a segment and -1 when it is still looking.
-
Segment Transforms: Perform manipulations on an entire segment of data
-
Segment Filter: Filters out segments preventing them from going forward to classification
-
Feature Generator: Extract meaningful information from a segment of data
-
Feature Transforms: Perform row-wise operations on a single feature vector
-
Recognition: Takes a feature vector as an input and predicts the categorization based on a predefined model
Sensor Transforms (se_tr_xxx.c)
Takes one frame of sample(s) at a time and a pointer to the end of the FrameIDX array
Performs an operation, such as magnitude, and stores it into the FrameIDX array
Returns the number of points added to FrameIDX array
Sensor Filter (se_filter_xxx.c)
Takes one frame of sample(s) at a time and a pointer to the FrameIDX array
Performs an operation on the incoming sample to modify it in some way, i.e., moving average filter
If it needs to, stores information in an internal ring buffer about other data it needs to use
Always returns time synchronized data
Returns -1 while it waits for more data; otherwise, it returns 1 when it has enough data to perform the filter operation
Segmentation Algorithm (sg_xxx.c)
Must have either window size or max buffer length defined as part of the algorithm. This is used to define the buffer size of the circular buffer.
Must make use of the ring buffer without modification to input data or data inside of the ring buffer
All parameters must be passed through a struct seg_params. All user-facing parameters must be defined in the Python input contract with a corresponding c_param:index.
All flags must be part of seg_params as multiple segmenters can use the same segmenter
Must have an init function that describes resetting the ring buffer after a segment is found
Returns 1 if a segment is found; otherwise, returns 0
Segment Filter (sg_filter_xxx.c)
Returns ‘
1’ or ‘0’. ‘1’ if the pipeline continues; ‘0’ if the pipeline should be terminated for this segment.
Segment Transforms (sg_tr_xxx)
Operates a segment of data
- Can modify data in the ring buffer but is not allowed to add new data to the ring buffer or add data to an additional ring bufferNote: This can potentially cause issues. A method to address ring buffer issues is currently unavailable.
Example is tr_strip, which demeans the data in the ring buffer
Feature Generators (fg_xxx.c)
Create a single or multiple features from a segment of data
Adds a feature as a float to the feature vector stored in kb_model
Returns the number of features added to the feature vector
Feature Transforms (fg_tr_xxx.c)
Takes a pointer to the feature generator and feature parameters
Operates on the feature vectors in place
Recognition
Takes a feature vector as input
Returns a classification result
Knowledge Pack Overview
The core of the Embedded SDK is the kb_model_t structure that stores information
for each model. Thekb_model_t defines the overall state machine.
The pointer to this object passes through each function then acts on it to
change/advance its state. The definition for this function is shown below, along
with definitions for each of the parameters.
typedef struct{
int framelen; // Number of columns in the ring buffer this pipeline is associated with
int sframelen; // Number of columns in the streaming data ring buffer this pipeline is associated with
int sg_length; // This is the length of an identified segment of data.
int sg_index; // This is the position of the start of the index in the ring buffer
int last_read_idx; // This is the index of the last read value from the rb
uint8_t parent; // index of the parent model
uint8_t feature_bank_index; // index of the head of the feature bank
uint16_t feature_bank_size; // number of features in a bank
uint8_t feature_bank_number; // number of feature banks
uint16_t feature_vector_size; // The size of the feature vector
uint8_t *feature_vector; // pointer to the current feature vector
uint8_t classifier_type; // This is the classifier type that the model uses
uint8_t classifier_id; // context to use when submitting this models feature vector
seg_params *psegParams; // Pointer to the segmenter data structure
FVCOMP_T *pFeatures; // pointer to the feature vector array
ring_buffer_t *pringb; // pointer to the ring buffer
ring_buffer_t *psringb; // Pointer to the streaming data buffer
SENSOR_DATA_T *frameData; // pointer to array containing the most recently added data sample (placed here then into the ring buffer)
// (Note: we could probably just add directly to the ring buffer instead of doing this copy in the future)
model_feature_gen_f feature_gen; // Pointer to the feature generator function
model_data_streaming_f data_streaming; // Pointer to the streaming data function
model_data_segmentation_f segmentation; // Pointer to the data segmentation function
model_recognize_vector_f recognize_vector; // Pointer to the feature vector classifier function
model_feature_transform_f feature_transform; // Pointer to the feature transform function
uint8_t *model_uuid; //Contains the 16-bytes used to identify the model in the cloud.
int total_classifications; //Contains the total classifications run on the system per power cycle.
kb_profile_t m_profile; //model profiler
} kb_model_t;
The following describes how kb_models are actually used. There are two main types of APIs for data running pipelines:
Passing a single sample at a time using a run model
Passing a buffer segment, then calling run segment
These functions return -1 when there is no classification yet (could be waiting for more data or something else). Other error codes can be returned as other negative numbers. Set up a specific ENUM for these to be defined.
These return 0 for unknown and 1, 2, 3… for the class. By using a combination of the model_index and the class, a user is able to map back to what the actual class represents.
This starts with the kb_run_model API, which is the simplest entry point into
running a model. This takes a piece of sensor data and the model_index to associate
that data with.
int kb_run_model(SENSOR_DATA_T *pSample, int nsensors, int model_index)
{
int ret = -1;
if (kb_data_streaming(pSample, nsensors, model_index))
{
if (kb_segmentation(model_index) == 1)
{
kb_feature_generation_reset(model_index);
if (kb_feature_generation(model_index) == 1)
{
ret = kb_generate_classification(model_index);
kb_feature_generation_increment(model_index);
return ret;
}
else
{
kb_reset_model(model_index);
return -2;
}
}
}
return -1;
}
The model then goes through four main stages:
kb_data_streaming: Handles streaming data that comes in. Returns -1 or 1kb_segmentation: Looks for segments of data and returns 1 or -1kb_feature_generation: Generates features for a specified modelkb_generate_classification: Recognizes the feature vector stored in the model
All of these functions are defined in kb.c and follow a similar pattern. One is
described in more detail here to help you understand the basic design philosophy.
You can look at others in the kb.c file for your own
understanding.
The function kb_recognize takes the model_index. Then, call the
kb_feature_transform function, which takes the generated
feature vector and prepares it to be passed to the trained classifier algorithm.
When callingkb_recognize, the prepared feature vector is fed to the
classifier algorithm. This returns an int value. 65535 is checked for, which is a
reserved pattern for Unknown.
int kb_generate_classification(int model_index)
{
int ret = -1;
if (kb_feature_transform(model_index) == 1)
{
ret = kb_recognize(model_index);
if (ret == 65535)
{
ret = 0;
}
}
return ret;
}