9.5.12.2 Enhanced Strobe Mode Enabled
In order to switch to HS400 mode, the host driver must perform the following steps:
- Initialize the device.
- Select the device with CMD7.
- Read the DEVICE_TYPE[196] field of the Extended CSD register to validate whether the device supports HS400.
- Read the STROBE_SUPPORT[184] field of the Extended CSD register to validate whether the device supports HS400.
- If supported, set the SDMMC_MC3R.ESMEN to ‘1’ to enable the Enhanced Strobe mode in the controller.
- Set the “Timing Interface” parameter in the HS_TIMING[185] field of the Extended CSD register to 0x1 to switch the device to High Speed mode.
- Set SDMMC_HC1R.HSEN to ‘1’ to switch the controller to High Speed mode.
- Set the clock frequency to a value not greater than 52 MHz.
- Read the DRIVER_STRENGTH[197] field of the Extended CSD register to find the supported device drive strengths. Note: This step may be skipped if changes to driver strength are not needed.
- Set the “Selected Driver Strength” parameter in the HS_TIMING[185] field of the Extended CSD register to the appropriate driver strength for HS400 operation.
- Set BUS_WIDTH[183] to 0x06 to select the dual data rate x8 bus mode.
- Set the “Timing Interface” parameter in the HS_TIMING [185] field of the Extended CSD register to 0x3 to switch the device to HS400 mode.
- Set SDMMC_MC3R.HS400EN to ‘1’ to switch controller to HS400 mode.
- Change the SDCLK frequency to the HS400 operating frequency.