11.1.5.3 BSR Mode Entry and Wake-up

The following figure shows the recommended power-down sequence to place the device in BSR mode (Backup Mode with SDRAM in Self-refresh mode to save the context). A combination of the LPM and SHDN signals, both outputs of the Shutdown Controller (SHDWC), requests a special powering mode to the external power supply where VDDIODDR is maintained. These outputs are supplied by VBAT present in BSR mode. In a similar way to the power-down sequence, the NRST signal must be asserted prior to turning the SAMA7D6 power supplies off.

Figure 11-6. Recommended Power Sequence at BSR Mode Entry
Table 11-14. BSR Mode Entry Timing Specification
SymbolParameterConditionsMinMaxUnit
tSHDNSHDN delay at backup mode entryDelay from SHDN low to NRST low0ms
tRSTPDNRST delay at power-downDelay from NRST low to the first supply out of its operating range0ms
The following figure shows the recommended power-up sequence to wake up the device from BSR mode. Upon a Wake-up event (WKUP pin, RTC alarm, etc.), the Shutdown Controller automatically toggles its SHDN output back to VBAT to request the external power supply to restart. This power-up sequence is the same as the one shown in Figure 11-2. In particular, the supply groups definition is the same. The LPM pin is not automatically reset, and therefore the external power supply may enter a power saving state at wake-up. To make the power supply return to normal operation, the LPM pin must be software-reset in the SHDWC as soon as possible in the wake-up process.
Figure 11-7. Recommended Power Sequence at Wake-Up from BSR Mode
Table 11-15. Wake-Up from BSR Mode Timing Specification(1)
SymbolParameterConditionsMinMaxUnit
t0VDDIN33 delayDelay from SHDN high to VDDIN33 turn-on0ms
t1VDDIN33 to periphery group delayDelay from established VDDIN33 to the first periphery group supply established-0.3ms
t2Periphery group to VDDCORE delayDelay from the last periphery group established supply to VDDCORE supply turn-on0ms
t3Reset delay at power-upFrom established VDDCORE to NRST high8ms
Note:
  1. The term "established" refers to a power supply established at 90% of its final value.